Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Shop Tips  -  Power to the Bread Board
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 20 May 2015 3:17 PM Date Created
  • Views 2369 views
  • Likes 12 likes
  • Comments 13 comments
  • pomona_test_wire
  • stem
  • power_cords
  • stem_academy
  • bread_board
Related
Recommended

Shop Tips  -  Power to the Bread Board

jw0752
jw0752
20 May 2015

Previous Shop Tips:

http://www.element14.com/community/people/jw0752/blog/2015/05/11/shop-tips--plate-glass

 

http://www.element14.com/community/people/jw0752/blog/2015/05/16/shop-tips--mind-the-wires

 

 

 

 

Power to the Bread Board:

Until retirement, a couple years ago, I did very little bread boarding of circuits. While my job kept me immersed in the very specific niche of electronics that pertains to Dental Equipment servicing almost no free time was available to experiment or explore further. One of the small problems that was encountered, as I began to bread board, was how to best deliver power to the board. At first I hooked up the banana jacks that came with the bread board kit but, quickly, these were found to be clumsy and not very flexible. I tried alligator clipping to components or to bare wires sticking up from the board. In both of these scenarios the wire or component was often pulled from the board.

 

image

 

image

 

image

 

It was decided that the best solution would be to make up some power supply wires specific for the needs of my shop. The power supplies in my shop all use the standard banana jack / plug for their output connection. So I ordered some good quality test lead wire and some banana plugs.

 

Here is a link to the wire that I chose. It is available in Red and Black, has a 10kV silicone rubber insulation and the wire core is 18 AWG consisting of 192 (41 GA) copper conductors. The feel of the wire is soft and very flexible like a long piece of spaghetti.

 

http://www.newark.com/pomona/6733-2/test-lead-wire-50ft-18awg-copper/dp/63H2515

image

 

 

While it was a little pricey it is better to have a little initial $ pain and not regret every time the wire gets used. The extra wire will come in handy and some of my buddies will want a cord or two also when they see how nice this wire is.

 

Here is the procedure that was followed to make up the bread board power cord that I wanted.

 

image

 

Wires are cut and tagged so resistance can be noted

 

image

 

Banana Plugs are attached to one end of the cords.

 

image

 

On the bread board end of the wire a "Y" is soldered into place.

 

image

 

The "Y" Assemblies.

 

image

 

Wire ends of the "Ys" are completed by adding proper sized pins for the bread board and insulating with shrink tubing.

 

image

 

Completed cords with ID and Resistance labels.

 

Here are some of the examples of why I find this arrangement very useful for my bread board experiments:image

 

If I feel that my circuit will require higher current I double up the wires on each rail.

 

image

 

If higher currents aren't an issue it is really nice to be able to pull V+ and V- both from the upper and lower power rails.

 

 

Occasionally while conducting an experiment it is necessary to have a separate voltage source. While it is perfectly acceptable to build up a small regulator or converter or even just a resistive divider, I have found that a small battery pack with bread board wires is often easier and quicker. Here are my battery packs for bread board experiments.

 

image

 

These are simple tools and modifications but they continue to repay the effort of making them by simplifying hookup and minimizing the problem of having to jury rig hookups and patches to bread board experiments.

 

John

  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +5
    Nicely done, John! I'm doing something similar using a female barrel jack adapter with screw terminals, in which I can fasten a couple of jumper wires
  • DAB
    DAB over 11 years ago +2
    Good blog John. I have to say, you keep your wires in very good shape with labels and nice heat shrink tubing. My lab is considerably more messy. Keep up the good work, DAB
  • mcb1
    mcb1 over 11 years ago +2
    Great idea. I have one of these (well similar with the jacks) but because of the size, it's not often used. I might have to make some of your leads ...much more friendly on smaller boards. Mark
  • e14 Contributor
    e14 Contributor over 11 years ago

    Great idea image  I made my own alligator clip terminated multimeter leads years ago so they can clip directly onto components. This blog post had inspired me to make some terminated with breadboard wires since measurements on breadboards is a regular part of "Timmy" my multimeters pastime!

     

    Thanks for the idea

     

    Lucie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to kellyhensen

    Hi Kelly,

    Thank you, that was nice of you .

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kellyhensen
    kellyhensen over 11 years ago

    John:
    This is great stuff - i love the photos and how precise you are with your labeling of the wires.  I've tagged this blog so that it will appear on the STEM Academy - teachers and educators who might be new to breadboards and using them in the classroom will benefit from this information.  Keep up the good work!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to bluescreen

    Hi Sagar,

    Thanks for checking out the blog. My next post is still about wires but the one following will be back to bread boards.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • bluescreen
    bluescreen over 11 years ago

    Great piece! Makes me want to start tweaking my breadboard too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>