Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog The small challenges in life. Fixing a bad CFL
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 24 Dec 2016 7:31 AM Date Created
  • Views 1609 views
  • Likes 8 likes
  • Comments 10 comments
  • compact_flourescent_lights
Related
Recommended

The small challenges in life. Fixing a bad CFL

jw0752
jw0752
24 Dec 2016

The Compact Flourescent Light or more commonly a CFL. For some time I have been popping open the ones that go bad and salvaging the board components.

 

image

 

This one stopped making light but I could see that the small filament heaters at the two ends of the tube were still working. I opened it up by putting a screw driver in the seam of the plastic base and twisting. If you try this be sure to use some good leather gloves. If you do not at some point the driver will slip and you will stab your hand and be angry that you did not take my advice.  Here is what the insides look like:

 

image

 

Each bulb usually contains the same components; a couple of inductors, 6 diodes, a trigger diode, a high voltage 22 uF electrolytic, a 1:1:1 high frequency transformer, 2 NPN transistors and several capacitors and resistors. I began my search for the problem by checking the transistors and diodes. I had to take the transistor out as it had an unusual base to emitter connection. After checking several other similar transistors and finding a consistent reading I put the it back into the circuit. In a short period of time I found a 2.7 nF 1200V Mylar with a dead short. The capacitor was replaced and the bulb was reassembled. This is the first time I have been able to repair a CFL. I should be unhappy that my time now is worth so little but it was fun and I am happy anytime I can fix something that is not suppose to be fixable.

 

image

 

John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago in reply to DAB +6
    I had to laugh as I used to work on $30,000 x-ray units and now I am specializing in $2 light bulbs. John
  • mcb1
    mcb1 over 9 years ago +3
    Amazing that a simple cap died and took out what is supposed to be a long life lamp. Not sure we should be seeing the connection to power it though ...
  • jw0752
    jw0752 over 9 years ago in reply to mcb1 +2
    Thanks for your correct observation about the test jig. I let expediency get ahead of better judgement in posing the bulb for the picture. This site is generally pretty good about not portraying a cavalier…
Parents
  • mcb1
    mcb1 over 9 years ago

    Amazing that a simple cap died and took out what is supposed to be a long life lamp.

     

    Not sure we should be seeing the connection to power it though ... image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to mcb1

    Thanks for your correct observation about the test jig. I let expediency get ahead of better judgement in posing the bulb for the picture. This site is generally pretty good about not portraying a cavalier attitude towards mains power thanks in large part to your vigilance. Thank you for this.

     

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    Easy fix ...

    We all understand the test jig, but we're all aware that electricity and safety aren't foremost for others.

     

    I understood it was also powered by your isolation transformer, so therefore you'd need to get both leads for it to be unsafe image

     

     

    What surprises me is how little is holding the two halves together.

    I would have though you'd need more than a simple twist, and it would destroy getting it back together.

     

    Cheers

    Mark

     

     

    image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 9 years ago in reply to mcb1

    Hi Mark,

    They aren't all the same with regards to separating. This is one of the better ones. The hard ones it becomes much more important to have a good pair of gloves on when trying to work the screw driver into the crack.

     

    You have a good memory to remember that I work the 120 on my bench off an isolation transformer. You are correct it take two leads to tango in this situation but your cropped replacement photo eliminates any misunderstandings.

     

    The units have the 22 uF electrolytics but I have yet to find one of these failed or damaged. The transistor used in this model is a D128PL which I have not been able to cross reference but the transistor tester shows it as an NPN with a built in flyback diode. There is considerable heat near the circuit board as there is visual evidence of carbonization of the circuit board particularly near the transistors.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 9 years ago in reply to jw0752

    John

    Good advice about the gloves, I'm sure someone will fail to read it.! image

     

    The transistor used in this model is a D128PL

    You could try 2SD128PL.

    Not uncommon for japanese makers to drop the 2S from the front.

     

    I've never subscribed to CFL's.

    My house has Dichroic with suitable beam angle and wattage to suit the requirement, but I do understand some places with recessed fittings where there is little light spill and require 4,6 or even 8 in a medium sixed room.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Problemchild
    Problemchild over 9 years ago in reply to mcb1

    Yeah those components are highly stressed inside of a CFL and rarely do they get near the expected lifetime.

    Hacking them open you can get access to a good source of high voltage components..at least some of them should be in good nick!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • Problemchild
    Problemchild over 9 years ago in reply to mcb1

    Yeah those components are highly stressed inside of a CFL and rarely do they get near the expected lifetime.

    Hacking them open you can get access to a good source of high voltage components..at least some of them should be in good nick!