Personal Blogs
  • Community Hub
  • More
Personal Blogs
John Wiltrout's Blog Using Extremely Sophisticated Electronics to Solve a Real World Problem
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jw0752
  • Date Created: 4 Mar 2017 6:33 AM Date Created
  • Views 2892 views
  • Likes 18 likes
  • Comments 54 comments
  • tilt_alarm
Related
Recommended

Using Extremely Sophisticated Electronics to Solve a Real World Problem

jw0752
jw0752
4 Mar 2017

If you don't want to be disappointed by this blog don't read any further cause I lied.

 

The problem is that I have just signed up for a new Garbage Service. The new bin is to be left on the curb by my house in a very specific position so that the truck can come by and use its robotic arm to pick up the bin and tip it upside down to empty it. The arm then returns the bin to the curb in exactly the same position that I left it. I do not know when the truck comes so I find my self checking the bin several times a day to see if it has been dumped yet. The exercise involved in walking to the curb and looking into the bin is OK and probably actually good for me but the neighbors may notice and wonder why I am obsessed with the trash bin. I wanted a way that I could just look out my door and know immediately if the bin had been tipped or not. Here comes the Extremely Sophisticated Electronics part:

 

image

 

OK its not that sophisticated but one has to at least admit that its simplicity is beautiful. It is powered by 4 AA batteries and uses a Tilt Switch to trigger a small SCR. The SCR turns on a RED / BLUE 1 Hz LED flasher that continues to flash until the reset button is pushed. The circuit has been built into a small plastic box and protected from rain by a sealed plastic freezer bag. Here are pictures of the unit untriggered and triggered.

 

image

 

image

 

Before attaching the unit to the Trash Bin I called the company to see if they minded if I drilled (2) 3.175 mm holes so that I could mount the alarm. They told me "sure you can drill the holes as long as you don't mind paying for the bin". No Holes! OK. Back to the drawing board yielded an the idea to mount a bracket to the Alarm and then use a hose clamp to attach to the handle of the bin without drilling any holes or making any marks. Here is a picture of the Alarm mounted to the bin.

 

image

 

And

 

image

 

Now all I have to do is count the minutes until Tuesday when I can test it out.

 

John

  • Sign in to reply

Top Comments

  • jw0752
    jw0752 over 9 years ago +8
    Final Report: The pickup has occurred twice since the windy day. Both times the bin was placed back where I left it and the blinking Red Blue LED was visible from my door even in sunlight. The eye is very…
  • michaelkellett
    michaelkellett over 9 years ago +7
    I hate to disappoint you John but this isn't going to work. On Tuesday you'll hear a bit of noise in the street and you'll look out of your window just in time to see one of those cute little bomb disposal…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to Workshopshed +7
    Andy Clark (Workshopshed) wrote: Looks interesting, my only concern is that it's going to physically interfere with the trucks equipment Tomorrow is the big day. I have four possible scenarios: - the collectors…
Parents
  • Workshopshed
    Workshopshed over 9 years ago

    Before leaving for work on Thursday, I carefully align my bin with the edge of the path.

    When I return if the bin has been moved slightly, e.g. is 3 doors down upside down in a bush, then I know that the bin men have visited.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 9 years ago in reply to Workshopshed

    My system is that I wake up late, by which time the trash collectors have already been by.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 9 years ago in reply to Workshopshed

    My system is that I wake up late, by which time the trash collectors have already been by.

    • Cancel
    • Vote Up +5 Vote Down