Personal Blogs
  • Community Hub
  • More
Personal Blogs
Mark's Blog A brief update on the LED driver application
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Instructorman
  • Date Created: 12 Nov 2013 6:31 PM Date Created
  • Views 401 views
  • Likes 0 likes
  • Comments 0 comments
  • led
  • ws2811
  • pic
Related
Recommended

A brief update on the LED driver application

Instructorman
Instructorman
12 Nov 2013

This weekend I successfully developed a coding approach that allowed me to drive the LED strings discussed in previous posts with a PIC microcontroller.  My work with the Agilent 33522B ARB gave me enough insight into timing and power supply loading that I could begin work on writing code to get a PIC to generate pulse streams to produce light displays on the LED strings.

 

In upcoming blog posts I will continue to illustrate how the Agilent ARB was used to characterize the LED devices and the approach I took that enabled full control of the LED strings using a PIC microcontroller.  I challenged myself to write the pulse generating routine without resorting to in-line assembly, use of hardware timers or interrupts.  The algorithm was devleoped in a really simple high level language - PIC BASIC Pro.  A good amount of thought went into getting the algorithm to work so that pulse timing was not violated.  To generate well timed 500 ns pulses I used a 10 MHz external resonator and boosted the clock up to 40 MHz using the PIC's high speed PLL clock multiplier.

 

Writing a function to produce a continuous stream of properly timed pulses in real time was the major hurdle.  Once the funciton was working it took mere minutes to develop all sorts of interesting light patterns - light chasers, color changing fades, sparkles.  There should be enough time for me to get this project to the point where I can place a few LED light strips on the Christmas tree and remotely control the light pattern.

 

I hope to have a post up this weekend sharing what I've done so far.

 

Mark