Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog Frequency Response Analyser Progress
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 24 May 2020 4:54 PM Date Created
  • Views 2273 views
  • Likes 9 likes
  • Comments 10 comments
  • signal generator
  • amplifier
  • dds
Related
Recommended

Frequency Response Analyser Progress

michaelkellett
michaelkellett
24 May 2020

I first blogged about this project in March. Seems quite while ago now but I have found some time to work on it.

The main boards have been made and assembled.

Mostly it works OK, (and one has been used to solve an entirely different problem for a customer.)

One of the connectors is too close to the debug connector but it doesn't need any links of track cuts.

I've spent a lot of time working on the processor and really getting to know it.  The original proof of concept code did all the processing in the ADC interrupt service routing but I've moved away from this to use DMA for the ADCs and DACs and the processing is done on blocks of data. This allows me to use the ARM CMSIS DSP filtering library code.

My first application for this board is for it to work as a dual channel true RMS AC Milli-voltmeter - it can already do tricks that normal DMMs can't match like flat response from DC - 100kHz, but with optional 2nd or 4th order Butterworth or Chebyschev high and low pass filters to control the bandwidth. Currently I've defined 74 low pass filters (I don't make these one at a time - the coefficient and header files are automatically generated by a series of MATLAB scripts.).

 

At about this point some paid for work got in the way, reducing the scale of Frequency Analyser to thought experiments while walking the dog. This maybe wasn't a bad thing because it made me realise that the biggest limitation of the current design is that it's outputs are not beefy enough to realise the potential of the signal processing in terms of real measuring. (It can output +/- 4V pk  but has a 1k source impedance.)

But I'd like to measure general network impedances (anything from coils and capacitors to loudspeakers) and with variable DC bias.

 

So I started thinking about a booster amplifier, and as always when you are just thinking it got quite fancy !

 

At first I wanted +/- 15V from a 50 ohm source, able to drive short circuits or any phase angle load at 10V RMS or 15V DC as appropriate.

DC - 100kHz, (or more if possible), low distortion, low noise and reasonably cheap.

 

The basic power amp looks like this:

 

image

 

In the simulation it manages -80dB 2nd harmonic distortion at 100kHz into 50 ohm load - I'll believe it when I measure it !

The response is flat to well over 1MHz and the power bandwidth equally good.

The front end op amp means that the DC precision is good.

 

But the dog pointed out that you can't use the same DAC for the DDS frequency synthesiser and the DC offset for testing things like capacitors. (Because you might want 14V DC bias and a 1V AC signal - so you would be using only 1/14th of the DAC resolution, and it's only a 12 bit DAC to start with.)

 

So we agreed on a dual 16 bit (slow) DAC to add offsets.

 

And to measure impedances we need to measure on both sides of the built in 50R source resistor - which means we need monitoring on both sides of the resistor, ideally with fast switching which means solid state switches with wide bandwidth, low distortion and low crosstalk.

 

At this point I thought I'd better get on with it before the plot was totally lost - feature creep only limited by the size of the drawing !

 

image

 

The board looks like this:

image

 

 

It's only for prototyping - in the end everything will need to go one board.

 

I've ordered the boards and bits  - so a three week wait for more progress on this will give me some time to work more on the basic analyser - maybe get the display working.

 

MK

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 6 years ago +4
    I was searching my files for some document, and came across old lab coursework I'd written back in college.. I'd totally forgotten, this is how we measured networks during practical lessons back then.…
  • shabaz
    shabaz over 6 years ago +3
    Hi Michael, Really nice project! I've been thinking of making an amplifier for a DDS too, but it never left paper. I was going to use THS3091 but your discrete PA output is much more interesting. I will…
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to shabaz +3
    shabaz wrote: I was searching my files for some document, and came across old lab coursework I'd written back in college.. I'd totally forgotten, this is how we measured networks during practical lessons…
  • dubbie
    dubbie over 6 years ago

    Very nice. Not my cup of tea, but still, nice. Maybe put some wheels on and make it into a mobile robot, then it would be really nice!

     

    Dubbie

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 6 years ago in reply to shabaz

    Hello Shabaz, nice to see you kept your notes !

    I have all my notebooks from when I started working (45 years worth !!) but nothing from school or Uni.

     

    The ADCs on the micro do all the hard work, many of the STM32H7 series  have dual 16 bit ADCs (one has three) - I don't currently know any way of getting dual 16 bit SAR ADCs capable of 2MHz+ sampling rates cheaper - and you get them integrated with a fast processor and dual 12 bit DACs for about £10. I'm only sampling at 500kHz to keep the processing burden manageable.

    The problem with routing the signals is that the switches cost a lot - the 4 mpxs on the amplifier board are about £4 each, relays have other issues and don't cost much less.

    The micro board doesn't currently have signal routing or the option of gain (it can do 10V or 1V RMS full scale sensitivity) so I shall need another little board to add these features.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    I was searching my files for some document, and came across old lab coursework I'd written back in college.. I'd totally forgotten, this is how we measured networks during practical lessons back then.. just with a sig-gen and a 'scope : ).

    image

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    Hi Michael,

     

    Really nice project! I've been thinking of making an amplifier for a DDS too, but it never left paper. I was going to use THS3091 but your discrete PA output is much more interesting. I will ditch my design hehe, since yours is way ahead.

    My offset adjustment was just 10-bit (AD5293 digipot, driving an op-amp similar as you have it (except mine was wired non-inverting), driving the inverting input into the THS3091, but since 10-bit is not very granular I intended to also have a trimmer resistor on the inverting input of the digipot's op-amp for tweaking so that I wouldn't have some non-zero offset I couldn't remove in 10 bits.

     

    I've been playing with CMSIS DSP recently too, it's impressive how these features are available across all (or maybe nearly all) Cortex-M processors.

    Also, it's really cool how you're able to switch the measurements across both outputs. Are they going to ADCs in the microcontroller, or some separate ADC board?

     

    Anyway, it's an awesome project, looking forward to seeing it all come to shape!

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 6 years ago

    Interesting project.

     

    DAB

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
<