Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Kellett's Blog In Praise of Polydoh
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelkellett
  • Date Created: 31 Jan 2023 5:23 PM Date Created
  • Views 2401 views
  • Likes 15 likes
  • Comments 8 comments
  • workholding
  • polydoh
Related
Recommended

In Praise of Polydoh

michaelkellett
michaelkellett
31 Jan 2023

After seeing it recommended by  /members/shabaz I bought myself some Polydoh. It's a low melting point plastic supplied as little spheres. You put it in hot water and it goes clear and moldable. I've used it to make quick covers for pin headers. It sets to a white hard but not brittle white plastic wehn cold. It can be written on with a suitable (indelible) fibre tip pen.

image

Recently I had a different problem.

My wife's sister had bought some Victorian style bath taps but the bezels supplied with them would not slide right up to the body of the tap as she wanted. So I said I would machine the bell shaped bezels, thinking it would be easy to open up the holes on a lathe.

Unfortunately I wasn't able to hold the parts in a lathe chuck, the outer face is not cylindrical and the chuck makes only point contact. If I put anything soft in to protect the polished metal surface the chuck just didn't hold.

The other day I realised that Polydoh could rescue me here.

I started with the bezels on a piece of model board (foamed poly-propylene that you can buy in sheets). The screws are to give the Polydoh something to key onto.

image

Then I moulded on the Poldoh.

image

Once it was set I clamped the model board up in the mill.

image

I used this nifty gadget to find the centres of the existing holes.

image

And then the mill could do its bit.

image

I poured boiling water into the bezels and that softened the Polydoh enough for me to be able to pull them out.

And fit them to the taps:

image

Thanks  /members/shabaz

(You can buy the same stuff in bigger bags and cheaper under the name "Whitemorph")

Blog edited for test purposes 11:07 am 02/02/2023

MK

  • Sign in to reply
  • cstanton
    cstanton over 3 years ago

    Mm, we had a box of this at the hackspace and I totally overlooked it - nice application

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to ralphjy

    Hi Ralph,

    I've not noticed that, it may be an insignificant difference or a particular brand as you say. Usually the mix is one colored bead for (say) 20 plain beads, so it's only a tiny amount of pigment. However, I've noticed that the Whitemorph that Michael mentioned, comes in an all-black variety (i.e. they have already placed the tiny amount of pigment into the beads), which I'm keen to try, since a darker shade could be handy too. However if it solidifies too soon, it is easy to reheat with hot air (which will soften the outer few millimetres depth of it, and then continue working with it. I used it to make a microphone holder once (I had misplaced it), and while it worked great, it would have blended in more if it were black in that case.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 3 years ago

    Great stuff.  I’ll have to try it.

    I read that adding color makes it harder to work with - shortens the setup time.  Might be a problem with a particular brand.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 3 years ago

    Wow!  That is fantastic!  Now I've really got to remember to buy some PlayDoh.
    And shabaz , plastic ends for connectors... I know where to apply that!  Thanks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 3 years ago

    Very neat idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>