Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Wylie's Blog Distributed Fiber Optic Sensing - Beyond Temperature
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelwylie
  • Date Created: 30 Apr 2014 6:13 AM Date Created
  • Views 624 views
  • Likes 2 likes
  • Comments 2 comments
  • sensing
  • distributed
  • fiber
  • sensor
Related
Recommended

Distributed Fiber Optic Sensing - Beyond Temperature

michaelwylie
michaelwylie
30 Apr 2014

In my last blog post I talked about what a distributed sensor is, using a fiber optic cable as a distributed temperature sensor, and a little about spatial resolution. This blog post will talk about going beyond temperature, in fact, it's about measuring distributed strain. You may have noticed the first blogpost didn't discuss the mechanism which allows the optical fiber to be used as a distributed sensor; the mechanism is light scattering and that will be the topic of my next post. One could argue, that the ability to measure distributed strain is, by far, the most economically valuable parameter that can be measured. One very good example is oil pipelines; the fiber can be wrapped helically as shown in Figure 1. The $800 million dollar oil leak by Enbridge in Michigan has shown that we need to be proactive about our aging oil delivery system.

image

Figure 1: Helically Wrapped Fiber on a Pipe with a Local Strain Event.


With a system such as this, if a leak were to occur, shown as a red spot in Figure 1, it would appear as a spike in the local strain of the fiber. If the medium were heated, the spike could appear even larger as some systems are sensitive to both temperature and strain. The response to such an event would appear as shown in Figure 3.

  image

Figure 2: Resolved Strain from the Local Strain Event


Figure 4 shows the results from such an experiment where a pipe was thinned and pressurized. The thinning was done such that it modeled wall thinning from pitting. The strain data was gathered, interpolated, and wrapped around a 3d model.

image

Figure 3: 3D Model Showing Wall Thinning.


Don't forget, next time we'll talk about the sensing mechanism!

  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Good blog.

     

    I wondered how you could use fiber optics as a strain gauge.

    Are you planning to put together a full circuit design to show how a maker could play with the fiber?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to DAB

    Thanks. I could come up with one that wouldn't necessarily be distributed, but you can make a strain gauge by using attenuation. It's really simple in principle; you treat the fiber so that bending it causes lots of loss and then you glue it to something that deforms. Measurand, who I am not affiliated with, does this kind of thing for their sensors. Having said that, all you would need is a light source, fiber, and detector; the calibration would probably make me cry though. For the distributed stuff you need lasers, usually in the communications band (1500 nm 'ish). So, distributed sensing would be a little too expensive for the maker market right now, but you could cobble a system together for maybe $40,000 USD.

     

    You have proposed an interesting idea though, fiber optic sensors for the maker community. I should probably look into that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 12 years ago in reply to DAB

    Thanks. I could come up with one that wouldn't necessarily be distributed, but you can make a strain gauge by using attenuation. It's really simple in principle; you treat the fiber so that bending it causes lots of loss and then you glue it to something that deforms. Measurand, who I am not affiliated with, does this kind of thing for their sensors. Having said that, all you would need is a light source, fiber, and detector; the calibration would probably make me cry though. For the distributed stuff you need lasers, usually in the communications band (1500 nm 'ish). So, distributed sensing would be a little too expensive for the maker market right now, but you could cobble a system together for maybe $40,000 USD.

     

    You have proposed an interesting idea though, fiber optic sensors for the maker community. I should probably look into that.