Personal Blogs
  • Community Hub
  • More
Personal Blogs
Michael Wylie's Blog Trying Out the CodeBug
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: michaelwylie
  • Date Created: 23 Nov 2015 6:12 AM Date Created
  • Views 1349 views
  • Likes 3 likes
  • Comments 9 comments
  • codebug
Related
Recommended

Trying Out the CodeBug

michaelwylie
michaelwylie
23 Nov 2015

I got a CodeBug about a month ago with the intent of cloning the game Simon. I quickly found out the device is severely limited, but very easy to use. This, of course, is the old "Ease of Use" vs "Flexibility" issue for any new device\language. In this case, it was my fault for not checking the capability before jumping in. Even though I wasn't able to create Simon, I was able to have lots of fun with the device. It is incredibly easy to use, but at times, incredibly annoying for advanced users. This is one instance where the device is targeted very well to its intended audience. That can't be stressed enough, they are doing an excellent job at meeting their target audience. My two year old son loves the device, he's always asking for the CodeBug. I can load in a simple name scrolling program and we can identify letters together.

 

To add to the code base for the device I created the basic interface to scroll across the screen with button presses. This is the classic Space Invaders scrolling spaceship type of code. With a random number generator I could add random ships attacking like a scrolling shooter. A screenshot of the code is below, but I also shared it under the name 'Moving Around'.

 

image

 

The code above makes sense if you invert the CodeBug so the buttons point downward. Pressing the B button moves the lit LED to the left and pressing the A button moves the lit LED to the right. The code wraps the lit LED around the edges. I had to practice with the pause time for the best response, which occurred at 200 ms. I also kept track of the old position so that the LED didn't flicker.

 

I'm not a fan of polling buttons; I prefer interrupts, but this is a limit of the environment provided. It would be nice if the inventors could include a random number generator that can generate a random number between two limits. For example, generate a random number between 0 and 4 which could be used to light a random LED on the screen.

  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 10 years ago in reply to johnbeetem +3
    Hi John! The best way to equate it; sometimes we see beginner programmers in Arduino with massive main functions because they've not read the chapter on functions or arrays? In the case of the codebug…
  • michaelwylie
    michaelwylie over 10 years ago in reply to johnbeetem +3
    Shabaz has explained it quite well. Simon should generate a random sequence. The best I could do is generate a pseudo random sequence in the CodeBug. Also, storing the sequence values would be difficult…
  • michaelwylie
    michaelwylie over 10 years ago in reply to johnbeetem +1
    I've searched around some forums and that doesn't seem to be an option yet.
Parents
  • johnbeetem
    johnbeetem over 10 years ago

    I'm curious: why weren't you able to do Simon?  Didn't the original Simon have a 4-bit TMS1000 processor?  I would hope CodeBug would have a lot more processing power than that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to johnbeetem

    Shabaz has explained it quite well. Simon should generate a random sequence. The best I could do is generate a pseudo random sequence in the CodeBug. Also, storing the sequence values would be difficult, since CodeBug has no array functionality.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • johnbeetem
    johnbeetem over 10 years ago in reply to michaelwylie

    Michael Wylie wrote:

     

    Shabaz has explained it quite well. Simon should generate a random sequence. The best I could do is generate a pseudo random sequence in the CodeBug. Also, storing the sequence values would be difficult, since CodeBug has no array functionality.

    I see.  It's like when I had to program stacks and trees in early-1970s BASIC on my high school's computer versus programming in the far more versatile and eloquent PDP-11 assembly language.

     

    Can you bypass CodeBug's pretty graphical programming language and just use C?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 10 years ago in reply to johnbeetem

    I've searched around some forums and that doesn't seem to be an option yet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 10 years ago in reply to johnbeetem

    I've searched around some forums and that doesn't seem to be an option yet.