Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nate Chapman's Blog 3D Printer called "Buzz Lightyear" Part 2 Marlin Firmware Mechanical Endstops (Ramps)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Nate1616
  • Date Created: 5 Feb 2014 7:23 PM Date Created
  • Views 1771 views
  • Likes 0 likes
  • Comments 6 comments
  • 3d
  • printing
Related
Recommended

3D Printer called "Buzz Lightyear" Part 2 Marlin Firmware Mechanical Endstops (Ramps)

Nate1616
Nate1616
5 Feb 2014

I was asked to help get a Cartesian style printer up and running and noticed that the Marlin Firmware was not set correctly for the Mechanical endstop configuration the users had selected.  This doesn't really fit into my printer setup but thought I would talk and explain how to setup the firmware for use with a mechanical endstop.  Lets first discuss if its better to use NO or NC on the endstop.  The answer is NC.  This will prevent the issue of crashing the platform into the endstop if something comes undone.  The wiring configuration will look like this:

1 = com = wire to signal on your electronics

2 = normally closed (NC) = wire to ground on your electronics

3 = normally open = not required

image

Note that most Cartesian style printers have the endstops connected to the min pins on the board.  It is best to disable the max if not used by going into the pins.h file and setting them to -1.

image

Once hookup is complete the Marlin firmware will need updating.   Open the Configuration.h file and scroll down to the line

 

#define ENDSTOPPULLUPS // Comment this out (using // at the start of the line) to disable the endstop pullup resistors.

 

Note that this should NOT be commented out as the pullups need to be supplied by the Ramps board.  Now scroll down and little further to the lines:

 

bool X_MIN_ENDSTOP_INVERTING = false; // set to true to invert the logic of the endstop.

bool Y_MIN_ENDSTOP_INVERTING = false; // set to true to invert the logic of the endstop.

bool Z_MIN_ENDSTOP_INVERTING = false; // set to true to invert the logic of the endstop.

bool X_MAX_ENDSTOP_INVERTING = true; // set to true to invert the logic of the endstop.

bool Y_MAX_ENDSTOP_INVERTING = true; // set to true to invert the logic of the endstop.

bool Z_MAX_ENDSTOP_INVERTING = true; // set to true to invert the logic of the endstop.

 

Make sure that the min endstops are set to false.  This is because when the axis hits the switch a digital 1 will be read so no inverting is needed.  Don't worry about max as you disabled them above.  The last thing to mention is, if you hit home and you notice that the printer is moving the wrong direction check the lines:

 

#define X_HOME_DIR -1

#define Y_HOME_DIR -1

#define Z_HOME_DIR -1

Setting these to -1 will have the bed home left, back and extruder carriage down.  This would be looking at the front of the printer.  I started to add a lot of comments to a standard version of Marlin that I hope will help users get up and printing.  Here is a sample

image

Does anyone find adding detailed comments to Marlin above useful?  If so when its finished I will post it for everyone to download.

 

Nate

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Hi Nate, I came in to this post a little late. I think you are saying that you want your printer to always begin at the stops so that nothing bad happens on powerup? I agree that you should always leave…
  • DAB
    DAB over 12 years ago in reply to Nate1616 +1
    Hi Nate, Now I see it and I agree. If you go with a ground position, then you will not detect a loose or undone cable. Using a high as the default ensures you have connected limit switches when you start…
  • DAB
    DAB over 12 years ago in reply to Nate1616 +1
    Thanks for the clarification. DAB
Parents
  • DAB
    DAB over 12 years ago

    Hi Nate,

     

    I came in to this post a little late.

    I think you are saying that you want your printer to always begin at the stops so that nothing bad happens on powerup?

    I agree that you should always leave the system at some initial position before you begin operation.

    It is an easy check to make with the Boolean input from the limit switches and lets you enter the normal operation mode in safety.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Nate,

     

    I came in to this post a little late.

    I think you are saying that you want your printer to always begin at the stops so that nothing bad happens on powerup?

    I agree that you should always leave the system at some initial position before you begin operation.

    It is an easy check to make with the Boolean input from the limit switches and lets you enter the normal operation mode in safety.

     

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • Nate1616
    Nate1616 over 12 years ago in reply to DAB

    Hey DAB

    What I was trying to say is that when a print is started the machine will find home and move to start positions from there.  Now lets say a wire came unplugged on the endstop or a bad connection was present and the endstops were wired NC.  This will trigger the system to say stop and not have it keep going smashing into the frame or pushing the hot-end into the bed.

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to Nate1616

    Hi Nate,

     

    Now I see it and I agree.  If you go with a ground position, then you will not detect a loose or undone cable.

    Using a high as the default ensures you have connected limit switches when you start.

    Very good idea.

    Thanks

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Nate1616
    Nate1616 over 12 years ago in reply to DAB

    Hello DAB

    Using High as the state when triggered allows for failure to occur but machine to pick this up and stop.  Since the switch is wired normally closed, Ground and Signal are connected pulling the signal Low.  Once the switch is hit or something happens as stated above the ground is cut and signal is pulled high telling the controller to stop movement.

    image

     

    Nate

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to Nate1616

    Thanks for the clarification.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Nate1616
    Nate1616 over 12 years ago in reply to DAB

    No problem DAB.  Thanks for looking at the blog.  I would think that this would get more comments as various questions on 3d printing have appeared in the discussions.  Maybe that means I just explained it to well.  lol probably not.image

     

    Nate