Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Flight Simulator 101 or back to college - part 8: The Earth and its mathematics.
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 19 May 2016 8:42 PM Date Created
  • Views 1816 views
  • Likes 7 likes
  • Comments 19 comments
  • flight_simulator
  • nexgen
  • Math
  • feature_tutorial
  • simulator
Related
Recommended

Flight Simulator 101 or back to college - part 8: The Earth and its mathematics.

phoenixcomm
phoenixcomm
19 May 2016

Why did I say: "The Earth and its mathematics", because all of the math used in flight, or navigational simulators or SPS(games), are based on the Earth and it's dimensions ~ though the NAV simulation represents but a small fraction of the math used in flight simulators.

image
figure 1

➀ Having nothing to do with the definition of Nautical Miles (“nMile”), from ???, we know that at the Earth's equatorial circumference is 21,604.2 [or 21,639 or ???] nMile. From High School Math and Geography, we know that a great circle is defined as any plane which passes through the center of the Earth (if the Earth were a sphere) [see figure 1]. We also know that the shortest distance between any two points of the surface of a spherical Earth must be a great circle route. Now, if the Earth were only a sphere.

➁ From High School Math, we know that a circle has 360ℴ (degrees), So if we divide 21604.2 by 360 or 21604.2n.m. /360 = 60.011 ≈ 60n.m at the equator. Remember that the closer you get to the poles , the longitudinal degrees converge, therefore, the change must be accounted for by using the cosine of the latitude.

 

The following inverse pair of formulas describe the spherical relationships between the difference in distance (Δdist) along a parallel of latitude (lat) corresponding to a difference in longitude (Δlong), and vice-versa.  (The formulas are simply stated here without explanation, but a full explanation of their derivation can be found in the book ‘Astro Navigation Demystified’ ).
  • Δdist = Δlong x Cos(lat), and inversely
  • Δlong = Δdist ÷ Cos(lat)
image
figure 2

 

 

The traditional, historic definition of 1 nMile is 1 minute [= 1/60 degree] of latitude along the Greenwich meridian - thus, by this definition, 60 nMile = 1 degree of latitude; the current standard SI definition: 1 nMile is 1852 meters.

➂ Engineers and Cartographers do use degrees, as anyone who has looked at a map will recognize: latitude and longitude are denoted in degrees, minutes, and seconds; but, we will use radians for angle measurement So what is a radian?

Looking at a circle[figure 2], we get the definition of a Radian as the angle subtended at the center of the circle by an arc of the circumference of the circle whose length is equal to the radius of the circle.

∠XOY = 1 radian, where r = OX = OY = XY

Again from High School Math, we know the total circumference of a circle of radius, r, is 2 ∙ π ∙ r; thus, there are 2 ∙ π Radians in the circumference of a circle.

Since 2 ∙ π radians is equivalent to 360 degrees, a full circle, the relationships are :

  • 1 radian  = 180 / π degrees, and inversely
  • 1 degree = π / 180 radians.

A radian can be written in a variety of ways: 1c, 2 radians, 3r, 4R, 5 ㎭.

The defined and some (approximate) derived relationships between degrees and radians:

360º = 2 ∙ π ㎭

1º = .01745 ㎭

1 ㎭ = 57.2957º

 

Keep Tuned In, More To Come

~~ Cris  image  

19MAY2016

PS. Thank you, Paul, for all your help!

 

 

24MAY2016 fixed title typo it sb its

  • Sign in to reply

Top Comments

  • D_Hersey
    D_Hersey over 10 years ago +1
    Many more writers describe what a radian is than describe the motivation behind using it 360 is convenient when we seek to divide the circle by prime factors of 360, or products thereof In a universe of…
  • phoenixcomm
    phoenixcomm over 10 years ago in reply to balearicdynamics +1
    Hi Enrico, whats up?? please check out http://www.phoenixcomm.net/~phnx2000/sim/demo/index.shtml you can launch it by clicking at the top. This was written in Perl about 8 or 10 years ago. Almost no documentation…
  • DAB
    DAB over 10 years ago +1
    Another post that brings back memories. I remember a lot of meetings during an integrated navigation system design where all of these ghastly details were discussed at great length. Made me want to be…
  • phoenixcomm
    phoenixcomm over 10 years ago in reply to D_Hersey

    can you also measure angles with this method? say you have an angle of 30 deg. in some calculations pi does not drop out. remember in aircraft all angles are degrees. you can add and subtract an angle as long as there both in degrees and so will your output. and btw who came up with this (your) method. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • D_Hersey
    D_Hersey over 10 years ago

    Whole turn = 360 degrees = 2 pi rad

     

    puts the modulus at one

     

    works well with floating point

     

    1 seems less arbitrary than 360

     

    If the 2 pi term 'drops out,' why put it in?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 10 years ago in reply to phoenixcomm

    Nice demo and fast algorithm. image

     

    Converting from Perl is just a challenge ! I've done something like this running on a PHP server. I have a problem on my server just in these days but as it is solved I put it online so you can check how it works.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 10 years ago in reply to DAB

    Right... And I have bridge to sell you!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 10 years ago

    Another post that brings back memories.

     

    I remember a lot of meetings during an integrated navigation system design where all of these ghastly details were discussed at great length.

     

    Made me want to be a flat earth adherent.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>