This is the ADF Control Head that I chose for my project. It is a Collins 614L-8. they are plentiful on eBay
The Analysis The Unit is tuned via a 400Hz synchro transmitter. So it looks like I will have to find a replacement for the synchro. The Loop Switch in the upper left must be rewired and the switch logic for the Band Selector Switch behind the Tuning Knob seems ok, but that will have to be verified. The Gain Control is just a 5k pot, and the Function Switch behind it just needs some pull-up resistors. It looks like I can drive the Tuning Meter with a PWM signal from the controller. Also, there is a BFO Switch that
PS: In TM 11-5826-225-35 section 1-32 Receiver Tuning Meter page 40 says:
"Tuning Meter is M301 mounted on the control unit front panel is a dc microammeter requiring 100 microamperes of current for full-scale deflection. The negative side of M301 is grounded.."
The Plan Well first I need to score a copy of the maintenance manual they are kind of pricey on eBay so I dug a little more. In the military, the Control Unit is part of AN/ARN-83 and I found pdf copies of TM 11-5826-225-12 and TM 11-5826-225-35 with schematic, part diagrams, etc. Also, you can score the operator's manual here.
Next, we have to identify the goes inta and the goes outas, so here goes:
| Connections Map | ||||
| PIN | I/O | DESCRIPTION | CPU PORT | CPU PIN |
| O | Loop Ant, Right Step | |||
| O | Loop Ant, Right Slew | |||
| O | Loop Ant, Left Step | |||
| O | Loop Ant, Left Slew | |||
| O | Function Switch, ADF | |||
| O | Function Switch, ANT | |||
| O | Function Switch, LOOP | |||
| O | Range Switch, 190 – 400 | |||
| O | Range Switch, 400 – 850 | |||
| O | Range Switch, 850 – 1750 | |||
| O | BFO Switch | |||
| O | Gain Control, Bottom | |||
| O | Gain Control, Top | |||
| O | Gain Control, Arm | |||
| I | Tuning Meter | |||
| G | GROUND | |||
| P | Dial Lamps | |||
| P | Panel Lamps | |||
| D | Syncro - L1 | |||
| D | Syncro - L2 | |||
| D | Syncro - L3 | |||
| D | Syncro 400 hz power | |||
| **NOTE: O = Output; I = Input; P = Power; D = To Be Deleted | ||||
Cris ~

-
DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Comment-
DAB
-
Cancel
-
Vote Up
0
Vote Down
-
-
Sign in to reply
-
More
-
Cancel
Children