Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator How to add old ps/2 keyboard interface to an Arduino
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 14 May 2024 2:37 AM Date Created
  • Views 960 views
  • Likes 5 likes
  • Comments 4 comments
  • flight simulator
  • nexgen
  • diy cockpit
  • ps2_keyboard_encoder
  • arduino
  • software
Related
Recommended

How to add old ps/2 keyboard interface to an Arduino

phoenixcomm
phoenixcomm
14 May 2024

imageHow many PS/2 keyboards do you have? More than one, I'd bet. Well, stop trying to hang them on your tree, and use them not the whole thing just the encoder. BTW that's the little black thing on the rear. 

image
1----DATA
3----GROUND
4----+5 V DC at 275 ma
5----CLLK

Of the six pins, we will only use four (4) of them. So what do we need? This will use an Arduino. and get this library.
Reference > Libraries > Ps2keyboard
This library is compatible with all architectures and boards.

image
image

Lib Code My Code

PS2Keyboard keyboard;
void setup() { delay(1000); keyboard.begin(DataPin, IRQpin);
Serial.begin(9600);
Serial.println("Keyboard Test:"); }
void loop() { if (keyboard.available()) { // read the next key char c = keyboard.read(); // check for some of the special keys
if (c == PS2_ENTER) { Serial.println(); }
else if (c == PS2_TAB) { Serial.print("[Tab]"); } else if (c == PS2_ESC) { Serial.print("[ESC]"); }
else if (c == PS2_PAGEDOWN) { Serial.print("[PgDn]"); }
else if (c == PS2_PAGEUP) { Serial.print("[PgUp]"); }
else if (c == PS2_LEFTARROW) { Serial.print("[Left]"); }
else if (c == PS2_RIGHTARROW) { Serial.print("[Right]"); }
else if (c == PS2_UPARROW) { Serial.print("[Up]"); }
else if (c == PS2_DOWNARROW) { Serial.print("[Down]"); }
else if (c == PS2_DELETE) { Serial.print("[Del]"); }
else { // otherwise, just print all normal characters Serial.print(c); } } }

#include const int DataPin = 8;
const int IRQpin = 5;

void setup() { delay(1000); keyboard.begin(DataPin, IRQpin);
Serial.begin(9600);
 }

keyboard()check for some of the special keys
switch (keycode)

case ENTER:{ doLine();}  // Send line to the processor.
break;
case CAPS: // USE AS ALPHA
default:{ // Keys that are not defined
}break;

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    I got rid of most of mine when I upgraded my computer.

    I now have everything on USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 2 years ago

    I got rid of most of mine when I upgraded my computer.

    I now have everything on USB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to DAB

     DAB Hope do didn't toss the real IBM XT/AT keyboard with interchangeable cable! it was the best keyboard ever made. Great finger feel and feedback! I may still have one downstairs in the garage. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago in reply to phoenixcomm

    Most of them were Dell keyboards, which were pretty good, but a guy was refurbishing old machines to get kids on the internet, so I gave them to him.

    I might have at least one of the IBM keyboards somewhere in my stash.

    I still have an original TEMPEST qualified IBM computer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to DAB

    cool, but when I lived in Pennington, between Princeton and Trenton. I was doing surplus, and I got a query if I wanted an old 360/50 well I said yes. and dragged it to where I lived, put on an OS, and then a Terminal Server (non-IBM) and sold time to students. the HD failed and that ended its life and I scraped it.