Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Howto: NFS (Network File System)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 30 Apr 2015 12:30 AM Date Created
  • Views 2985 views
  • Likes 1 like
  • Comments 15 comments
  • rpc
  • software_design
  • file_sharing
  • protocols
  • nfs
  • feature_tutorial
  • cifs
  • linux
Related
Recommended

Howto: NFS (Network File System)

phoenixcomm
phoenixcomm
30 Apr 2015

Ok what in the world of Microsoft and Windows and Linux is NFS and why do I need it... Really I'm very happy with SMB or CIFS,  or Samba (reversed engineered SMB) so why change to NFS??

  1. SMB is a kludge, its what you see is maybe what you get.
  2. and it really is not Open...
  3. CIFS is single threaded which makes it SLOW!
  4. and NFS just works, and it's dam fast!!

 

History:

NFS is a distributed file system protocol originally developed by Sun Microsystems in 1984, allowing a user on a client computer to access files over a network much like local storage is accessed. NFS, like many other protocols, builds on the Open Network Computing Remote Procedure Call (RPC) system. The Network File System is an open standard defined in RFCs, allowing anyone to implement the protocol.  There have been several versions with version 4 the latest.

 

My Network is comprised of several Linux Boxes on a 1 Gigabit Network (Player, Whirlwind, RSS), I also have a slower 100 Megabit Backbone which has my slower stuff (WiFi, network printers, etc.  I also have an additional 100 Megabit Network for NexGen my Simulator.  All of the Boxes are LinuxMint Ver 17r2. For this HowTo I will only concern ourselves with version 4.

 

How I Did It:

I am currently using Whirlwind as my desktop and file server.  There are a lot of Howto's out there and they all have there part but here is mine so here goes.

 

First I have to get NFS on my server.  You have you choice of using Synaptic or the terminal.. I will use and show you the terminal.

$ sudo apt-get install nfs-kernel-server nfs-common

Then edit your exports file. The follow 4 lines are my "exports", remember they will not be the same.

$ sudo vi /etc/exports

/mnt/MyData/public    192.168.1.1/24(rw,async,no_root_squash,subtree_check)

/mnt/MyMedia/Music  192.168.1.1/24(ro,async,no_root_squash,subtree_check)

/mnt/MyMedia/media  192.168.1.1/24(ro,async,no_root_squash,subtree_check)

/mnt/MyMedia/p2p      192.168.1.1/24(rw,async,no_root_squash,subtree_check)

 

so let explain my magic:

  • /mnt/......  Where my filesystem is mounted
  • 192.168.1.1/24  Who I want to share it with.. in this case I am sharing it with everybody hence the /24
  • ro or rw    Read Only or Read Write
  • async    allows the NFS server to violate the NFS protocol and reply to requests before any changes made by that request have been committed to stable storage (e.g. disc drive).
  • no_root_squash  Very often, it is not desirable that the root user on a client machine is also treated as root when accessing files on the NFS server. To this end, uid 0 is normally mapped to a different id: the so-called anonymous or nobody uid. This mode of operation (called 'root squashing') is the default, and can be turned off with no_root_squash.
  • subtree_check is also used to make sure that files inside directories to which only root has access can only be accessed if the filesystem is exported with no_root_squash even if the file itself allows more general access.

 

Now restart the NFS server

$ sudo service nfs-kernel-server start

 

You can test you service and exports by using this:

$ showmount -e

Export list for Whirlwind:

/mnt/MyData/public 192.168.1.1/24

/mnt/MyMedia/p2p  192.168.1.1/24

/mnt/MyMedia/media 192.168.1.1/24

/mnt/MyMedia/Music 192.168.1.1/24

 

Your Done!!

 

Now the Client.... (RSS)

install just the client.

$ sudo apt-get-install nfs-common  $ sudo apt-get install nfs-common

 

you can use showmount -e whirlwind on the client to show the servers exports but if you use name on your machines you must update your /etc/hosts file.... (good idea)

$ sudo /etc/hosts

192.168.1.23  Whirlwind

 

now try a mount command. I used my /mnt/  I added two directories under /mnt/ public and music. so here is what you need..

$ sudo mount -t nfs whirlwind:/mnt/MyData/public /mnt/public

now look in /mnt/public for your shares.. Got them. Good now one last thing.. Let make them mount when the machine starts.. cool

 

$ sudo vi /etc/fstab

Whirlwind:/mnt/MyData/public  /mnt/public

whirlwind:/mnt/MyMedia/Music /mnt/music

 

I think im done...

Cris H. image

PS 17JUNE2015 I made a small error! in the client machines you must add NFS to the fstab

>>>>>>>> Whirlwind:/mnt/MyData/Public     /mnt/public     NFS

 

PS 21OCT2016 I made a small error! in the line: $ sudo apt-get-install nfs-common

>>>>>>>   $ sudo apt-get install nfs-common

 

BTW if you want to mount your files on a local window 7 box, its not that hard Mount your NFS share on Windows 7

  • Sign in to reply

Top Comments

  • phoenixcomm
    phoenixcomm over 9 years ago in reply to shabaz +3
    Guys, shabaz Jan Cumps since you are both talking about the dark days... In 1977/8 or so I worked for Interdata in Oceanport. I helped deliver our 8/32 serial 1 to Bell Labs in Homedel. this was the first…
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to e14 Contributor +2
    In answer to my first question, the clients do not automatically reconnect. They seem to hang a bit. I had to re-mount my nfs shares once the NFS server was available after going out of service. This is…
  • phoenixcomm
    phoenixcomm over 9 years ago in reply to e14 Contributor +2
    texadactyl Richard nope I use mostly LinuxMint and Solaris on my Sun UltraSparc. I have one box that runs windows for Ventura Publisher (It has things in it like Page Setup, Frames {this is where you type…
Parents
  • e14 Contributor
    e14 Contributor over 9 years ago

    When your NFS server is rebooted, what affect does this have on the Linux client machines?  Do they automatically reconnect?

     

    Did you have any issues with access control?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to e14 Contributor

    In answer to my first question, the clients do not automatically reconnect.  They seem to hang a bit.  I had to re-mount my nfs shares once the NFS server was available after going out of service.

     

    This is no big deal to me and probably helps to keep the NFS client as simple as possible.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to e14 Contributor

    Hi Richard,

    I've noticed that if the NFS server is offline (e.g. accidentally powered off) and then the client is rebooted, the client hangs (I believe indefinitely) waiting for the NFS server to come up.

    I'd like it to attempt the mount for a period of time (say 30 seconds) and then abort and continue the Linux boot. According to here, there is a 'bg' switch which can help in this scenario, although I'm not sure it is will also apply in your scenario too. Maybe it is worth a try since it seems closely related.

    For my scenario I'm considering just using automount (autofs) because my NFS server is non-critical to the boot process and I'd rather only mount when required.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to shabaz

    shabaz  My remote NFS reference is for a family LAN file server so I do need it available on demand.  The only time that I get the hanging affect is when I reboot our LAN server following a kernel upgrade (infrequent).  I can live with that.  If I were running a small office or larger, then I would do more tuning. 

     

    Note that Samba recovers from outages much faster than NFS.  With respect to speed, I disagree with the author (phoenixcomm ) about Samba versus NFS performance, in general.  However, I think that the author is using Windows computers at home which might explain the slower SMB/NMB speeds.  I have benchmarked NFS versus Samba using 100% Linux machines and found both protocols to run roughly at LAN speed.

     

    I saw that the original post did not discuss the /etc/fstab type=nfs options such as bg and hard/soft so I'll assume that the author just took defaults - normally just fine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 9 years ago in reply to e14 Contributor

    texadactyl Richard nope I use mostly LinuxMint and Solaris on my Sun UltraSparc. I have one box that runs windows for Ventura Publisher (It has things in it like Page Setup, Frames {this is where you type}. My Indenting and bullets are alway right and guttering is a snap thanks to the Page Setup/Controls).  This is the Grand Daddy of desktop publishing. The only other thing that even comes close is Quark (which I can't stand). It started out as a Xerox product, and then was sold to Corel which just killed it off. Open Ofice writer is ok for a few pages, etc.  Sorry for rambling.

    About the speed difference between Linux/Unix and MS Windows XP or Win7. Both versions of Windows are not threaded, or Single Threaded, whereas Linux/Unix are Multi-Threaded, and therefore faster( which is a relative matter as speed counts:  CPU, network switches, etc ) as well as CPU load (what else is going on at the time.  I am running an AMD phenom II with 4 cores, (it's 5 or 6 years old.) it also holds my NFS shares (media/movies, media/music), Public. My network for my house, VOIP phones, lab are on multiple networks.

    • wifi1 printers, Laptop,  bedroom TV+Kodibuntu
    • wifi2 phones { in progress RasberryPi with Asterisk }
    • Lan1 100Mb:  wifi1 WRT54G  { in progress Home automation system } using a ZigBee network.
    • Lan2 100Mb:  wifi2 WRT54G (phones only)
    • Lan2 1Gb backbone: Cisco 3500XL in the Office, living room TV+Kodibuntu, Lab
    • Lan3 100Mb: WRT54G  Aircraft private bus.

     

    BTW I also renamed /home to /_home and add a link to /export/home/ with this stunt when you install the new OS your home directors are still there like nothing happened (Thunderbird does not know or care) yes you will have to reload some libs, and programs. but its better than a forklift upgrade. LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 9 years ago in reply to e14 Contributor

    texadactyl Richard nope I use mostly LinuxMint and Solaris on my Sun UltraSparc. I have one box that runs windows for Ventura Publisher (It has things in it like Page Setup, Frames {this is where you type}. My Indenting and bullets are alway right and guttering is a snap thanks to the Page Setup/Controls).  This is the Grand Daddy of desktop publishing. The only other thing that even comes close is Quark (which I can't stand). It started out as a Xerox product, and then was sold to Corel which just killed it off. Open Ofice writer is ok for a few pages, etc.  Sorry for rambling.

    About the speed difference between Linux/Unix and MS Windows XP or Win7. Both versions of Windows are not threaded, or Single Threaded, whereas Linux/Unix are Multi-Threaded, and therefore faster( which is a relative matter as speed counts:  CPU, network switches, etc ) as well as CPU load (what else is going on at the time.  I am running an AMD phenom II with 4 cores, (it's 5 or 6 years old.) it also holds my NFS shares (media/movies, media/music), Public. My network for my house, VOIP phones, lab are on multiple networks.

    • wifi1 printers, Laptop,  bedroom TV+Kodibuntu
    • wifi2 phones { in progress RasberryPi with Asterisk }
    • Lan1 100Mb:  wifi1 WRT54G  { in progress Home automation system } using a ZigBee network.
    • Lan2 100Mb:  wifi2 WRT54G (phones only)
    • Lan2 1Gb backbone: Cisco 3500XL in the Office, living room TV+Kodibuntu, Lab
    • Lan3 100Mb: WRT54G  Aircraft private bus.

     

    BTW I also renamed /home to /_home and add a link to /export/home/ with this stunt when you install the new OS your home directors are still there like nothing happened (Thunderbird does not know or care) yes you will have to reload some libs, and programs. but its better than a forklift upgrade. LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to phoenixcomm

    I was mostly reacting to the 4 points in your original post which did not specify which computer OS was slow or single-threaded.  I don't have any Windows products in my home so I wouldn't be able to judge.

     

    Wow, you have a lot of equipment in your home.  I'll never feel bad about buying more techie toys again!  (=:

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 9 years ago in reply to phoenixcomm

    Hehe I do the same trick with /export/home since Solaris days too : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to phoenixcomm

    Aw, Solaris.  My first real unix experience was on Oracle Applications running on Solaris.

    that's where I learned writing shell scripts. A skill that has very much faded away by now...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 9 years ago in reply to shabaz

    Guys, shabaz Jan Cumps since you are both talking about the dark days... In 1977/8 or so I worked for Interdata in Oceanport. I helped deliver our 8/32 serial 1 to Bell Labs in Homedel. this was the first non-DEC port of UNIX. I have had my hand in it ever since. I will never understand the LINUX distros. why in the hell do they put things in /var that should never be, like parts of the your web server pagers.. /var should be only for your logs! The best DOS attack is to just ask a web server for just one small bit of info. This transaction is recorded  in /var/logs/www/<name>{error.log & transfer.log} when this gets full, that is to say, that volume, your system has no more space and just dies.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 9 years ago in reply to phoenixcomm

    phoenixcomm What goes where is configurable E.g. which folder to peg/store configuration, logs, other stuff.  From the "www" reference, I'll assume that you are talking about the Apache or Tomcat web/app server(s).  Easy to avoid cluttering up /var.  Secondly, with a symbolic link for any folder, you can point anywhere else (E.g. /opt or a USB drive). Also, /var itself can be mounted anywhere (E.g. under /opt or on a USB drive).  Commercial Apache admins always make these kinds of changes to match the available physical storage.

     

    By the way, are you aging your Apache logs?  See https://www.loggly.com/ultimate-guide/apache-logging-basics/