Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Nexgen: CANaerospace: RSS: C-3436A Radio: Build ii
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 26 Aug 2021 10:57 PM Date Created
  • Views 1413 views
  • Likes 5 likes
  • Comments 5 comments
  • offtheshelfch
  • flight simulator
  • nexgen
  • arduino mega 2560
  • rss
  • c-3436a radio set
  • canaerospace
Related
Recommended

Nexgen: CANaerospace: RSS: C-3436A Radio: Build ii

phoenixcomm
phoenixcomm
26 Aug 2021

image

Well, here I am again, what is this the third time? I last took this up in the blog Nexgen: CANaerospace: RSS: C-3436A Radio: Build i. So this is part II of the build, covering the hardware, 2x RS232 cutouts, securing the CAN interface, as well as the relay for the panel lights. I will also wire the DIN-5 power connector to the rear of the unit.

Also, please note below the new wiring guide!

After that, I will have to test the Radio Head with the Slave. The output frequency will be converted into two 4-bytes with an additional two bits in the LSB for power and lights. , so I have to get creative on how to compose the message: 

 

mnemonic P1 pin J1 pin Arduino
n/a A 1
n/a B 14
n/a C 2
n/a D 15
n/a E 3
SQL F 16 A0
n/a G 4
MC5 H 17 22
MC4 I 5 23
MC3 J 18 24
MC2 K 6 25
MC1 L 19 26
n/a M 7 n/a
FRAC1 N 20 27
FRAC2 Q 8 28
FRAC3 P 21 29
FRAC4 O 9 30
FRAC5 R 22 31
GND S

10

23

Arduino
LV P2 A J2 2 Arduino
VOL B 15 A1
LMP C 33
GND D Arduino
COMM E Arduino
PWR F 3 Arduino
G Arduino
H Arduino
P3 Unused
SPI to CANbus
newmoic Arduino CANmod
MISO 50 SO
MOSI 51 SI
SCLK 52 SCLK
SS 53 CS
INT2 21 INT

 

0 1 2 3 4 5 6 7
High Hex Low Hex
Power Jack Wiring
PIN VOLTAGE
1 +5vdc
2 N/A
3 GND
4 +12vdc
5 +24vdc


image

  • Sign in to reply

Top Comments

  • colporteur
    colporteur over 5 years ago +1
    Do you have any side profile pic of your micro in a tub? Looks like some pretty elaborate holes to accommodate electronics.
Parents
  • colporteur
    colporteur over 5 years ago

    Do you have any side profile pic of your micro in a tub? Looks like some pretty elaborate holes to accommodate electronics.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • colporteur
    colporteur over 5 years ago

    Do you have any side profile pic of your micro in a tub? Looks like some pretty elaborate holes to accommodate electronics.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to colporteur

    The hole between DIN-5 and DB25 boo-boo

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to colporteur

    colporteur

    1image2image3image4image

    BTW The 5x small holes on the front and the back come with the box, little cooling. LOL

    and I use Gorilla Glue (instant gel) for securing the PCB to the case The white rails are from HO supplies. I use them to reinforce the jacks.

    ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 5 years ago in reply to phoenixcomm

    I thought I was the only person to kludge plastic boxes into viable housings for electronic gear. Nice job.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 5 years ago in reply to colporteur

    colporteur he'll no long time.  BTW these are shoe boxes from container store and less than 5$

    ~~Cris