Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen Flight Simulator: Hacking the Navigation Computer Display: Internal Cabling
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 20 Oct 2018 3:03 AM Date Created
  • Views 237 views
  • Likes 3 likes
  • Comments 0 comments
  • cp-1252/asn-128
  • diy cockpit
  • diy electronics
  • display interconnections
  • nexgen flight simulator
Related
Recommended

NexGen Flight Simulator: Hacking the Navigation Computer Display: Internal Cabling

phoenixcomm
phoenixcomm
20 Oct 2018

Well, this was a mess, and I blame it on myself. In my rush to work on the box, I disconnected all the plugs, I just wanted them out of my way. No, I did not cut them nor did I record what was hooked to what and where.  So I had to do this one on my own.image

On the back of the unit, there are five 50-pin male receptacles, which are 10 x 10 easy. The Jacks are labeled J1 through J5 and have cables attached to them. The other end of the cables has a 34-pin male header. One is pin 1 to pin 34, while the Other is pin 35 to pin 68. Onto these headers, you have female headers of assorted sizes. Below is two tables that show the interconnections. The first table is to show the interconnections between the Jacks on the rear to there destination (From - To). The second table is pretty much bare as I have started to figure out the interconnections between the displays and the Jack field.

The plan is to build a backboard with 5 headers on it, with two Arduinos Megas there will be an ethernet shield to send data to the NavIOSS (IOSS I/O Subsystem. I will use I2C to send information between them.

JPWPins

Display

Jack

TOComment
J1
P1

1 through 34

W6P1

1-9

NAAlpha  DisplayDS1
W6P210-17NAAlpha  DisplayDS2
W6P318-26NAAlpha DisplayDS3
W6P437-34NAAlpha DisplayDS4
P235 through 68
W6P535-42NAAlpha  DisplayDS1
W6P643-51NAAlpha  DisplayDS2
J2
P233 through 68
W6P752-59NAAlpha  DisplayDS3
W6P860-67NAAlpha  DisplayDS4
J3
P2
W6P8pin 687 Segment Display
P333 through 68
W7P333-467 Segment Display
W7P447-647 Segment Display
J3
P4
W7P11-147 Segment Display
W7P215-327 Segment Display
P51 through 24
W7P51-137 Segment Display
W7P614-267 Segment Display
J4
P627 through 52
W7P727-397 Segment Display
W7P840-527 Segment Display
P71 through 20
P81 through 20
J5
P81 through 20
P91 through 20
W5P912-20Header 41Mode SwitchHeader 42
W5P31-7Display Switch
W5P61-3Dimmer?
W5P74-6LEDs
W5P87-11Relay
W7P101-9
W5P514-20Thumbwheel Switch
W5P216-20Thumbwheel Switch
PINJ3J3J3J4J5
ULULULULUL
1-35
2-36
3-37
4-38
5-39
6-40
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34

These tables will be updated as new information becomes available.

C Harrison