Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen Flight Simulator: Power System Basics
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 15 May 2014 10:16 PM Date Created
  • Views 567 views
  • Likes 0 likes
  • Comments 2 comments
  • charging
  • nexgen
  • batteries
  • power-system
  • aircraft
  • hardware
  • nexgen_flight_simulator
  • safety-of-flight
  • diy_cockpit
Related
Recommended

NexGen Flight Simulator: Power System Basics

phoenixcomm
phoenixcomm
15 May 2014

Ouch... Where do I start.. Questions:

  1. How many power plants? ie Engines, APU, RAT, etc.
  2. Is you system going to be AC or DC based?
  3. What will be the prime voltage? 12, 24, or 48 volts
  4. Is there a ground power port? (makes life easy)
  5. etc...

image

Well here is a overview of my airplane. You will notice that it is a twin. There are two alternators, and starters. You see  my alternators have had the diodes ripped out of them so the unit produces AC at 400Hz which is accomplished by applying a 400Hz sine wave on the Alternator Exciter. By engaging the ALT1 or ALT2 contact or we can turn on the DC rectifier.

When the two alternators are out putting at same voltage and phase we can turn on the TIE RELAY so that each alternators can split the load.  The AC TIE RELAY is used for isolation. That is if you have a alternator failure. The failed alternator can be isolated and its load can be support via the other alternator. (author CAH 17MAY2014)
There is also two other contactors one controls the EXTERNAL POWER  the other is the battery disconnect.

In this way you can't discharge your battery via the EXTERNAL POWER JACK.  The two Master Switches on the panel are a SPDT (Single Pole, Double Throw) with center off. So if both switches are in the EXTernal positions the 24vdc sense line is on only when the generator (external power) is on, which energizes the GROUND POWER RELAY, which in turn puts 24vdc on the BATTERY BUS.

So when you have the switches in GEN postilions, the alternator, is spinning happily, there is voltage on the BATTERY BUS from the DC rectifiers, controlling the battery when charging in flight or on the ramp.

 

 

image  Tune in later, more to come!

~~Cris

 

BTW

  • What this diagram does not make clear is that both DC Rectifiers are attached to the Battery Charging Circuits via a diode so that you can not back feed the battery or the Chargers themselves.
  • Also not shown is the DC BUSS TIE RELAY which ties both out puts together
  • Also not shown is the BATTERY DC BUS TIE RELAY
  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +1
    Are you going to include the start up whine for the engines? I still remember watching Sky King as he powered up is airplane every episode. The sound is ingrained on my memory. DAB
Parents
  • DAB
    DAB over 12 years ago

    Are you going to include the start up whine for the engines?

    I still remember watching Sky King as he powered up is airplane every episode.

    The sound is ingrained on my memory.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Are you going to include the start up whine for the engines?

    I still remember watching Sky King as he powered up is airplane every episode.

    The sound is ingrained on my memory.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 12 years ago in reply to DAB

    not even close to that.. But YUP! So you liked Sky King on the tube (I miss it) it had big radials....

    but im using 2 Ford Torus  3.0L engines and since this is a canard its very quiet. but with the pipes you will get a good sound ie.. Like a car starting...LOL

    hey im downloading the first 4 episodes when I get I will put them up on my server if you wish..

    ~ Cris