Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Getting the lab working: New Drill Press
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 29 Apr 2018 1:52 AM Date Created
  • Views 1322 views
  • Likes 10 likes
  • Comments 14 comments
  • nexgen
  • diy cockpit
  • drill press
  • instrument cutout templete
  • xy stage
Related
Recommended

NexGen: Getting the lab working: New Drill Press

phoenixcomm
phoenixcomm
29 Apr 2018

This is a necessary evil of any lab, workshop. I have needed one for quite awhile. When I moved from New Jersey to in 1979 I left my floor unit with my bother. Imported yes, but well done, and morse taper removable chuck. So the other day Harbor Freight was having a Black something Sale and with the coupons and what not I pick this one up for about 40 bucks.
imageimage

Major Components

  1. Drill motor unit

  2. Drill Plate

  3. Base

  4. Column

I did not really expect much. I opened the box, nothing missing. (that's a good sign). First problem: They give you 3 bolts, washers, and split washers to hold the column to the base. This was a good time to try out Loctite # 243 medium strength goo. But PROBLEMS:

  1. there are 3 tapped holes in the drill base. You Will Need a thread, Chase.
  2. The lamp is a POS that's right pure crap. It will have to go and  LED one should replace it.

Other than that hiccup it when together very nicely. While getting ready to put the cuck in place. I found out that the chuck has a tapper (JT33) and just presses on.

imageimage

TESTING:

I will have to get a dial indicator to see the run-out. But it seems to be fairly accurate, and I can not see any substantial run-out.

You will notice that I still have the protective plastic bags over the parts.  (Did you ever cut plastics?)

 

Wish List:

  • Rack Lift for Drill Plate!
  • See problem #2!

 

~~ Cris H. image

 


Back to the Index III
image

Updates:

1. (May 3, 2018) Could use an "X & Y" table, controlled by an Arduino, and web interface could even use G-Code. As drilling 5 holes for instrument mounts is a pain - in - duh - ass! No Boo Boos!!

  • Sign in to reply

Top Comments

  • mcb1
    mcb1 over 8 years ago +3
    Ah I can add comments now. .. Nice price for the Drill Press. I'm thinking mine needs to have a light attached again. The last one vibrated and broke the stupid plastic that it was attached with, and a…
  • rsc
    rsc over 8 years ago +2
    You’re going to need a good wide machinists vice next. I spent more on my vise than on my drill press. Scott
  • genebren
    genebren over 8 years ago +2
    Not bad for the price. I have an old Craftsman drill that looks like the original that this was cloned from. Mine has been in use for more than 30 years. You can never have too many tools, unless you run…
Parents
  • mcb1
    mcb1 over 8 years ago

    Ah I can add comments now. ..

     

    Nice price for the Drill Press.

    I'm thinking mine needs to have a light attached again. The last one vibrated and broke the stupid plastic that it was attached with, and a LED sounds like just the answer.

     

    I like the switch position.

    Too many are on the side and need you to turn and look.

     

     

    I might need to buy one of these.

    https://www.machineryhouse.co.nz/D199

    I'm just looking if they have a distributor a bit closer ...

     

     

    You'll like this one.

    I got to see the prototype and it certainly is different.

    https://www.carbatec.co.nz/product/6312-voyager-dvr-drill-press

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to mcb1

    that center plate is cool but I cant mount it to my table. and well $$$$2K for a press.. with a direct drive well its different.  bet you, we could get rid of the pulleys too. It just one more project that I don't have to do now.. LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 8 years ago in reply to phoenixcomm

    Famous Toyota advert saying here "Bugger".

     

    I've looked at the link and my hand is itching over the credit card for the drill press and plate, plus they have some other cool stuff .....

    Yes the direct drive is a fantastic looking drill and capable of so much, but not something I need either.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 8 years ago in reply to phoenixcomm

    Famous Toyota advert saying here "Bugger".

     

    I've looked at the link and my hand is itching over the credit card for the drill press and plate, plus they have some other cool stuff .....

    Yes the direct drive is a fantastic looking drill and capable of so much, but not something I need either.

     

    Mark