Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Hacking; Gray 2 BCD Encoder (using TTL)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 2 Nov 2022 5:27 PM Date Created
  • Views 1827 views
  • Likes 5 likes
  • Comments 8 comments
  • flight simulator
  • nexgen
  • diy hardware
  • diy cockpit
  • mcp23017
  • 74LS7400
  • 74LS148
  • 74LS08
  • ttl logic
  • Gray Code
  • BCD Code
Related
Recommended

NexGen: Hacking; Gray 2 BCD Encoder (using TTL)

phoenixcomm
phoenixcomm
2 Nov 2022

imageOK, I Have had it up to you know where with the GRAY CODE!! When I have written this decoder in software, it takes a loop or two, It just eats CPU time. This is ok if you can use interrupts. But the Ardunio does not return the interrupt value to you directly. No, it uses what is called a SIDE-EFFECT! Incredibly, this means you have to look for the interrupt number. This is from the Arduino website itself: "ISRs are special kinds of functions that have some unique limitations most other functions do not have. An ISR cannot have any parameters, and they shouldn't return anything." This is not correct, in fact, the return type must be a VOID.  So I have crawled back to my hardware days and came up with this: (diagram below). Now I can take the decoded BCD and apply it to an MCP23017. Now I have two choices waste a nibble (4-bits) which will handle 2 decoders or 4 decoders but I will have to do some bit shifting.  - CAH Nov 2, 2K22

image

Part Price Count Price
SN74LS00N 0.12 3 0.36
SN74LS08N 0.98 1 0.98
SN74LS148N 2.05 2 4.10
TOTAL 5.44

Prices are from Newark Electronics
(web pricing)

2 of 5 Gray Code BCD
INPUTS OUTPUTS
A B C D E D C B A
0 X X 0 0 0 0
1 X X 0 0 0 1
2 X X 0 0 1 0
3 X X 0 0 1 1
4 X X 0 1 0 0
5 X X 0 1 0 1
6 X X 0 1 1 0
7 X X 0 1 1 1
8 1 0 0 0
9 X X 1 0 0 1
  • Sign in to reply
Parents
  • dougw
    dougw over 3 years ago

    If you do the lookup in your MCU instead of an external memory there is no problem with jitter.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to dougw

    I don't waste the CPU for this.  most of the time its just MHZ and KHZ, in one radio I have 5 groups..:(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to dougw

    I don't waste the CPU for this.  most of the time its just MHZ and KHZ, in one radio I have 5 groups..:(