Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Hacking: Loadmeter, Dual, Weston 248697
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 21 Mar 2023 9:49 PM Date Created
  • Views 459 views
  • Likes 6 likes
  • Comments 0 comments
  • flight simulator
  • nexgen
  • diy cockpit
  • arduino mega 2560
  • 248697
  • hardware
  • dual
  • weston
  • software_design
  • Loadmeter
  • software
Related
Recommended

NexGen: Hacking: Loadmeter, Dual, Weston 248697

phoenixcomm
phoenixcomm
21 Mar 2023
image
image

The Analysis: The Loadmeter is divided into 3 parts. Parts 1 and 2 are identical and are the meters. Part 3 is the lighting equipment. Let's talk about the meter for a minute.  The meter is most likely a D'Arsonval movement. . It consists of a movable coil placed within the field of a permanent magnet. image The Image on the left is from instrumentationtools.com/darsonval-movement/# So basically it is a little motor. That is the spring(s) hold the meter to 0 and when a voltage is applied to the coil, the meter is deflected. 
Now the meter scale is 0 to 1.5 in 15 ticks, so I have to come up with 15 values (resistors) essentially a voltage divider, but I think I will do it a little easier, and here's how. First I find the voltage to go to full scale with my adjustable power supply. I must pick a resistor value to set the full-scale defection from the Arduino's analog write. for this I will only use A(+) and B(-) connections to the meter. Remember I only have to do this for one meter, not both, as I will replicate the solution on the other side as well.
My Power Supply's output at 0 Vdc bounces the meter around, so this tack is a bust. Since the maximum voltage on the Arduino Mega's analogWrite() is 5 Vdc. I will use the map() function to control the voltage to the meter via the analogWrite(pin1, meter1) command where pin1 and meter1 are defined. So here is my codebase:

#define meter1
#define meter2
#define pin1 8
#define pin2 9

// CONSTANTS
#define 3// CONSTANTS0sec 30000;
#define inMin 0;
#define inMax 255;
#define outMin 0;
#define outMax 100;

void setup() {
Serial.begin (9600);}

void loop() {
for (inputVal = 0; inputValue < 256; inputValue++ ) {
delay( 30sec );
meter1 = map( inputVal, inMin, inMax, outMin, outMax);
analogWrite( pin1, meter1);

Serial.print( "Map Value = ");
Serial.println( meter1 );
}}
image

Later: