Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Hacking:  Panel Lighting Control - (5956888-503)
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 29 Sep 2018 6:09 PM Date Created
  • Views 449 views
  • Likes 3 likes
  • Comments 0 comments
  • nexgen
  • diy cockpit
  • lighting controls
  • dc-9
  • 5956888-503
  • diy electronics
  • nexgen flight simulator
Related
Recommended

NexGen: Hacking:  Panel Lighting Control - (5956888-503)

phoenixcomm
phoenixcomm
29 Sep 2018

This panel was used on McDonnell Douglas DC-9. It was placed on the Upper left-hand side of the Forward Control Pedestal. If you wish to see it click here. Then click on the picture and it is item 1 in the photo.imageimage

Lucky the analysis will be very quick, as the schematic is on the units bottom plate. So the Analysis: Panel inner and outer control are both 10 position rotary switches. The Red Control is an 8 position rotary switch coupled to a transformer. The Third Control is marked White, and are connected with a double gang wire wound potentiometers.

Plan: Most of my lights are: 28v, 12v, and 5vdc for LEDs. So I have included the following table to help. The connector is a Burndy DC22E20-41P. Its mate should be a  Burndy DC26F20-41S. I have included a partial pinout diagram below#Connector. Please see the Component Description Page here.

PINnumberDescriptionWhat goes where
b28Panel Lamp - Ground Bound
D27Panel Light V-
C26Panel Light V+
G25VCC R1+12vdc Bus
H24VCC R2+28vdc Bus
J23Wiper R228vdc Lighting Bus
c22Wiper R112vdc Lighting Bus

I will run 28vdc (H) from the 28vdc buss through R2 and out the wiper via (J) and to the 28vdc lighting Bus. I will do the same for the 12vdc buss as well.
I will have to open up the controller and remove the knobs and panel to see what the requirement is.
(a few hours later)Well, I opened it up (you can see the pretty pictures), and found the light panel. And it is a 5vdc led panel made by Spectrlux part number 9915674-505. A quick call to them should let me know if I need to limit the current or not.
(next day) Wow, after playing telephone tag yesterday, I am no better off. When you call them you get a machine and NOBODY ever picks up. (I need a plan here). Late in the day I got a call from Spectralux and assured me that the panel has small light bulbs. Onwards and Upwards!

imageimageimage
image 1
The Guts
image 2
Back of the Light Panel
image 3
Rear Connector
imageimage
image 4
DC-9 Cockpit Panel is outlined in Red.

image 5
Proposed Schematic