Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Hacking the Fuel Load Indicator III - Hardware Design
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 26 Aug 2018 8:12 AM Date Created
  • Views 498 views
  • Likes 2 likes
  • Comments 0 comments
  • diy cockpit
  • hardware plan
  • software overview
  • fuel load indicator
  • nexgen flight simulator
  • hacking
Related
Recommended

NexGen: Hacking the Fuel Load Indicator III - Hardware Design

phoenixcomm
phoenixcomm
26 Aug 2018

I have talked about the Fuel load Indicator twice before, first here and then here. So here is the hardware design and its analysis.image

Analysis:  In my last blog I noted that between the display and the switches I am using about 25 pins + ground and power. So to recap here are the pins: I have added a second table which shows the I/O connections. The reason that I chose the STM32 was for its size. It can easily fit inside the enclosure (approximately 7cm square).

The Plan:

The Hardware: Since the original back will be of no use to me I will have to print a new one. I will have two connectors on the rear. 1) a DB-7 for my CANbus Data and  2) a DIN 5 for my 5 volts. I will have to use UTA, the University of Texas at Arlington, Maker Space Laser Cutter to cut my vector board (FR4 PCB) to shape. In this way,  I can put my connect the STM32xx and the two  (2) TI PCF8574 I/O expanders.

The Software Overview: The software design is rather simple as the STM32 is just being used as a dumb terminal but without the keyboard This will only need 4 keys And instead of a UART and  RS-232RS-232 I will be using a CANbus transceiver

Display Info
Mnemonic J1 pins IO Exp STM32
D6 1 IC1-11
D4 2 IC1-9
GND display 3
GND logic 4
D0 5 IC1-4
D5 6 IC1-10
D3 7 IC1-7
D1 8 IC1-5
A1 9 IC2-5
D2 10 IC1-6
A0 11 IC2-4
A2 12 IC2-6
FL - Not Used 13
CLS.1 14 10
CLS.2 15 11
WR 16

 

12
CE.2 17 13
RD.2 - Not Used 18
RD.1 - Not Used 19
CE.1 20 14
D7.2 22
CLK.2 21 15
CLK.1 23 16
D7.1 24 IC1-12
RST.1 25 17
RST.2 26 29
A3 & A4 27 IC2-9
Vcc 28
A3 & A4 29 IC2-7
Vcc 30

 

I/O Interfaces
Mnemonic STM32 Header
USB-
USB+
CanRX 45
CanTX 46
SDA2 22
SCL2 21
Switches
Test-C 3
FILL 39 4
TEST 40 5
Set-C 3
Set-UP 41 1
Set-DOWN 42 2
Keep Tuned In, More To Come   ~~Cris  image
Back to the Main Index
image
REVISIONS: