Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen RSS: Hacking the Gables G-1981 ATC Panel
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 19 Oct 2019 12:44 PM Date Created
  • Views 356 views
  • Likes 2 likes
  • Comments 0 comments
  • diy cockpit
  • arduino mega 2560
  • octal encoded decimal
  • nexgen flight simulator
  • arduino mega
  • software
Related
Recommended

NexGen RSS: Hacking the Gables G-1981 ATC Panel

phoenixcomm
phoenixcomm
19 Oct 2019

Well, here we are back at the ATC panel. The ATC panel function is to identify your aircraft to the tower via secondary radar. After a quick call to Gables Engineering in Florida. I explained what I needed and why they graciously sent me a print with the connector and schematic to me. The table below is indexed by functionality not pin numbers.imageimage

 

 

 

The connector on the rear of the panel is:

ZZB-AC-1722-5522-55P

 

BTW:

I had to rout around inside to see what was going on with some of the switches, so for all of you that like to see blood and guts, I have included an interior shot showing the switch mechanism.  image

 

PIN Connects To: Terminal: FUNCTION db25 ARDUINO MEGA
SQUAWK CODES
2 S1A B POS 3xx A1 22
3 S1A C A2 23
4 S1A D A3 24
5 S1 E POS 4xxx A4 25
6 S1B F A5 26
7 S1B G A6 27
9 S2A N POS 2x A7 28
10 S2A O A8 29
11 S2A P A9 30
13 S2B J POS 1 (units) 10 31
14 S2B K A11 32
15 S2B L A12 33
TRANSPONDER #1
16 S8A IDENT A13 34
21 S5 LO SENS A14 35
22 S3 STBY A15 36
23 S3 ON A16 37
24 S4 MODE A A17 38
25 S4 MODE B A18 39
26 S4 MODE D A19 40
19 TEST A20 41
43 S5 ANN.  LIGHT A21 42
TRANSPONDER #2
18 IDENT B1 43
32 LOW SENS B2 44
33 S3 STBY B3 45
34 ON B4 46
28 S4 MODE A B5 47
29 S4 MODE B B6 48
30 S4 MODE D B7 49
42 TEST B14 50
44 ANN. LIGHT B115 51
ALTITUDE REPORTING SW
GND S6 AC+BC B16 na
1 S6 ALT REPORT B17
45 S6 A1 COMPUTER 1 B18 52
46 S6 A 2 COMPUTER 2 B19 53
LIGHTS
38 PANEL LAMPS B11 Relay #1 1NO
39 PANEL LAMPS B23 Power Supply Ground
41 DIAL LIGHTS B21 Relay #2 NO
40 DIAL LIGHTS B9 Power Supply Ground
CHASSIS GROUNDS
8 B13
17 B25
SPARE PINS (NOT USED)
20, 27, 31, 35, 47, 48, 49, 50 51, 52, 53, 54, 55

Since I am using all most every digital I/O pin on the Arduino just for the ATC panel, I have to get creative. I have to deal with 4 more digital pins for the slaves' address plus COM 1 only used with the USB serial, and COM2 which handles RS-485 Full-Duplex (8bits) Traffic over RS-232.

Since I only have to read the Address Nible on startup, I can do this on startup.

There are two main loops.

1 loop is for the incoming messages and you must decide if it is for you.

Yes: parse the command and do it.

No: get the next buss message.

2 loop checks for changes on any of the switch states

Yes: update the value and send it to the controller.

No: Go back to sleep.

 

Message Formats

Send  to A Slave from the Controller

Start Byte Address Byte Command Byte Payload End Byte

 

Send to the Controller from a Slave

Start Byte Address Byte Command Byte Payload End Byte

 

Notes:

  • Payload Field can be of any length
  • There might be times where you might have two addresses in the Address Byte such as 54 where 5 is the target (another Slave), and 4 is the Slave Sending the info.
  • The SQUAWK Codes are a group of four (4) digits indicating from zero (0) to eight (8) but there are only three wires, ie S1A.B, S1A.C, S1AD. This leads me to think that they have used Octal encoding.
Decimal Code Octal Code
MSB LSB
0
1
2
3
4
5
6
7
8

 

Keep tuned in, More to come Sunglasses

UPDATE 8-25-22 -- I have removed the binary codes in the above table as there are 9 digits.