Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Rudder Pedals .ii Boeing 737 Overhaul
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 15 Oct 2019 4:26 AM Date Created
  • Views 1934 views
  • Likes 2 likes
  • Comments 2 comments
  • rudder pedals
  • b-737
  • boeing
  • nexgen flight simulator
Related
Recommended

NexGen: Rudder Pedals .ii Boeing 737 Overhaul

phoenixcomm
phoenixcomm
15 Oct 2019
image
image
image

Ok, you all know if you are keeping up, I scored a pair of B-737 rudder pedals on eBay for about 200 bucks. So the first thing I have to do is take the pedals apart and clean them. The parts diagrams and part numbers come from the Boeing 300/400/500 IPC (Illustrated Parts Catalog),
section 27-21-00-36 page 0.

Analysis / Plan

  • Rudder Pedals

As you can see from the picture the rudder pedal tubes have been cut off, and the attachment point by the pedal's receiver which is drilled through for the peddle, also there are four (4) rivets per pedal two per side, which will have to be removed and then replaced when the new tube's OD has been reduced on a lathe, and to really complicate this the through-hole is ~1.48" and electrical EMT conduit size is 1.25" which has a nominal OD of 1.51" with a .065 wall thickness. In real life, this tube is a swedge tube, but since this is priced as unobtainium I will fake it by printing the swedge (neck) then side a larger piece of EMT over the assembly.

The lower supports on the tubes will be standard 1.25" EMT, as this will simplify life.

  • Toe Brakes

The Toe Brakes are actuated by pressing the top of the pedal forward or down with your toes. On the pedal is the brake arm with a rod end. Unfortunately, the lever arm at the base is missing and will have to be printed as well. The brake shaft can be just a threaded rod.

  • Rudder Self Centering

Rudder Self Centering will be accomplished via two air cylinders. Piping is Front to Front and Back to Back, with springs on the shafts to help in Rudder centering.

  • Toe Brakes

Toe Brakes will use small dampers from the automotive world. This should give the required resistance. 

  • Sign in to reply
Parents
  • colporteur
    colporteur over 7 years ago

    What is your ultimate goal, if you were to put the pedal to the metal?

    OOOh so bad!

     

    Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to colporteur

    colporteur  Please describe "put the pedal to the metal" if you mean to the limits the 1.5" EMT over 20" should not bend? And you can only go so far until you hit the stops. Remember the tubes that were cut off go to the lower mount. Towards the botton of the tube you will see a tie rod end at 90 deg from the tube this goes to you yoke that both arms are connected to and a potentiometer mounted on the vertical axis. 

    Now getting back to the dam tubes I could possibly ream out the 1.48 hole to accept standard EMT. This could be accomplished with lathe and a 4 jaw chuck and a dial indicator. The first method is a LOT less work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 7 years ago in reply to colporteur

    colporteur  Please describe "put the pedal to the metal" if you mean to the limits the 1.5" EMT over 20" should not bend? And you can only go so far until you hit the stops. Remember the tubes that were cut off go to the lower mount. Towards the botton of the tube you will see a tie rod end at 90 deg from the tube this goes to you yoke that both arms are connected to and a potentiometer mounted on the vertical axis. 

    Now getting back to the dam tubes I could possibly ream out the 1.48 hole to accept standard EMT. This could be accomplished with lathe and a 4 jaw chuck and a dial indicator. The first method is a LOT less work.