Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: Rudder Pedals
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 31 Jul 2015 11:01 PM Date Created
  • Views 2230 views
  • Likes 3 likes
  • Comments 7 comments
  • nexgen
  • rudder_pedals
  • crosswind
  • ch
  • flight_simulation
  • diy
  • thrustmaster
  • diy_cockpit
Related
Recommended

NexGen: Rudder Pedals

phoenixcomm
phoenixcomm
31 Jul 2015

Well, you know you need rudder pedals to perform coordinated turns, and differential braking. I used to have this solved with a  Thrustmaster  RCS (Figure 1), But in moving etc they got strayed, misplaced or stolen. Sometime in 2011 I came across this hot mess (Figure 2) using two (2) air cylinders cross plumbed, ensures device centered.

imageimageimageimage

Thrustmaster RCS

Figure 1

A good idea, bad implementation.

Figure 2

CH pedals

Figure 3

CH pedal internal

Figure 4

Athough the pedals are fixed (not good) the idea is brilliant. The other day while scrounging around at a local Goodwill store, I came up with a set of CH Products pedals (Figure 3). So here is the plan...

  THE ANALYSIS:  >The end unit should look somewhat like figure 1. That is one bar anchored in the center on a pivot. This has a mounting plate on either end mounted with a pivot. then the top can just be a rod that is also mounted on the plates and has a center pivot as well. This gives us the movement that we require for aircraft pedals.The CH pedals will be affixed to plates so the end results resembles Figure 1. The CH pedals cable only has 4 wires and will have to be replaced by a standard DB-25 cable that I have laying around. The unit will need 3 axis, two for brakes (one each pedal) and a center for the rudder

imageimage

Close Up of the Mount

Figure 5

Crosswind pedals

Figure 6

If you look at figure 4 you will see the pedal sits on a post coming up through from the base the pedal pivots on the white arm. This could be replaced with a hunk of DelrinRegistered plastic or some soft brass.  The two pivot points are a pair of sealed bearings. Figure 6 is a picture of the new kid on the block.

8/1/2015 In response to mcb1. Figures 7 and 8 are the real things from a Beechcraft. You will notice that each pedal is attached to a bar with an arm. You will also notice the brake cylinder mounted to pedal as well. this is for differential breaking. In Figure 9 you can clearly see them with the guts out of the way.  You now can see clearly the yellow actuator arms. These would be connected to a clevis on the tail. So you now can use one pot or two. Now this is where you could mount the two air cylinders, connected to each other (Figure 2). The two air cylinders would keep the pedals centered, and aligned without the need for the second cross bars (Figures 1, 6).


 

imageimageimage

Beechcraft  Pedals: Top Right

Figure 7

Beechcraft Pedals: Top Rear

Figure 8

Beechcraft Pedals: Stripped

Figure 9

 

imageimage

Beechcraft Pedals: with BellCrank

Figure 10

Beechcraft Pedals: Showing the Geometry

Figure 11

8/2/2015 Ok I just posted the blurb below and found these two photos (Figures 10, 11). This will make my life easier. I can mount my Rudder Potentiometer via the center of the Bellcrank. For auto centering, I can mount my two air cylinders on each end of the  Bellcrank.  I hope this clears thing us for the non-aircraft types,  and my self..  lol

~~Cris

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    Hi Chris,

     

    Are you going to add some feedback through the pedals or just use them to drive your simulator?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    Hi Chris,

     

    Are you going to add some feedback through the pedals or just use them to drive your simulator?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 11 years ago in reply to DAB

    DAB, you have the cart before the horse, at this time.. right now does not even fly..