Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen Sim: Converting the Game Port to USB  - F-18E Joystick - Part 4.1
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 15 Jan 2018 3:12 PM Date Created
  • Views 777 views
  • Likes 7 likes
  • Comments 3 comments
  • nexgen
  • joystick
  • hardware
  • flight_simulation
  • suncom
  • f-15
  • nexgen_flight_simulator
  • rebuild
  • software
Related
Recommended

NexGen Sim: Converting the Game Port to USB  - F-18E Joystick - Part 4.1

phoenixcomm
phoenixcomm
15 Jan 2018

imageI was going to use my Suncom F-18 Tallon Joystick but I had an F-18 Joystick from High Rev Simulations. They over-built stuff, now DOA, but Bugeye Technologies can help you. The switches are all Military quality made by Otto Controls. The Joystick base has Hall Effect sensors for the Roll and Pitch axes

IDE-34

Pin*

Pin Name*

Connection
22 AAS_PB Auto Acquisition Switch: Pull Back
23 AAS_PF Auto Acquisition Switch: Push Forward
24 ASS_sel Auto Acquisition Switch: Push Down
25 WRB_sel Weapon Release Button: Push Down
26 CS_sel

Castle Switch: Push Down

27 CS_TD Castle Switch: Tip-Down
28 CS_TU Castle Switch: Tip-Up
29 CS_TR Castle Switch: Tip-Right
30 CS_TL Castle Switch: Tip-Left
31 NWS_sel Nosewheel Steering Button: Push
32 TRMS_PF Trim Switch:  Tip-Front
33 TRMS_PR Trim Switch: Tip-Rear
34 TRMS_YR Trim Switch: Tip-Right
35 TRMS_YL Trim Switch: Tip-Left
36 TRMS_sel Trim Switch: Push Down
37 PDLS_sel Paddle Switch:
38 GUN_sel Gun Trigger:
39 RECS_sel RECCE Switch
GND GRIP GROUND
BLACK HES.1:  Ground
BLACK HES.2:  Ground
RED HES.3:  Vdd (+5vdc)
GREEN A0 HES.4:  X-Axis
WHITE A1 HES.5:  Y-Axis
HES.6:  "R"
HES.7: "B"

The Plan:

Well, the first thing I have to do is take it apart to determine the pin-outs. It's time to poke around with my DVM. The first thing is to find  Ground. I need a reference for the switch www.f-15e.info has all of the info and more. It seems that the joystick IDE interface has problems, So I'm going to do a rewire of sorts that is just replace the internal wiring and connectors with a round Floppy IDE cable that has a plastic cover over a shield and it has very tiny wires.imageimage

 

The columns Pin and Pin Name refer to an Arduino Mega 256, the Pin Name is the Symbolic name used in my Program.

 

Wiring should be straightforward I just need 2 male 34pin  headers (Wire-Wrap). A small PCB. The pin is offset by 1 space so Pin #1 of the cable is P22 on the Arduino.

There is one other thing to deal with, its the Hall Effect Sensor Plate, for the X and Y Axises This requires a separate connector a MOLEX 7-Pin 2.54mm Female Locking Connector.

In the photo (lower left) you can see the plate with the Hall Effect Sensor plate and the tube to which the stick is mounted. I will peel off seven wires from the bundle.

 

image image
image image

 

NUMBER REVISIONS DATE
1 Changed F-15 to F-18 15JAN2018
2 Changed pin 39 Definition to RECCE Switch. 15JAN2018

 

    Stay Tuned More to Come
  ~ Cris image

  • Sign in to reply

Top Comments

  • genebren
    genebren over 8 years ago +3
    Wow! Now that is a joy stick.
  • jw0752
    jw0752 over 8 years ago +2
    I love seeing the insides of electronic devices. John
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to genebren +1
    Yup, just like the real thing, just no 39 pin cannon connector at the bottom.
Parents
  • jw0752
    jw0752 over 8 years ago

    I love seeing the insides of electronic devices.

    John

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • jw0752
    jw0752 over 8 years ago

    I love seeing the insides of electronic devices.

    John