Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen Sim: Hunting List for Connectors!!
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 19 Jan 2018 5:19 AM Date Created
  • Views 1040 views
  • Likes 9 likes
  • Comments 5 comments
  • connectors
  • nexgen
  • equipment list
  • nexgen flight simulator*
  • part number
Related
Recommended

NexGen Sim: Hunting List for Connectors!!

phoenixcomm
phoenixcomm
19 Jan 2018

imageThis is a long time in coming: a cross-index of my equipment, by Part Number, Description, and Connector(s), and Mate(s).

Please check back as this will evolve over time. ~Cris image

/members-area/personalblogs/b/nexgen-flight-simuator/archive/2018/01/18/nexgen-sim-hunting-list-for-connectors/edit#
Manufacture Abbreviations
A Ametek As Austek B
Boeing
Cm Carma MFG, C Collins Crc
Conrac Corp
D Douglas
H Honeywell G Gables Engineering K

King Radio

Ky Korry M Military P

Parker

Pd Precision Display Technologies P Suncom Pd Precision Display Technologies
T Teledyne c Custom

Status Symbols
 image Have It.  image Mate + Cable End.
image Cable is Finished. image Note

Notes:

  • 14 MAR 2021 added Column Harness to the table -CAH Harnes & Connector part numbers can be found in the Master Parts Catalog
  • 1 OCT 2022 clean up the mess of the transfer to a new platform.
  • 31 JAN 23 STILL cleaning up the mess.

 

REVISIONS:

  1. 28 JAN 2021 - "Plug (Female), Contact Arrangement +Wire"..... Fixed Part Numbers and Mate and added pictures
  2. NASA - Automated Stall-Speed Warning System
  3. 4 FEB 2023 Repaired Hyperlinks.
TYPE Part Number Description M Documentation Connector Mate Stat Harness SLAVE Shelf
Flight Instrument Group by Type or Part Number
329B-8U Indicator, Attitude Direction  6" C 48-7121-8
771806
LA2.
331A-7 522-3138-004 Indicator, Horizontal Situation 4" C (1) MS2426R22B55P8X
(2) MS2426R22B55P9X
LA2.
Indicator, Vertical Speed T GUT JOB L.WS3
RM8-680.903 Indicator, Angle of Attack M83723-09H12 10N LA2.
C6E 174469-656 Indicator, Radio Compass C L.WS3
B0202 81905 Indicator, Speed (Kn/hr) GUT JOB LA2.
CP-128/ASN-128 Indicator, Radio Compass M/C L.BS4
H6L
Indicator, Turn and Slip Replace with servo drives GUT JOB LA2.
ID-453/ARN-30

Indicator, RMI

M TM 11-5826-215-35

Please See:
3436A/ARN-30D 

image 27-00004-00 NA L.WS3
3049804 Indicator, Stall Margin  (2) Crc
Non-Flight Instrument Group by Type or Part Number
8DJ176L[ZD2] Engine, Speed, N1 x 2 A Document MS3113H-18-32P DC26F18-32S LA2.
248697 Indicator, Load, DC, Dual A LA2.
Radios Group by Type or Part Number
3436A/ARN-30D Panel, Control, Radio M TM 11-5826-215-35

 

 

  image

27-00001-00

27-00002-00

614L-8 Panel, Control,  Radio, ADF C LA1.1
G-1981 Panel, Contro,  Radio,  ATC G pin-outs ZZB-AC-17 22-55P LA1.2
G-3717 Panel, Control, Radio, VHF/NAV G (1) ZZB-A0-17 22-55P
(2) 2426R16824PN
LA1.3
G-4214 Panel, Control,  Radio, Comm G DL60R-22-55P6-1A LA1.4
G-4518 Panel, Control,  Radio,  NAV/DME G " MS24264R16B24PNMS24264R16B24PN MS24266R16B24SNMS24266R16B24SN LA1.5
KFS585B Panel, Control,  Radio,  ADF K DB-37M DB-37F LA1.6
530712-1 Panel, SECAL ? ? MS-3474W12-10P
Flight Control Group
Pilot's Side Stick.
Dual Throttle Quadrant Sc Add finger Lifts detents: off, start/idle, power, 80% power
Rudder & Brakes Custom See: Boeing 737 IPC: Chapter 27-21
Other Things
Panel, Computer, NAV TM 11-5841-281-12 GUT JOB
219-100-001 Indicator, Fuel Load P PARTIAL GUT JOB LDS.1
594001-8 1680-01-015-0512
1680-01-396-9848
A10A Fire Warning Switches
5956888-503 Panel, Control, Lighting D DC22 E 41P L.BS4
7-F511F00121-1 Panel, Processor Select TM 1-1520-251-10 D38999/20JB35PN D38599/26JB35SN  image LA2.
11862

CVAC#

8-C069-322

Switch, Landing Gear Cm L.BS.2

 

Engine Start and Generator Control Panel c
F/A-18C/D (proto) Pd Document 5 BNC Connectors 5 BNC to VGA     image 27-00003-00 NA
BEZEL c
BEZEL SWITCHES c DB37 male
BEZEL LAMPS c
SPARE WHIPS
Description Slave End Mate
DB-25m to DB-25m Cable ~6,feet
Plug (Female), Contact Arrangement: 11-35 + Wireimage

DTL-38999

ES27467T11F35S | 5935-01-201-4423
MS27467T1135S   
Plug (Female), Flange Mount, Contact Arrangement: 24-19 +Wire (~2")image MS3470W24-19S
image

Contact Arrangement: +Wire (1)

DTL-38999 MS27467T11F35S MS27496T11F35S
MIL-DTL-38999 Series IIBulkhead, Male, 10" with 14PIN DIP Male + 3x SMA  MS27508E16A8P
Plug (Female) 19 pin ARC to 12096 - DB25M + 1m Cable

ARC-12096

DB25M
97-3106A-22-14P (19 pin) to DB25M w/ 7' ribbon cable.

AN-3106B-22-14S

DB25M

image
Plug (Male), Bulkhead, Contact Arrangement: 24-19 + Wire MS3470W24-19S eyelets
Plug (Male), Bulkhead, and some pins with small wires. image MS3474-W12-10P
Plug (Female), Bulkhead, Contact Arrangement: 20-16 + Wire MS3470W20-16S eyelets
image Plug (Male), Bulkhead Arrangement: 14-18+ Wire with lugs image MS3470W14-18P eyelets
DB-9F w/Mount & wire ~ 12" longimage DB-9F
DB-25M w/Shell & wire 10"~ DB-25M

image4-pin Female Universal MATE-N-LOC AMP connector with 16" wires terminated with eyelets 794707-1

1-480702-1
PINS:
350690-2 24-18
350918-3 18-14

complete cable with 9-pin plastic twist-lock connectors at each end. image HD16-9-9p-1939P

HD16-9-1939S

 

REVISIONS

  1. 28JAN2021 - "Plug (Female), Contact Arrangement +Wire"..... Fixed Part Numbers and Mate and added pictures
  2. NASA - Automated Stall-Speed Warning System
  3. 26 APR2024 Various Updates & font changes
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago +3
    One of my first projects involved searching for obscure Military Qualified connectors. Not a simple job then and with even fewer manufacturers, I suspect it is even more difficult today. DAB
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to genebren +2
    Very. But it not happening overnight and I don't think I will ever be done LOL
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to DAB +1
    Yes, this is a pain in the ass, and Yes I am always looking for cables that still have one to two feet of wire on it. Send info and you price (if any) and I will p/u postage. Just need the part number…
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to genebren

    The name of this project could be The Never Ending Story. LOL

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to DAB

    Yes, this is a pain in the ass, and Yes I am always looking for cables that still have one to two feet of wire on it. Send info and you price (if any) and I will p/u postage. Just need the part number and photo of the contact arrangement. image

    Cris

    Btw  the please distribute this list to to you palls

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 8 years ago in reply to genebren

    Very. But it not happening overnight and I don't think I will ever be done LOL

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 8 years ago

    One of my first projects involved searching for obscure Military Qualified connectors.

     

    Not a simple job then and with even fewer manufacturers, I suspect it is even more difficult today.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • genebren
    genebren over 8 years ago

    This is sounding like a very serious project.  I await the final chapter in your build.