Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: The Lab: Compaq IEEE 1284 Test Box:
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 29 Oct 2023 8:26 PM Date Created
  • Views 1596 views
  • Likes 7 likes
  • Comments 10 comments
  • nexgen
  • debuging
  • the lab
  • IEEE 1248 test box
  • Compaq
  • hacking
Related
Recommended

NexGen: The Lab: Compaq IEEE 1284 Test Box:

phoenixcomm
phoenixcomm
29 Oct 2023

imageOk, So what is this gem, I just uncovered in my junk box, well what the heck is IEEE 1284 well not sure so I looked it up  "IEEE 1284 is a standard that defines bi-directional parallel communications between computers and other devices. It was originally developed in the 1970s by Centronics and was widely known as the Centronics port, both before and after its IEEE standardization. Wikipedia". So as it turns out it's the standard bi-directional printer port. Hmmm, I might be able to use it, so as I could not find much info on the box I decided to just unbox it. What I found was the following.

  • XC68HC912B32 -- 16Bit CPU, memory, lots of I/O
  • AM7205-15RC   -- FIFO, 8KX9
  • M4-128/64          -- CPLD MACH 4 Family 5K Gates 128 Macro Cells
  • MAX237CWG    -- RS-232 Interface
  • SG615PTJC      -- CRYSTAL OSCILLATOR (29.4912Mhz)
image image

Well as you can see this is straightforward, except for the CPLD. If we assume (this may not be good), that the male header on the top of the device is not there, or to say, since I don't know what it does, hence it does nothing at this point. 

here are the next steps:

  • to find some sort of wall wart about 5-9 or pick in the middle 7vdc 
  • connect a serial monitor on the DB-9F and see if it talks. (alive or dead)

More to come ~~ CAH

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    Now that is an oldie.

    I still remember when everyone preferred parallel interfaces, then USB kind of took over, probably because it was cheaper to build and people were less concerned about throughput.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 2 years ago

    Now that is an oldie.

    I still remember when everyone preferred parallel interfaces, then USB kind of took over, probably because it was cheaper to build and people were less concerned about throughput.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to DAB

     DAB but it is still used today, 8 bits both ways there is no reason you couldn't do an 8-bit to i2c  then well you get the idea. But do you remember GPIB? my HP 6632A has it and I can control it from my computer... tada ~~Cris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago in reply to phoenixcomm

    Yes I remember the GPIB.

    Made the mistake of criticizing it during an interview with HP.

    Needless to say, I did not get the job.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • phoenixcomm
    phoenixcomm over 2 years ago in reply to DAB

     DAB  that was not a mistake my friend that was like stepping off the observation deck on the Empire State Building without a parachute. wait I think i know a better one than that:  William Shakespeare - "Hoist with his own petard" and of course to finish it with the image below. 

    imageBTW what wrong with GIB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago in reply to phoenixcomm

    The early GPIB was a bit tedious to program correctly.