Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator NexGen: The Lab: Harbor Freight Cross Slide Vice
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 10 Dec 2022 10:17 PM Date Created
  • Views 575 views
  • Likes 6 likes
  • Comments 2 comments
  • flight simulator
  • nexgen
  • the lab
  • Cross Slide Vice
  • harbor freight
Related
Recommended

NexGen: The Lab: Harbor Freight Cross Slide Vice

phoenixcomm
phoenixcomm
10 Dec 2022

Last month I picked up this beast at a garage sale for less than 20 bucks, imageit is missing one of the handles which I will have to replace. In the condition that it is somewhat less than 5 out of 10. Big wish. I wonder how I can change the stupid cheap handles to a nice vernier movement. The biggest problem this thing has going against it is that the clamp handle is at the rear of the vice. The second problem is the axis is sloppy.

Now let's see the fixes that I will do...

  1. Take it apart all the way. All of the hardware on it (nuts and bolts) will be replaced by Allen Cap-head bolts with nuts and the new hardware should have black oxide.
  2. Sand the 4 shims (for the ways), and make sure no burs, bumps, etc.
  3. Reverse the direction of the clamp bar, and modify the bar as in Fix the Orientation, the Flopping clamp handle. See videos 2, 3
  4. Re-assemble with new hardware, and grease the three lead screws. Adjust the lead screw collars.

Videos

  1. Review and getting rid of the slop! (This is the first thing to do!!)
  2. Fix the Orientation
  3. Deleting the Floppy Handle
  • Sign in to reply
Parents
  • shabaz
    shabaz over 3 years ago

    Hi Cris,

    That's great value. Also, you might be lucky, maybe each revolution is a convenient value, e.g. 2mm per revolution or something, so you can just count the turns or approximately rotate half-way for 1 mm etc. Not as good as proper marked dial with handles as you mention, but it might be good enough (rotating in just one direction to get rid of the sloppiness as you no doubt know).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • shabaz
    shabaz over 3 years ago

    Hi Cris,

    That's great value. Also, you might be lucky, maybe each revolution is a convenient value, e.g. 2mm per revolution or something, so you can just count the turns or approximately rotate half-way for 1 mm etc. Not as good as proper marked dial with handles as you mention, but it might be good enough (rotating in just one direction to get rid of the sloppiness as you no doubt know).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • phoenixcomm
    phoenixcomm over 3 years ago in reply to shabaz

    Thanks for the tip!! I wish I had some marked dials though.