Personal Blogs
  • Community Hub
  • More
Personal Blogs
NexGen Flight Simuator Where are we now, November 2022
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: phoenixcomm
  • Date Created: 18 Nov 2022 7:16 PM Date Created
  • Views 1025 views
  • Likes 7 likes
  • Comments 2 comments
  • flight simulator
  • nexgen
  • diy cockpit
  • ethernet
  • canaerospace
  • arduino
  • linux
Related
Recommended

Where are we now, November 2022

phoenixcomm
phoenixcomm
18 Nov 2022

imageOk, there has been a lot of movement in my design or should I say architecture? We have moved from my hatred of USBs where things never come up on the same address twice. A prime example is the Arduino IDEs virtual serial port. Oh, well I'm digressing. The way the system works is simple there are two communications systems going on here. 

  1. Ethernet which is used for NAVbus communications. This network controller is the NAV model, and it connects to boxes that rely on the aircraft position, in the three axes, plus the accelerations in the three axes as well, it also gives latitude and longitude on the earth. The Radio Sub System or RSS also must have both the aircraft position and the position on the earth, as well as its altitude, for some of its math problems.
  2. CANaerospace which is used for most of the intercommunication between the Feild Replaceable Units or, FRUs and the servers like NAV, RSS, etc. 
  3. CANbus which is used in some cases only if the device is a standard CANbus device. 

imagePlease Note that this system is much easier to implement as the CANaerospace protocol uses the ISO stack as well as Ethernet, So the protocol converter is written in a few lines of JAVA. Also, CANaerospace is self-identifying. That is to say that the data payload, is identified by the header, which includes number/string types, as well as other info. 

I could not find a good icon for Radio FRU, so it now has blinking lights, al la modem. The same holds true for the Protocol Converter. 

  • Sign in to reply
Parents
  • phoenixcomm
    phoenixcomm over 3 years ago

    Jan Cumps Ok there were other reasons to use Ethernet vs USB,  First USB has length limitations of about 3m. Second to go over that limitation you need some sort of extender, the most common is USB-Ethernet and at the other end, you use an Ethernet-USB converter, which costs about somewhere between 20 to 80 bucks. I just use an Ethernet shield for the Arduino Mega which costs about 12 bucks on eBay. 

    More point I use terminated CAT-5 patch cord for my CANAerospace cabling. So I only need to buy two items 1. MCP2515 CAN Bus Module with a TJA1050 transceiver 2. Dual RJ45 Ethernet Connector Breakout Board, off of eBay for less than a ten spot. 

    Point to ponder I don't believe that USB ever used the ISO network model. And I wouldn't even think about trying to pass CAN over it. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • phoenixcomm
    phoenixcomm over 3 years ago

    Jan Cumps Ok there were other reasons to use Ethernet vs USB,  First USB has length limitations of about 3m. Second to go over that limitation you need some sort of extender, the most common is USB-Ethernet and at the other end, you use an Ethernet-USB converter, which costs about somewhere between 20 to 80 bucks. I just use an Ethernet shield for the Arduino Mega which costs about 12 bucks on eBay. 

    More point I use terminated CAT-5 patch cord for my CANAerospace cabling. So I only need to buy two items 1. MCP2515 CAN Bus Module with a TJA1050 transceiver 2. Dual RJ45 Ethernet Connector Breakout Board, off of eBay for less than a ten spot. 

    Point to ponder I don't believe that USB ever used the ISO network model. And I wouldn't even think about trying to pass CAN over it.