Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog FRDM-KL25z and TMP36 sensor
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 25 Jun 2013 12:10 AM Date Created
  • Views 1038 views
  • Likes 0 likes
  • Comments 2 comments
  • 2.9v
  • frdm-kl25z
  • tmp36
  • arduino
  • 3.3v
Related
Recommended

FRDM-KL25z and TMP36 sensor

ntewinkel
ntewinkel
25 Jun 2013

I've been working on a data logging system for my greenhouse - basically just a way of tracking soil moisture, sunlight, rain barrel water level, and of course temperature inside and outside of the greenhouse.

 

I built most of it for Arduino, as I have several of them, and only one KL25z - and I have other plans for the KL25z board image

 

But I thought I'd try the TMP36 temperature sensor with the KL25z, as the Arduino has a couple of limitations that are bugging me for the project:

* First, to keep things simple I've been saving the data in a plain array in memory, but the Arduino Uno only has 2Kb RAM available, of which much is taken up by my program as it runs. The KL25z has a whopping 16Kb.

* Second, the Uno's ADC is only 10bit where the KL25z has 16bit ADCs. For the TMP36 sensor, which returns a set 10mV per degree, this should give us some extra accuracy.

 

3.3 Volts ?

One of the first things I noticed is that the temperature returned was always much too high. So I checked the actual voltage on the 3.3v pin, and it actually shows as being a steady 2.908 volts. That's kind of odd, but adjusting the code to use that number to find the proper temperature seems to give me the correct results.

 

I don't know why, but the Arduino was returning much steadier results from the TMP36 sensor, even when I decided to take the average of something like 100 readings on the KL25z. Not sure why that would be, but maybe a hardware guru can enlighten us on that image  I'm guessing that the added speed of the KL25z might have something to do with it. From a software perspective, it might be a good idea to take a lot of samples and return the statistical mean - given the extra speed and memory, the KL25z should be able to tackle that quite easily without significant delay.

 

Here is the code I used, if you want to try this at home:

 

#include "mbed.h"


AnalogIn tmp36sensor(PTB0);


float sum;


int main() {
    while(1) {
    
        sum = 0.0;
        
        for(int i=0; i<200; i++) {
            sum = sum + (tmp36sensor.read() * 290.8 - 50.0); // the 3.3v from the KL25Z is really only 2.908 volts
        }
    
        printf("Temperature = %0.1f \n", sum / 200.0);
        wait(2.0);
    }
}

 

The sensor read returns a value between 0 and 1, which is the percentage the input voltage is at, compared to the reference voltage. The 50 is the offset required for the TMP36 (allows for negative temperatures).

 

Cheers,

-Nico

  • Sign in to reply

Top Comments

  • vsluiter
    vsluiter over 13 years ago +1
    Nico, Others have found similar problems: http://mbed.org/forum/mbed/topic/628/?page=1#comment-3178 Maybe you could set the reference voltage to an internal reference to see whether that helps; with no…
Parents
  • vsluiter
    vsluiter over 13 years ago

    Nico,

    Others have found similar problems: http://mbed.org/forum/mbed/topic/628/?page=1#comment-3178

    Maybe you could set the reference voltage to an internal reference to see whether that helps; with no  API call for that, it would involve digging into the Freescale registers.

    Otherwise use a RC filter (small R, large C to quickly fill the Sample-and-Hold capacitor) to buffer the output of your sensor. Your temperature won't be changing that fast...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 12 years ago in reply to vsluiter

    Thanks Victor!

    Maybe that's something they're still working on. I'd rather avoid going to register level to do anything, but I might try the RC filter at some point.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 12 years ago in reply to vsluiter

    Thanks Victor!

    Maybe that's something they're still working on. I'd rather avoid going to register level to do anything, but I might try the RC filter at some point.

     

    Cheers,

    -Nico