Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Gobetwino
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 17 Mar 2012 4:42 PM Date Created
  • Views 3435 views
  • Likes 3 likes
  • Comments 22 comments
  • gobetwino
  • arduino
Related
Recommended

Gobetwino

ntewinkel
ntewinkel
17 Mar 2012

I was watching a conversation on the forum about questions regarding Arduino, which involved connecting Arduino to a Windows-based program named "Gobetwino", and it caught my interest.

 

In a nutshell, Gobetwino is a program that runs on your Windows machine, and waits for commands via the serial port.

You can use your Arduino (or any other micro-controller, or even another computer) to send commands to Gobetwino via the serial port.

 

So I set it up and after a bit of fiddling got it to open NotePad and had it type "Hello World!" into the new NotePad file image

 

Attached are the complete step by step instructions for both sides of the equation, in case anyone is interested.

 

ps, I did this on a WindowsXP machine (in a VirtualBox on Mac actually). The Gobetwino author also recommends XP, so it may not work the same way, or at all, on Vista or 7.

 

Cheers,

-Nico

Attachments:
Gobetwino.rtf
  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 14 years ago in reply to ntewinkel +1
    Hi Neil, Gobetwino with Open Office on XP seems to behave well for me. It opens OO, then starts typing things into the fields reliably. I couldn't figure out how to handle a timestamp in the time I had…
Parents
  • neilk
    neilk over 14 years ago

    Nico - many thanks for that; I've been meaning to play with Gobetwino for a while now and you gave me the impetus I needed! Now I need to make it do what I want it to do !!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to neilk

    You're very welcome, Neil! What is it you are wanting it to do?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to neilk

    Hi again,

     

    Yeah I gave into temptation and just bought another Arduino-Nano and 2x nrf24l01+ wireless cards - about $20 for all so that's not too bad.

     

    So that should allow me to send and receive data between two arduino boards over a longer distance than with the bluetooth.

     

    I shied away from getting the SD card module... for now image

     

    Haven't had time for the gobetwino-openoffice data logging yet, but this weekend is looking really good.

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to ntewinkel

    Hi Neil,

     

    Gobetwino with Open Office on XP seems to behave well for me. It opens OO, then starts typing things into the fields reliably.

    I couldn't figure out how to handle a timestamp in the time I had this morning, but it looks like it should be possible. It's hard to debug, since the Serial output goes to Gobetwino.

     

    I made a new blog post for the details and the sketch: http://www.element14.com/community/people/ntewinkel/blog/2012/03/26/gobetwino-with-open-office

     

    My wife kicked the tomato plants out of the house, so they are all in the greenhouse now - which means I really want to get this thing up and running soon to see if they're in any danger!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 14 years ago in reply to ntewinkel

    Hi Nico,

     

    Back from Paris - it wasn't long enough, but the weather was amazing for the time of year!

    Congratulations with OO in XP - I was having trouble with OO in W7.

     

    Outside of that, I also couldn't get time stamps to work, but I have achieved a breakthrough for me:

     

    1. Running a sketch on Arduino UNO connected to my W7 netbook.

     

    2. Sending commands to Gobetwino to start Notepad on the netbook and via the command line option in Gobetwino, open an existing empty file on my desktop XP PC, via my wireless network.

     

    3. Logging data from my temp probes and sending over the network to the file in the form 101 "," 101 "CR/LF"

     

    4. Closing down Notepad and saving the file on the desktop after a preset number of readings.

     

    The secret seems to be to give Notepad plenty of time to start up and open the file over the network. If you don't wait long enough, some of the data gets lost.

     

    Can you see the scenario - Arduino and netbook in the Greenhouse; desktop PC in my office.....sit down after breakfast and check the file.....go out later & reset the arduino.....long term, I want to try the bluetooth, because I don't want to leave the netbook out in the Greenhouse all the time.

     

    My tomato plants are out in my Greenhouse as well........looking OK so far

     

    All the best

     

    Neil

     

    PS - I will set up my own blog to document all this for anyone who might be interested.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to neilk

    Hi Neil,

     

    That's great! Good idea about using Notepad - much quicker to start and less stuff that can go wrong. I had something like a 10 second delay just to make sure. I think you can also do a serial.read() which (I think) waits to get the result from the program startup.

    I was thinking of maybe looking into the gobetwino logging feature as well, which makes the timestamps easier. So in the command you'd have to choose the one for logfile.

     

    And I suppose for either case you could have it type the data into a .csv file (it kinda looks like that's what you are doing already?), and then it can be imported as a spreadsheet for graphing or whatnot.

     

    And yes, I totally see the scenario. Have you actually been running it like that already?

    I've been busy all week trying to get all my other work done so I can get this installed in my greenhouse soon too. I'm still having a bit of trouble getting my LM34 Fahrenheit sensor to give believeable temperatures though.

     

    My tomato plants are looking pretty happy too. It being end of March I think the chance of a hard frost getting into the greenhouse is pretty slim now. Forecast says we still dip down to 0 C every night though...

     

    Looking forward to seeing your blog too!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 14 years ago in reply to ntewinkel

    Hi Nico,

     

    I think the initial serial read gets the program PID after startup. However, the bigger issue is waiting for the file to open on the networked PC.....watching the screen, Notepad seems to open fairly qickly on the W7 device, but with an untitled (ie new) file. Some time later - several seconds, the filename displayed changes to be the one specified in the gobetwino command line parameter. I had to put in another delay to make sure I didn't start sending data too soon.

     

    The gobetwino logging feature does look interesting, because of the timestamps - I may get to try that as well, locally first and then over the network.

     

    Sadly, my setup is only running with the netbook and desktop side by side on my desk - I keep thinking of reasons not to take the arduino and the netbook out into the greenhouse just yet.

     

    My latest idea is rather than leave the desktop switched on overnight, get the netbook/arduino to log data to a local file and then when it has finished - after a specific number of samples -  to ping the desktop and wait until it is there and then copy the data file over the network to the desktop.

     

    I have tested the gobetwino file copy (but not over the network yet). I haven't tried the gobetwino pingt.

     

    I am using LM35 temp monitors - they are OK but they have problems of their own - I haven't sorted all of those out yet, but if I take enough readings (100) at say 20mS intervals and take an average, I get reasonable results.

     

    I wish I had more time - including time to write a blog about all my adventures with the arduino greenhouse data logger. I'll get to it soon!

     

    All the best

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neilk
    neilk over 14 years ago in reply to ntewinkel

    Hi Nico,

     

    I think the initial serial read gets the program PID after startup. However, the bigger issue is waiting for the file to open on the networked PC.....watching the screen, Notepad seems to open fairly qickly on the W7 device, but with an untitled (ie new) file. Some time later - several seconds, the filename displayed changes to be the one specified in the gobetwino command line parameter. I had to put in another delay to make sure I didn't start sending data too soon.

     

    The gobetwino logging feature does look interesting, because of the timestamps - I may get to try that as well, locally first and then over the network.

     

    Sadly, my setup is only running with the netbook and desktop side by side on my desk - I keep thinking of reasons not to take the arduino and the netbook out into the greenhouse just yet.

     

    My latest idea is rather than leave the desktop switched on overnight, get the netbook/arduino to log data to a local file and then when it has finished - after a specific number of samples -  to ping the desktop and wait until it is there and then copy the data file over the network to the desktop.

     

    I have tested the gobetwino file copy (but not over the network yet). I haven't tried the gobetwino pingt.

     

    I am using LM35 temp monitors - they are OK but they have problems of their own - I haven't sorted all of those out yet, but if I take enough readings (100) at say 20mS intervals and take an average, I get reasonable results.

     

    I wish I had more time - including time to write a blog about all my adventures with the arduino greenhouse data logger. I'll get to it soon!

     

    All the best

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ntewinkel
    ntewinkel over 14 years ago in reply to neilk

    Hi Neil,

     

    I see - that file open would add a fair chunk of time, especially over the network.

     

    Would it be possible to just write the file on the netbook in a shared folder, and then use the other computer to connect to the netbook's share in the morning?

     

    I think the LM35 might be just the Centigrade version of the Fahrenheit sensor I have (or vice versa), so in theory they likely get hooked up the same way. Did you have to add a resistor to it?

     

    Tomorrow being, theoretically at least, a "day of rest" I should be entitled to some tinkering time, methinks!

     

    Cheers,

    -Nico

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 14 years ago in reply to ntewinkel

    Hi Nico

     

    Doh!  why didn't I think of that - I'm always looking for a "clever" solution that exploits as much as possible.......sighs.

     

    I just have the LM35 connected across +5v and 0v, with the centre leg delivering 10mV/deg celsius, but, with an effective offset of 2 deg, because the o/p is 0v at 2 deg.

     

    The first problem I encountered was that the first reading in any set of readings is always significantly lower than the rest. Apologies if you already know this!

     

    On googling, I find the problem is alleged to be a combination of at least 2 issues:

    1. The LM35 is relatively high impedance, compared with the analog pins on the Arduino, so there are current flow problems or something like that.

    2. The Arduino analog pins are multiplexed & it takes time for that to stabilise when you switch pins - ie reading more than 1 analog pin.

     

    Anyway, the recommended solution seems to be to read the pin, discard the reading, wait about 5 mSec and then read it again.............seems to be the answer.

     

    My second problem is a result of me being lazy and not using a screened cable for the LM35 that needs to be a long way from the Arduino.......the signal is quite low - 200mV for 20 ish celsius.......so I get quite a bit of hum and variability on those readings............just haven't got round to replacing the cable!

     

    I have been in the garden and greenhouse all morning and about to partake of Sunday lunch....best meal of the week.

     

    Hope you get some time to tinker

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to neilk

    Hi Neil,

     

    Thanks for the hints on the temp sensor, I'll give that a shot.

     

    I spent most of yesterday actually doing some planting in the greenhouse, but I took some time today to work on the MSP430 launchpad that I have here - it's that $4.30 (includes shipping!) board from TI. The basic demo it comes with sends temperature from it's onboard temperature sensor via serial to a windows GUI.

    I figure that would be a good unit for this project, as it's so inexpensive. Then it doesn't matter as much if a slug shorts it out image

     

    So I've been modifying the demo code to remove the unwanted parts of the demo and to make it send a readable string for the temperature, rather than a single byte. Wow I have to tell you that's nasty cryptic stuff - it's C but not nearly as clear and easy as our friend the Arduino!

    It doesn't have as much stuff (power, memory, pins) as the Arduino, but for many projects it could make a viable alternative. Too bad the programming environment is so complex.

     

    I got it sending strings for the temperature, so it's just a step away from hooking up to gobetwino.

     

    Then I got an email from a client needing some stuff, so I guess I best get on that!

     

    Hope you're off to a good start this week.

     

    Cheers,

    -Nico