Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Gobetwino
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 17 Mar 2012 4:42 PM Date Created
  • Views 3396 views
  • Likes 3 likes
  • Comments 22 comments
  • gobetwino
  • arduino
Related
Recommended

Gobetwino

ntewinkel
ntewinkel
17 Mar 2012

I was watching a conversation on the forum about questions regarding Arduino, which involved connecting Arduino to a Windows-based program named "Gobetwino", and it caught my interest.

 

In a nutshell, Gobetwino is a program that runs on your Windows machine, and waits for commands via the serial port.

You can use your Arduino (or any other micro-controller, or even another computer) to send commands to Gobetwino via the serial port.

 

So I set it up and after a bit of fiddling got it to open NotePad and had it type "Hello World!" into the new NotePad file image

 

Attached are the complete step by step instructions for both sides of the equation, in case anyone is interested.

 

ps, I did this on a WindowsXP machine (in a VirtualBox on Mac actually). The Gobetwino author also recommends XP, so it may not work the same way, or at all, on Vista or 7.

 

Cheers,

-Nico

Attachments:
Gobetwino.rtf
  • Sign in to reply

Top Comments

  • ntewinkel
    ntewinkel over 14 years ago in reply to ntewinkel +1
    Hi Neil, Gobetwino with Open Office on XP seems to behave well for me. It opens OO, then starts typing things into the fields reliably. I couldn't figure out how to handle a timestamp in the time I had…
Parents
  • neilk
    neilk over 14 years ago

    Hi Nico

     

    The MSP430 sounds interesting; I'll check it out!

     

    I haven't made much progress in a forward direction, other than re-writing a huge amount of code and consequently achieving a tremendous feeling of self-satisfaction:-

     

    I'm not a C programmer - my programming was ALGOL, FORTRAN, various assemblers and finally MUMPS or M, before I ceased programming more or less commpletely around 20 years ago. Consequently, since taking up with Arduino, I have been totally reliant on the (EXCELLENT) published reference information and forums.

     

    For instance, I'd never heard of stdlib and particularly the atoi() and itoa() functions, until I saw them and  puzzled over them in the gobetwino sample sketches. I also had no idea about using pointers, again until I saw it in the same place.

     

    Basically, I have rewritten all my I/O code to use pointers with character Arrays instead of String objects and atoi().........and scrapped a lot of my own code that I had laboriously written to do the same jobs. Self-satisfied is how I feel!

     

    Also - We have our grandaughters staying (8 and 11) so there are other demands on my time between breakfast and their bedtime!

     

    Perhaps I will have a little more time after Easter when they go home.

     

    Best wishes

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • neilk
    neilk over 14 years ago

    Hi Nico

     

    The MSP430 sounds interesting; I'll check it out!

     

    I haven't made much progress in a forward direction, other than re-writing a huge amount of code and consequently achieving a tremendous feeling of self-satisfaction:-

     

    I'm not a C programmer - my programming was ALGOL, FORTRAN, various assemblers and finally MUMPS or M, before I ceased programming more or less commpletely around 20 years ago. Consequently, since taking up with Arduino, I have been totally reliant on the (EXCELLENT) published reference information and forums.

     

    For instance, I'd never heard of stdlib and particularly the atoi() and itoa() functions, until I saw them and  puzzled over them in the gobetwino sample sketches. I also had no idea about using pointers, again until I saw it in the same place.

     

    Basically, I have rewritten all my I/O code to use pointers with character Arrays instead of String objects and atoi().........and scrapped a lot of my own code that I had laboriously written to do the same jobs. Self-satisfied is how I feel!

     

    Also - We have our grandaughters staying (8 and 11) so there are other demands on my time between breakfast and their bedtime!

     

    Perhaps I will have a little more time after Easter when they go home.

     

    Best wishes

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • neilk
    neilk over 14 years ago in reply to neilk

    Hi again Nico

     

    I looked at the MSP430 & watched the 2 launchpad videos............amazing.

     

    The only UK agent I could find quickly, with the MSP430 in stock, will charge me £3.26GBP - similar to your $4.30, but also £12.00GBP - around $17 for shipping...................................I am kind of speechless. There may have also been a further 20% tax on top - I didn't get that far in the ordering process!!!!!!!!!!!!!!

     

    However, If I bought 20 of them, I would get free shipping.................

     

    All the best

     

    Neil

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 14 years ago in reply to neilk

    Hi Neil,

     

    I found that the easiest and cheapest way to buy it was straight from Texas Instruments on their own website. All the third party places charge horrible amounts for shipping and handling. Plus you can add a few sample chips that way too - I picked up a few 20-pin chips for the added IO pins.

     

    And I still got it overnight that way, so either they have lightning fast couriers or they have warehouses in every country.

     

    The MSP430 is a lot harder to program though. That's almost worth the extra bucks for the Arduino! It's the super cheap price that makes it interesting, so $17 shipping ruins that for me - I just received an Arduino Nano yesterday that cost me $15 on eBay *after* shipping. (Still waiting for the 2 wireless cards)

    If you can't get it straight from TI, it's small and light enough that I could reship one to you for probably about a dollar if we take it out of the box. But I'm pretty sure if you go straight to the TI website that you can get it direct.

     

    I've only done a little bit of Fortran in my days - it was one of my first work terms as part of the university degree. Then it was pretty much all C up until I got into (Apple) Newtonscript and then Java. So with C now being the standard for firmware, that's a useful skill to have again image

     

    Cheers,

    -Nico