Personal Blogs
  • Community Hub
  • More
Personal Blogs
Nico teWinkel's Blog Tinkerkit Braccio Robot Arm
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ntewinkel
  • Date Created: 31 Jul 2022 6:28 AM Date Created
  • Views 3463 views
  • Likes 8 likes
  • Comments 3 comments
  • unicorn
  • tinkerkit
  • Braccio
  • robot arm
  • arduino
Related
Recommended

Tinkerkit Braccio Robot Arm

ntewinkel
ntewinkel
31 Jul 2022
Tinkerkit Braccio Robot Arm

The good folks of element14 were kind enough to send me this awesome robot arm as part of a contest reward shopping cart. Thank you element14 team!

Tinkerkit Braccio Robot Arm

It has a lot of little pieces to put together. Good thing I had help!

Tinkerkit robot arm contents

robot arm pieces

After a fun afternoon building this cool 3-D puzzle, this is what it looked like:

Braccio robot arm nearly done

There were a few parts that didn't quite fit - the tolerances appear to be very tight, and for two of the parts I needed to do some light sanding to have it all fit properly (and believe me, I tried plenty of angles first before doing that).
The assembly video helped quite a bit though, to compare how things fit together. The instruction pamphlet by itself lacked a few details, including the placement of the wires, and it misses a crucial step in getting the examples running - a library needs to be installed first. The website helps for that.
One thing that was a bit harsh is that the first example sets all the servos to their proper middle position - the instructions say you then have to adjust the servos if the robot arm isn't perfectly straight. Grimacing That would mean pretty much taking the whole thing apart! The arm is pretty close the way it is, and maybe the code can be adjusted to compensate.

I moved it to my desk to complete the final steps, and so I could hook it up to my computer to program the Arduino to control it.

Tinkerkit Braccio Robot Arm Complete

This robot arm kit comes complete with the Arduino shield to run all the servos. It also includes the special 4 amp 5v adapter to power all of it properly.

The only thing needed to complete it is the Arduino microcontroller. I used the Arduino Uno I had available, but it does support several other Arduino boards, including the WiFi versions that then allow control via an app, which would have been cool too.

Here it is showing off its pet unicorn.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

My conclusion?
Two thumbs up!
it's a fun project to build, easy to operate with Arduino code, and I can see it being used in fun silly future projects.

-Nico

  • Sign in to reply

Top Comments

  • genebren
    genebren over 4 years ago +1
    Fun looking kit! You made a good choice on utilizing you prize cart.
  • DAB
    DAB over 4 years ago +1
    Nice build Nico. Do you have an application in mind or did you get it just to play with?
  • ntewinkel
    ntewinkel over 4 years ago in reply to DAB +1
    DAB asked: >" Do you have an application in mind or did you get it just to play with?" I've had random fun ideas for robot arms over the years, but there's no direct need for it. The great thing about…
Parents
  • DAB
    DAB over 4 years ago

    Nice build Nico.

    Do you have an application in mind or did you get it just to play with?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 4 years ago in reply to DAB

    DAB asked:
    >"Do you have an application in mind or did you get it just to play with?"

    I've had random fun ideas for robot arms over the years, but there's no direct need for it. The great thing about the shopping cart rewards is that it allows up to pick up useful necessities as well as the occasional whimsical fun thing that I don't have to explain to the wife Smiley

    I really want to participate in the challenge to build a Rube Goldberg machine, so unless I get side-tracked I hope to use the robot arm for that soon Smiley

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ntewinkel
    ntewinkel over 4 years ago in reply to DAB

    DAB asked:
    >"Do you have an application in mind or did you get it just to play with?"

    I've had random fun ideas for robot arms over the years, but there's no direct need for it. The great thing about the shopping cart rewards is that it allows up to pick up useful necessities as well as the occasional whimsical fun thing that I don't have to explain to the wife Smiley

    I really want to participate in the challenge to build a Rube Goldberg machine, so unless I get side-tracked I hope to use the robot arm for that soon Smiley