Personal Blogs
  • Community Hub
  • More
Personal Blogs
Rachael's Blog A brief tour of my development lab
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rachaelp
  • Date Created: 16 Dec 2016 11:09 PM Date Created
  • Views 5664 views
  • Likes 17 likes
  • Comments 38 comments
  • lab_setup
  • lab_equipment
Related
Recommended

A brief tour of my development lab

rachaelp
rachaelp
16 Dec 2016

I thought I would give a brief overview of my current lab setup to show the equipment I use and how I have things configured, and outline how I want to change things etc, and what additional equipment I would like to have which will lead into a future blog post outlining some of the projects I am planning to augment my current setup. I should note that what you cant see in the picture below is that the other side is another two desks with my other computers on them which is where I do most of my EAGLE work so the Brix isn't the only computer in the setup.

 

So to start off here is a picture of my lab:

 

image

 

Here is a list of the main equipment in its current form:

 

Keysight MSO-X 3054A Mixed Signal Oscilloscope with all options unlocked

Keithley 2015 THD 6.5 Digit Bench DMM

Agilent  U1272AU1272A Hand Held DMM

Fluke PM6685 Universal Frequency Counter

TTi QL355T Power Supply

TTi  PL303QMDPL303QMD Power Supply

TTi  CPX400SCPX400S Power Supply

TTi LD300 DC Electronic Load

Metcal MX-5000 Soldering Station

Metcal MFR-1300 Desoldering Station

Metcal  HCT2-120HCT2-120 Hot Air Rework Station

Gigabyte Brix BX-BT-1900 running Linux Mint 18

Dell 24" Flat Panel Monitor

Luxo Magnifier Lamp

 

I also have an assortment of cables, programmers, USB-serial widgets, etc, etc which come in handy but I always seem to find I need something else! Maybe in time I will build up enough kit that I stop being held up by needing to source some extra random piece of kit!

 

So you can see I have a reasonable amount of test kit but there are a few gaps which I would like to fill:

 

Spectrum analyzer Unfortunately these are very pricey so I have to wait until I have a very good justification before I buy one I'm currently leaning towards a Tektronix  RSA306BRSA306B or a Signal Hound BB60C I've seen reviews on both of these on The Signal Path Blog http://thesignalpath.com/blogs/) and I can't currently make up my mind which I would prefer. Tek are obviously the bigger company with more resources but I would like the SignalVU software to run native on my Mac ideally which isn't currently an option but then it's not an option for the Signal Hound kit either. I think when you add in the cost of all the paid for options for Tek which are included free with Signal Hound then this is probably the more cost effective option if you need those features. What do others think of these two options? I'd also consider something older from eBay if I could find something decent at a reasonable price. A lot of the affordable ones are so old they have a floppy drive in them and they weigh a lot and make a huge amount of noise when turned on so I don't want anything like that, hence my current two top choices.

 

Vacuum manual assisted pick and place. This is similar to what shabaz is doing as outlined in one of his recent blogs (https://www.element14.com/community/groups/open-source-hardware/blog/2016/11/07/building-a-smt-pick-and-place-buddy) and I have some ideas for enhancing this further and integrating with EAGLE and some other cool additions (more on this in another blog).

 

I'd like to get my oscilloscope on the network. I've in the past connected to it using USB via SCPI using a python library and whilst it works it's not the most efficient way of doing things so I don't bother with that at the moment. Having access to the scope via the network will make controlling it and grabbing screen captures to put into write ups so much simpler. Unfortunately the DSOXLAN add on for it is £300 which is quite a lot as it combines a network port with a VGA port (Which I don't really need). I've seen some blog posts which show how to build a board which basically provides the RJ45 connector and connects it up as that is all that is required to make the network port accessible it seems so this seems quite a good option.

 

I'd also like a really stable and accurate 10MHz clock source which will feed into various equipment. Currently only the Frequency counter can accept an external reference clock but Spectrum Analysers and Signal Generators will as well. I've got an idea to build a GPS disciplined oscillator with multiple buffered outputs to take to various pieces of equipment. This will probably be a topic of a future blog post too.

 

One thing I do need to improve is the lighting setup. Whilst it's not too bad for the soldering station when the magnifier lamp is turned on, over the other end of the bench can get quite dark on dull days or at night so I need to have some additional lighting installed to improve this aspect.

 

Thanks for reading and feel free to make suggestions for things I should add to my lab setup.

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 9 years ago in reply to rachaelp +6
    Can't believe how neat you all are. I'm always embarrassed to show anyone the clutter on my bench. Do they still put a logo on the mats? This one probably dates from the 1990s.
  • balearicdynamics
    balearicdynamics over 9 years ago +6
    BTW... While in Spain I am organising to have a decent working developing and prototyping lab, from 3D printing to soldering station up to software development, here in the Netherlands I rent a romm"all…
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp +6
    There is never any end to the demands for more space - I have a factory unit with 1000 ft^2 and an additional 200 ft^2 for light storage above an internal ceiling. About 500 ft^2 is enclosed in an insulated…
Parents
  • mcb1
    mcb1 over 9 years ago

    suggestions for things I should add to my lab setup.

    A mess ..... it's far too tidy image

     

    That is a decent collection of equipment.

     

     

    I need to have some additional lighting

    I see you have added lighting under the top shelf which seems to be bright enough, but you need to replicate the same light levels on the desk.

     

    I still prefer focused lighting, and having seen some of the newer LED lamps, it makes sense to remove the heat aspect but keep the white light.

    The only issue I have found is that most are too wide to be useful over benches, given that they start from near the ceiling and are usually 60 degs beamwidth.

     

    You may get away with adding LED strip lighting along the front edge of the top shelf, with a suitable shield so it only shines downwards.

    It's worth experimenting with ...

     

     

    Mark

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to mcb1

    Hi Mark,

     

    mcb1 wrote:

     

    suggestions for things I should add to my lab setup.

    A mess ..... it's far too tidy

    LOL, yes I take your point! image To be fair it's not that tidy when I am mid project and I did tidy it up a little for the photo. I do try and put everything away once I have finished with them though so I know where everything is next time I need is and also so I have space to spread out with a new project rather than having to work around clutter.

     

    mcb1 wrote:

     

    I need to have some additional lighting

    I see you have added lighting under the top shelf which seems to be bright enough, but you need to replicate the same light levels on the desk.

    Yes I agree, the light level for the shelves is good, it's down at the bench that things aren't good enough.

     

    mcb1 wrote:

     

    I still prefer focused lighting, and having seen some of the newer LED lamps, it makes sense to remove the heat aspect but keep the white light.

    The only issue I have found is that most are too wide to be useful over benches, given that they start from near the ceiling and are usually 60 degs beamwidth.

     

    You may get away with adding LED strip lighting along the front edge of the top shelf, with a suitable shield so it only shines downwards.

    It's worth experimenting with ...

    Thanks for the lighting suggestions, I have quite a lot of things to look at on this front, I'll give an update once I have it all sorted image

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rachaelp
    rachaelp over 9 years ago in reply to mcb1

    Hi Mark,

     

    mcb1 wrote:

     

    suggestions for things I should add to my lab setup.

    A mess ..... it's far too tidy

    LOL, yes I take your point! image To be fair it's not that tidy when I am mid project and I did tidy it up a little for the photo. I do try and put everything away once I have finished with them though so I know where everything is next time I need is and also so I have space to spread out with a new project rather than having to work around clutter.

     

    mcb1 wrote:

     

    I need to have some additional lighting

    I see you have added lighting under the top shelf which seems to be bright enough, but you need to replicate the same light levels on the desk.

    Yes I agree, the light level for the shelves is good, it's down at the bench that things aren't good enough.

     

    mcb1 wrote:

     

    I still prefer focused lighting, and having seen some of the newer LED lamps, it makes sense to remove the heat aspect but keep the white light.

    The only issue I have found is that most are too wide to be useful over benches, given that they start from near the ceiling and are usually 60 degs beamwidth.

     

    You may get away with adding LED strip lighting along the front edge of the top shelf, with a suitable shield so it only shines downwards.

    It's worth experimenting with ...

    Thanks for the lighting suggestions, I have quite a lot of things to look at on this front, I'll give an update once I have it all sorted image

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down