Personal Blogs
  • Community Hub
  • More
Personal Blogs
Rachael's Blog A brief tour of my development lab
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: rachaelp
  • Date Created: 16 Dec 2016 11:09 PM Date Created
  • Views 5638 views
  • Likes 17 likes
  • Comments 38 comments
  • lab_setup
  • lab_equipment
Related
Recommended

A brief tour of my development lab

rachaelp
rachaelp
16 Dec 2016

I thought I would give a brief overview of my current lab setup to show the equipment I use and how I have things configured, and outline how I want to change things etc, and what additional equipment I would like to have which will lead into a future blog post outlining some of the projects I am planning to augment my current setup. I should note that what you cant see in the picture below is that the other side is another two desks with my other computers on them which is where I do most of my EAGLE work so the Brix isn't the only computer in the setup.

 

So to start off here is a picture of my lab:

 

image

 

Here is a list of the main equipment in its current form:

 

Keysight MSO-X 3054A Mixed Signal Oscilloscope with all options unlocked

Keithley 2015 THD 6.5 Digit Bench DMM

Agilent  U1272AU1272A Hand Held DMM

Fluke PM6685 Universal Frequency Counter

TTi QL355T Power Supply

TTi  PL303QMDPL303QMD Power Supply

TTi  CPX400SCPX400S Power Supply

TTi LD300 DC Electronic Load

Metcal MX-5000 Soldering Station

Metcal MFR-1300 Desoldering Station

Metcal  HCT2-120HCT2-120 Hot Air Rework Station

Gigabyte Brix BX-BT-1900 running Linux Mint 18

Dell 24" Flat Panel Monitor

Luxo Magnifier Lamp

 

I also have an assortment of cables, programmers, USB-serial widgets, etc, etc which come in handy but I always seem to find I need something else! Maybe in time I will build up enough kit that I stop being held up by needing to source some extra random piece of kit!

 

So you can see I have a reasonable amount of test kit but there are a few gaps which I would like to fill:

 

Spectrum analyzer Unfortunately these are very pricey so I have to wait until I have a very good justification before I buy one I'm currently leaning towards a Tektronix  RSA306BRSA306B or a Signal Hound BB60C I've seen reviews on both of these on The Signal Path Blog http://thesignalpath.com/blogs/) and I can't currently make up my mind which I would prefer. Tek are obviously the bigger company with more resources but I would like the SignalVU software to run native on my Mac ideally which isn't currently an option but then it's not an option for the Signal Hound kit either. I think when you add in the cost of all the paid for options for Tek which are included free with Signal Hound then this is probably the more cost effective option if you need those features. What do others think of these two options? I'd also consider something older from eBay if I could find something decent at a reasonable price. A lot of the affordable ones are so old they have a floppy drive in them and they weigh a lot and make a huge amount of noise when turned on so I don't want anything like that, hence my current two top choices.

 

Vacuum manual assisted pick and place. This is similar to what shabaz is doing as outlined in one of his recent blogs (https://www.element14.com/community/groups/open-source-hardware/blog/2016/11/07/building-a-smt-pick-and-place-buddy) and I have some ideas for enhancing this further and integrating with EAGLE and some other cool additions (more on this in another blog).

 

I'd like to get my oscilloscope on the network. I've in the past connected to it using USB via SCPI using a python library and whilst it works it's not the most efficient way of doing things so I don't bother with that at the moment. Having access to the scope via the network will make controlling it and grabbing screen captures to put into write ups so much simpler. Unfortunately the DSOXLAN add on for it is £300 which is quite a lot as it combines a network port with a VGA port (Which I don't really need). I've seen some blog posts which show how to build a board which basically provides the RJ45 connector and connects it up as that is all that is required to make the network port accessible it seems so this seems quite a good option.

 

I'd also like a really stable and accurate 10MHz clock source which will feed into various equipment. Currently only the Frequency counter can accept an external reference clock but Spectrum Analysers and Signal Generators will as well. I've got an idea to build a GPS disciplined oscillator with multiple buffered outputs to take to various pieces of equipment. This will probably be a topic of a future blog post too.

 

One thing I do need to improve is the lighting setup. Whilst it's not too bad for the soldering station when the magnifier lamp is turned on, over the other end of the bench can get quite dark on dull days or at night so I need to have some additional lighting installed to improve this aspect.

 

Thanks for reading and feel free to make suggestions for things I should add to my lab setup.

  • Sign in to reply

Top Comments

  • jc2048
    jc2048 over 9 years ago in reply to rachaelp +6
    Can't believe how neat you all are. I'm always embarrassed to show anyone the clutter on my bench. Do they still put a logo on the mats? This one probably dates from the 1990s.
  • balearicdynamics
    balearicdynamics over 9 years ago +6
    BTW... While in Spain I am organising to have a decent working developing and prototyping lab, from 3D printing to soldering station up to software development, here in the Netherlands I rent a romm"all…
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp +6
    There is never any end to the demands for more space - I have a factory unit with 1000 ft^2 and an additional 200 ft^2 for light storage above an internal ceiling. About 500 ft^2 is enclosed in an insulated…
Parents
  • jw0752
    jw0752 over 9 years ago

    Hi Rachel,

    This is a great looking shop. A while back many of the guys posted pictures of our shops and shared ideas. I went back and looked at it but it was very out of date at least in my instance. What are the blue mats that you are using on your benches?

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to jw0752

    Hi John,

     

    I've now had a chance to dig through my invoices and the blue ESD mats are from Multicomp ESD kits which I got from Farnell. Here is the link to the kit: http://uk.farnell.com/multicomp/069-0002/kit-esd-workstation-blue-0-6x1/dp/1736630

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to jw0752

    Hi John,

     

    Thats a good idea having the static strips along the front edge. I also like the glass work mat idea, very practical and as you say its impervious to solder splashes. The ESD mats are actually surprisingly resilient to heat / solder and I keep them looking clean with ESD surface cleaner (http://cpc.farnell.com/reztore/pp-3537/esd-surfacemat-cleaner/dp/TL13002) which seems to work really well.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to rachaelp

    Can't believe how neat you all are. I'm always embarrassed to show anyone the clutter on my bench.

     

    Do they still put a logo on the mats? This one probably dates from the 1990s.

     

    image

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to jc2048

    v 

     

    image

     

    I'm posting this to re-assure Jon that mess is good.

    I'm taking  a break from soldering the parts on to some boards for a 100MHz 80dB remote controlled amplifier.

    rachaelp

    I have  a cheapo Siglent spectrum analyzer which seems OK so far and according to Dave Jones the Ozzy blogger it's better than the equivalent price Rigols. I wanted one with a decent ish built in tracking oscillator and that gets a bit pricey with the TEK USB analyzers.

     

    MK

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rachaelp
    rachaelp over 9 years ago in reply to michaelkellett

    Oh that's a nice lot of kit in your lab! I see a very flash looking Lecroy scope, I can't quite zoom in enough to really make out what model it is. Is is one of the 12-bit HDO's?

     

    That's a good tip on the Siglent, I had forgotten about that one, I do remember watching Dave review that some time ago. I'll have to revisit his video and look at what their offerings are and how much they cost. I'd quite like the option to have a tracking generator too which is one thing where the Signal Hound has an advantage because the optional TG box is not too expensive to buy afterwards.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp

    The LeCroy is a WaveRunner 610Zi -  4 channels, 1GHz bandwidth, 8 bits, 10Gsamples (or 20Gs on just 2 channels) - I'm tempted by the idea of a 10 or 12 bit scope and the 610zi is paid for .... but I needed a new temperature/humidty chamber so that came first.

    Actually it is very, very seldom that I feel the need for 12 bit resolution and never (so far) at more than a few MHz so a Pico Hi Res scope might do.

    I'm expecting to do some work on a 16 bit, 8 channel, 10MHz data acquisition system later this year - so one of the prototypes might do as a high res scope.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp

    The LeCroy is a WaveRunner 610Zi -  4 channels, 1GHz bandwidth, 8 bits, 10Gsamples (or 20Gs on just 2 channels) - I'm tempted by the idea of a 10 or 12 bit scope and the 610zi is paid for .... but I needed a new temperature/humidty chamber so that came first.

    Actually it is very, very seldom that I feel the need for 12 bit resolution and never (so far) at more than a few MHz so a Pico Hi Res scope might do.

    I'm expecting to do some work on a 16 bit, 8 channel, 10MHz data acquisition system later this year - so one of the prototypes might do as a high res scope.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • rachaelp
    rachaelp over 9 years ago in reply to michaelkellett

    Very nice, I was looking at 2.5GHz one of those for the company I work for a while back (tight management wallets pushed us to a recon'd much older WavePro 7300 which wasn't nearly as capable sadly) and when I was kitting out my own lab I was trying to justify getting one of those as I love Lecroy scopes, but at the end of the day I got a 500MHz Agilent MSO with every single software add on for significantly less than Lecroy wanted for an ex-demo 1GHz WaveRunner with no options. By the time I added on Logic analyzer and all the useful software decode option licenses it was eye watering!

     

    That's a good idea re the Picoscopes, they've got some really nice bits of kit now at very reasonable prices and they do Mac/Linux software too which is a really important feature for me.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp

    I keep hoping that good scopes will get cheap - and while you do get more for your money now than 10 years ago it still seems that a nice scope costs about the same as a fairly reasonable car. Perhaps pressure from the Chinese sources will force prices down a bit. Keysight seem to often offer the option software as a bundle but LeCroy don't seem to feel the need to do that.

    Pico don't charge for decoders at all, and some of the stand alone logic analysers bundle a great mass of them in for 'free'.

     

    https://www.thedebugstore.com/lap-c-322000-logic-analyser-zeroplus.html

     

    Logic Analyzers-Zeroplus

     

    One of the modern 1GHz ZeroPlus models, 40 channels, 16M memory, 110 built in decoders is approx $3000.

     

    I have a little one of the LAP-C types and it's not bad at all - mine has limited memory so I use the LeCroy now.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down