Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog AnyCubic Mega-S - Prime Day
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 20 Jul 2019 8:28 PM Date Created
  • Views 2238 views
  • Likes 5 likes
  • Comments 20 comments
  • 3d printers
  • velleman k8200
  • anycubic
Related
Recommended

AnyCubic Mega-S - Prime Day

ralphjy
ralphjy
20 Jul 2019

After a fair amount of frustration trying to fix the hotend/extruder on my Velleman K8200 3D printer I finally decided that I should just go ahead and buy a new printer.  I really like the K8200, it has a large build area (20 x 20 x 20 cm) and has worked reliably for 6 years.  But recently I've been having lots of problems with it.  I think it started with some bad filament.  I kept getting jams in the Delrin isolator in the extruder due to expanded filament.  I replaced the isolator but that only helped a little and then I ended up with a clogged nozzle that I couldn't manage to clear.  So, I bought a new nozzle assembly and when I tried to replace the old one I realized that filament had oozed out onto the heater and created quite a mess.  I debated whether or not to buy an upgraded extruder assembly and to fix my z-axis mechanism which was wearing out.  Decided that I should look for a new printer instead.

 

I was debating whether or not it was worth it to buy a fully enclosed unit with auto-leveling.  I found that units with an equivalent build area to the K8200 were quite expensive and some used proprietary filament and/or software.  Then along came Amazon Prime Day and I saw the AnyCubic Mega-S printer for under $300 with Prime delivery.   I was a little concerned about such a low cost Chinese printer but the reviews were generally good, so I went ahead and bought it.

 

Here's the new printer next to the K8200.  It actually has a slightly bigger build area (21 x 21 x 20.5 cm) but has a smaller footprint and is about 15 cm shorter.

image

 

 

The major complaint that I've seen about this printer is that it is very noisy.  It also has loud fans in the base for the electronics.  Here's a short clip showing how noisy it is.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Here's the test print of the owl pair.  I'm satisfied with the print quality.  One concern that I have is that I now have a new tool flow.  I used to use Repetier software with a Slic3r slicer.  The recommended tool for this printer is Cura which should be fine although I haven't used it so may have a learning curve.

image

 

One feature that I really like is the Ultrabase bed.  It has stippled glass with a special coating that improves print adhesion when it's hot and print release when it is cools down.  Seems to work really well.  The bed has a little warp (higher in the center), so I'm not sure how well it will do with maximum size prints.

image

 

I'm currently using the SD card interface to print.  I'll be testing the USB interface with my Mac Mini shortly.  I'd like to use a Raspberry Pi with Octoprint but I've seen some reports of problems on the forums.  I'll try it after verifying the USB interface is working reliably.

 

The good news and hopefully not the bad news is that this printer came with a lot of extra stuff.

  1. 1kg spool of white filament
  2. 5 x 10m of different color filament samples (red, blue, green, yellow, beige)
  3. Spare print head assembly with filament tube
  4. 5 spare nozzles (0.4, 0.5, 0.6, 0.7, 0.8 mm)
  5. Spare limit switch
  6. Filament cutter
  7. Tweezers
  8. Toolkit (hex wrenches, open end wrenches, screwdriver)
  9. Nozzle cleaning rods
  10. SD card (with test print and software)
  11. USB SD card reader
  12. USB cable
  13. Print removal spatula
  14. Pair of latex gloves

 

Just hope it doesn't imply a lot of repair image

  • Sign in to reply

Top Comments

  • genebren
    genebren over 5 years ago +5
    I am in the market for a replacement printer (mine broke ). I have been looking at the AnyCubic 4MAX Pro 2.0 (quiet box). I am impressed in some of things that I am seeing on the descriptions, like the…
  • ralphjy
    ralphjy over 5 years ago in reply to neilk +4
    Hi Neil, The Mega-S has been (still is) a great utility printer. I use it on a weekly basis and it has held up well. I mainly use it to print holders, cases or adapters for my projects, so nothing fancy…
  • dougw
    dougw over 5 years ago in reply to ralphjy +4
    I have had my i3Mega for years and printed many hundreds of objects (all with PLA). I have never even had to level the bed. The bed surface is awesome at sticking when hot and releasing when it cools off…
Parents
  • genebren
    genebren over 5 years ago

    I am in the market for a replacement printer (mine broke image).  I have been looking at the AnyCubic 4MAX Pro 2.0 (quiet box).  I am impressed in some of things that I am seeing on the descriptions, like the motherboard seems to have replaceable driver modules with TMC2208 drivers.  Also a lot of the basic features seem like that are newer designs (extruder, etc.).  This seems to be a new model with little to no feedback and some good reviews, but has anyone heard anything about it?  If the experiences that you are having with the Mega-S scale up, this could be a nice printer.  Note:  The quiet part is nice as the printer sits about 3 feet from my ear (and also about the same distance from my wife's ear) and it can be quite distracting if I am really trying hard to concentrate.  Any thoughts would be greatly appreciated.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 5 years ago

    I am in the market for a replacement printer (mine broke image).  I have been looking at the AnyCubic 4MAX Pro 2.0 (quiet box).  I am impressed in some of things that I am seeing on the descriptions, like the motherboard seems to have replaceable driver modules with TMC2208 drivers.  Also a lot of the basic features seem like that are newer designs (extruder, etc.).  This seems to be a new model with little to no feedback and some good reviews, but has anyone heard anything about it?  If the experiences that you are having with the Mega-S scale up, this could be a nice printer.  Note:  The quiet part is nice as the printer sits about 3 feet from my ear (and also about the same distance from my wife's ear) and it can be quite distracting if I am really trying hard to concentrate.  Any thoughts would be greatly appreciated.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 5 years ago in reply to genebren

    The quietest printer I've tried is the Ultimaker 2. (it is enclosed) It is definitely a high quality printer, although the one I tried had a straight glass bed which is not ideal - maybe they have improved that aspect by now.

    My Anycubic is louder than Ultimaker but I am okay with it because the open frame allows easier maintenance. It can make some louder fan sounds during warmup - I am speculating the variable speed fans hit a speed that causes resonance. That loud phase may last a minute or two on warmup, but it isn't much compared to the whole print time.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to genebren

    The AnyCubic 4MAX Pro 2.0 looks like a nice printer with quite a few performance enhancements over the printer I have (not to mention the enclosed box).   If you get one I'd like to hear of your experiences.  It's not clear how they would vent fumes for printing material like ABS (one of the reasons I've never printed with ABS).

     

    The Mega-S is actually quite a noisy printer and I wouldn't want to sit next to one while it is printing.  The good news is that my computer room and work room are separate and I have a camera that I use to monitor the printer, so the noise is not an issue for me.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • neilk
    neilk over 5 years ago in reply to ralphjy

    ralphjy  wrote:

    The good news is that my computer room and work room are separate and I have a camera that I use to monitor the printer, so the noise is not an issue for me.

     

    Unfortunately, I have no option but to have the printer in the same room as my computer; it may even be 3 or 4 feet away from my ear!!

     

    Neil

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ralphjy
    ralphjy over 5 years ago in reply to neilk

    Maybe use noise canceling headphones image.  I haven’t tried that.  I do have a couple of computers in the work room to run the printer and the laser/cnc, but I don’t like being in the room when any of that equipment is operating.  I’ve got tinnitus, probably caused by being careless with hearing protection on the job.  I also don’t totally trust the laser goggles.  I usually reduce the laser intensity when I’m doing setup and use the camera to monitor for smoke/fire while it is running.

    • Cancel
    • Vote Up +4 Vote Down