Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog Genmitsu CNC 3018-PRO
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 8 Aug 2019 3:13 PM Date Created
  • Views 8948 views
  • Likes 8 likes
  • Comments 18 comments
  • genmitsu cnc 3018-pro
  • cnc router
Related
Recommended

Genmitsu CNC 3018-PRO

ralphjy
ralphjy
8 Aug 2019

I've had great success with my inexpensive AnyCubic 3D printer that I got on Amazon Prime day, so I finally decided to get myself a low cost (under $200) CNC mill. I wanted to get something that would allow me to drill holes with reasonable accuracy and also mill PCBs.   I settled on the SainSmart Genmitsu CNC 3018-PRO.  It has an XYZ working area of 300x180x45mm which is sufficient for most things that I do.  It uses GRBL rather than Mach3 control firmware but I think that should be sufficient for a beginner like me.  One reason for the low cost is this is an assemble it yourself kit.  Good news is that even with 3 trays of parts the assembly only takes about an hour or so.

 

Here's the box full of parts:

image

 

The Arduino based Controller PCB:

  • 3 driver boards and connectors on the right for the X/Y/Z stepper motors
  • Spindle motor driver and connector on the left
  • There are also connectors and circuitry for an optional laser module and display

image

 

The front view of the assembled unit:

image

 

The rear view of the assembled unit (need to finish the wire management):

image

 

GRBL Control software (Candle)

The kit comes with a mini CD with software, drivers, and test jobs.  My first application is to cut some proto PCBs to fit on top of MKR 1300 boards that I am using for my LoRaXes project, so I just need the ability to make linear cuts.  This is my first real experience with CNC and I'll need to figure out a tool flow that works for me.  I intend to use Openscad for CAD since I use that with my 3D printer and it exports DXF and SVG formats in addition to STL.  I need to figure out what to use for CAM (the equivalent to a slicer for 3D printing) to generate the GRBL GCode for the router.  The kit comes with a GRBL control program (Candle) that allows you to import and edit GCode and to visualize and control the CNC job.

image

 

For this simple job I just manually entered the GCode directly into the program.  Here is the the GCode:

(GCode for simple linear cut along Y axis)
(X=Y=Z=0 is set to surface of PCB at beginning of cut)


G90 (Use Absolute Coordinates)
G1 Z5 F500 (Move Z to 5mm with Feedrate 500mm/min)
G1 X0 Y0 (Home X and Y with Feedrate 500mm/min)
M03 S1000 (Start spindle CW with Speed 1000rpm)
G1 Y-1.0 (Move to Y -1mm with Feedrate 500mm/min)
G1 Z-0.7 F100 (Move Z to -0.7mm with Feedrate 100mm/min)
G1 Y31.0 (Move Y to 31mm with Feedrate 100mm/min)
G1 Z5 F500 (Move Z to 5mm with Feedrate 500mm/min)
M05 (Stop spindle)
G1 X0 Y0 (Home X and Y with Feedrate 500mm/min)
M30 (Terminate program)

 

I manually increase the cutting depth (line 10) for each cutting pass.  I don't think there is a "looping" construct in GCode so I'll just need to add multiple passes once I get the spindle speed and feedrate figured out for the PCB material and tool that I am using.  I copied and edited code from one of the sample jobs that was included.  I'll need to determine what the spindle speed setting is actually doing since the spec indicates 3 speeds: Spindle: 775 motor, 12V, 3000 RPM; 24V, 7000 RPM; 36V, 9000 RPM.  I don't know if the controller has a continuously variable voltage that would allow you to interpolate/extrapolate speeds (the line I copied had 1000 RPM).

 

Two things that I wish that they had provided with this kit - a decent set of clamps and some sample end mills.  I couldn't figure out how to use the "clamps" that they provided and the only routing bits they provided were "V" cutters that are suited for engraving in wood.  I couldn't figure out what type of clamp to use with the small PCB, so I 3D printed a fixture to hold it and to provide the "waste board" structure under it.  Luckily I had also salvaged some short 0.8mm end mills from somewhere in my past life.

 

Short video of first milling attempt

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply

Top Comments

  • luislabmo
    luislabmo over 7 years ago in reply to ralphjy +7
    Hello Ralph, As far as I know, to mill PCBs V solid-carbide bits are your best choice when engraving the outlines of the traces, you'll need to play a little with the dept and choosing the right bit angle…
  • genebren
    genebren over 7 years ago +6
    Ralph, I don't know if this is the same clamps that came with your CNC: These look a little wonky, but I suppose that they should work. It looks like the bolt with the wingnut slips into the t-slot and…
  • ralphjy
    ralphjy over 7 years ago in reply to fmilburn +5
    Hi Frank, This is somewhat subjective, but I think CNC milling is quite a bit more complex than 3D printing - at least for me (it could be that the slicer settings have been thoroughly wrung out, so I…
Parents
  • genebren
    genebren over 7 years ago

    Ralph,

     

    I don't know if this is the same clamps that came with your CNC:

    image

    These look a little wonky, but I suppose that they should work.  It looks like the bolt with the wingnut slips into the t-slot and the wingnut is loosely tightened.  Then the other bolt is tighten (bottoming on the plate) and providing clamping force to the work piece.  I have used the clamps that shabaz mentions above, and those work like a champ.

     

    Gene

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • genebren
    genebren over 7 years ago

    Ralph,

     

    I don't know if this is the same clamps that came with your CNC:

    image

    These look a little wonky, but I suppose that they should work.  It looks like the bolt with the wingnut slips into the t-slot and the wingnut is loosely tightened.  Then the other bolt is tighten (bottoming on the plate) and providing clamping force to the work piece.  I have used the clamps that shabaz mentions above, and those work like a champ.

     

    Gene

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • ralphjy
    ralphjy over 7 years ago in reply to genebren

    Hi Gene,

     

    Those are precisely what I got.  Wonky is a good description although they should work fine as you describe.  I guess I couldn't imagine tightening a screw down into the aluminum base.  I'll probably print some clamps like Shabaz suggested.  I was searching around for various lengths of M8 bolts and I found that 1/4-20 bolts work fine and are a lot easier to get at Home Depot image.

     

    Ralph

    • Cancel
    • Vote Up +3 Vote Down