Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog JQ6500 Standalone
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 9 Oct 2021 11:21 PM Date Created
  • Views 4671 views
  • Likes 0 likes
  • Comments 1 comment
  • 8002a audio amplifier
  • lipo battery
  • jq6500
  • flash memory
  • mp3 player
Related
Recommended

JQ6500 Standalone

ralphjy
ralphjy
9 Oct 2021

I previously wrote a post about the JQ6500 MP3 Player .

 

I wanted to build a standalone module that I could use in projects.  Some of my projects just require the ability to play one or two short audio tracks (~1-2 minutes) and the JQ6500 seems ideal for that.

 

I decided that I needed just a few functions that I could control with buttons rather than via the UART (so standalone without requiring a controller).

 

The particular module that I'm using implements an interface that allows selection of 5 different tracks using individual pushbuttons.

image

 

The JQ6500 chip has 2 ADKEY pins that allow keypad control by using a voltage divider to represent specific commands.   Only the first ADKEY pin is being used.

image

 

Resistors R9-R13 are pinned out on the module to allow track selection for the first 5 tracks.  ADKEY is also available as a header pin, so you can implement the other functions shown above by adding the appropriate resistors (these other resistors are not in the PCB layout).  Supposedly, you can control a total of 20 functions (I assume half would be on the other ADKEY pin - but I couldn't find the documentation for them).  I guess you could figure it out by trial and error if you were so inclined.

 

Here's the module I put together:

I added the Volume +/- and Play buttons.  I didn't have a 6.2Kohm resistor, so I used a 5.6K - you still get > 200 mV of separation on the divider and it seems to work fine.

image

 

The Volume buttons are double function (long press for volume up/down, short press for track increment/decrement).

 

I added a speaker and an 18650 battery.

 

 

Here's a short demo:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

I don't have a neat application yet like fmilburn - The Tin Man - Getting Started , but I'm sure that I'll find lots of use for this module.

  • Sign in to reply
Parents
  • fmilburn
    fmilburn over 5 years ago

    Nicely done!  I am going to make one too image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • fmilburn
    fmilburn over 5 years ago

    Nicely done!  I am going to make one too image