Personal Blogs
  • Community Hub
  • More
Personal Blogs
Ralph Yamamoto's Blog How to Repair a Kindle Fire HDX Due to Battery Bulging
  • Blog
  • Documents
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: ralphjy
  • Date Created: 20 Sep 2022 5:24 AM Date Created
  • Views 3242 views
  • Likes 11 likes
  • Comments 8 comments
  • kindle fire hdx
  • amazon kindle
  • swollen battery
Related
Recommended

How to Repair a Kindle Fire HDX Due to Battery Bulging

ralphjy
ralphjy
20 Sep 2022

I bought a 7" Amazon Kindle Fire HDX when it first came out in November 2013.  It's claim to fame was its high resolution 1920x1200 color display.  I've been using it pretty much daily since then for an hour or two for videos and puzzles.  Recently I've noticed the back of the case bulging and this morning I saw that the screen had started to separate from the case.

image

image

The unit itself is still working, but I think the mechanical stress will probably damage it soon.  I'm going to stop using it until I figure out whether I want to try installing a new battery.  I saw a video on YouTube that made the battery replacement look super simple, but I realized that it was for an HD unit not an HDX.  The HDX disassembly is quite a bit more complex.

All the replacement batteries that I've seen are made in China, I haven't figured out a good source.  

Here's one from Walmart for $18.59 (ships from California)

image

And one from batteryship.com in Wyoming for $35.60.  This one has positive reviews and also comes with tools.  Looks like the same battery that is sold on Amazon.

https://www.batteryship.com/htmlos/htmlos.cgi/batteryship/catalog.html?item=58-000043&model=Kindle+Fire+HDX+7+2013

Or I can buy one from Amazon for under $30 (Chinese brands, no tools, not Prime).

image

I guess I shouldn't complain as the tablet has worked well for 9 years.  I will probably try to fix it as I like the high resolution display which isn't available anymore.  The current resolution on the 7" and 8" Fire HD tablets is 1280x800.

I'll try to document the repair when I get around to doing it.

  • Sign in to reply
Parents
  • rsjawale24
    rsjawale24 over 4 years ago

    Do not keep it inside the device for long. Get it changed as soon as possible it might expand further and crack the screen or explode. Better to replace it at the earliest

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • rsjawale24
    rsjawale24 over 4 years ago

    Do not keep it inside the device for long. Get it changed as soon as possible it might expand further and crack the screen or explode. Better to replace it at the earliest