G'Day,
How can the following opto-isolator circuit output be used?
I purchased (on sale) a number of 4 channel opto-isolator modules from a Asian manufacture. I made the buy without due diligence on my part. The circuit works but there doesn't appear to be a way to use the existing connection as an output to do work.
There are four physical connection points on terminal strips. IN1 & G on the left are two physical connection points and V1 & G are the other two physical connections shown on the right. Assuming IN1 & G on left are input and V1&G on right are output, there doesn't appear to be a connection point on the output to do actual work.
In my haste to purchase such a great sales deal, I failed to realize there is no external connection on the south side of the 3K resistor. If V1 is supply and G is ground, then where is the output connection?
I do have a few electronic marbles rolling around in my head from post secondary education. That knowledge provides me no solution to how I get output from this circuit to do work without adding an additional physical connection. That is hard given the board uses surfaces mount components and very little space to make solder connections. I did make a connection to the south side of the resistor to test operation and it worked.
If someone has a suggestion on how to use the circuit without modification, I would appreciate it. Other wise the great sales deal was a bust.
Sean