Documents Comparison of SBCs in the market.
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 13 Apr 2016 5:58 AM Date Created
  • Last Updated Last Updated: 6 Oct 2021 8:49 PM
  • Views 1267 views
  • Likes 4 likes
  • Comments 6 comments
Related
Recommended

Comparison of SBCs in the market.

Sr NO

Name

Price  (in USD)

Open Source(Y/N)

Processor with Clock Speed

RAM

GPU

GPIO

Onboard Storage

Expandable Storage

Community

Support(on a scale of1 to 10)

Ethernet

WiFi

Bluetooth

GPS

Misc

1

Raspberry Pi 3 Model B

35.00

Y

Broadcom BCM2837(4× ARM Cortex-A53, 1.2GHz)

1GB LPDDR2 (900 MHz)

Broadcom VideoCore IV

40-pin header, populated

No

32GB

10/10

10/100 Ethernet

Broadcom BCM43438 chip provides 2.4GHz 802.11n wireless LAN

Bluetooth Low Energy, and Bluetooth 4.1 Classic radio support

No

2

Raspberry Pi Zero

5.00

Broadcom BCM2835

1 GHz ARM1176JZF-S single-core

512MB of LPDDR2 SDRAM

unpopulated 40-pin GPIO headernonononono

3

Raspberry Pi 2Model B

Broadcom BCM2836

900 MHz quad-core ARM Cortex-A7

4

Raspberry Pi 1Model B+

Broadcom BCM2835

700 MHz single-core ARM1176JZF-S

5

Raspberry Pi 1Model B

Broadcom BCM2835

700 MHz single-core ARM1176JZF-S

6

Raspberry Pi 1Model A+

Broadcom BCM2835

700 MHz single-core ARM1176JZF-S

7

Raspberry Pi 1Model A

Broadcom BCM2835

700 MHz single-core ARM1176JZF-S

8

ACME Systems Arietta G2514.00

Atmel AT91SAM9G15

ARM9 @ 400MHz

128MB/256MB of DDR2Unpopulated 40-pin header provides access to USB, UART, I2C, SPI, PWM, ADCC and SSC/I2S.noYes via MicroSDnoYes via add on cardnonoSerial Debug Port Header

9

Pine A64+ 2GB

 

http://wiki.pine64.org/index.php/Main_Page

29.00Y

Allwinner A64 SoC

Quad-core ARM Cortex A53

1.2 GHz

 

http://tinyurl.com/jx7z97y

2GB DDR3

Dual-core Mali-400 MP2

500MHz

GPIO: 46 dedicated

NoneVariety such as MicroSDForums; Time will tell (kick-start)10/100/1000on USD USD 10.00 daughter cardon USD USD 10.00 daughter cardPlanned daughter card

Other interfaces:

UART: 3;

i2c bus: 2;

SPI bus: 2;

IR receiver;

Audio 3.5mm mini-jack;

CSI-Camera;

DSI-LCD Panel;

10

11

12

13

14

15

16

17

18

19

20

  • sbc
  • diy
  • raspberrypi
  • comaprision
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 10 years ago in reply to spannerspencer +1
    Thanks. Have created it as a followup to the poll on best SBCs in the market. Would love for more and more people to collaborate on this and make it helpful for the community.
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to e14 Contributor +1
    I would not be filling it. Its for everyone to fill. I am not an expert regarding SBCs and hence the poll and this doc. Would be helpful if you can do it for us. Please improve upon is as you fell is helpful…
Parents
  • spannerspencer
    spannerspencer over 10 years ago

    Good start. Keep going -- this could be REALLY useful! If you can get it populated we'll take a look at promoting it across the Community  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to spannerspencer

    Thanks. Have created it as a followup to the poll on best SBCs in the market. Would love for more and more people to collaborate on this and make it helpful for the community.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to spannerspencer

    Thanks. Have created it as a followup to the poll on best SBCs in the market. Would love for more and more people to collaborate on this and make it helpful for the community.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • spannerspencer
    spannerspencer over 10 years ago in reply to e14 Contributor

    Ah yes! I've added the poll to that page's featured content, and also shared it into the Single-Board Computers and Members sections image

     

    And I've voted for my own fave image