Polls 6502 or Z80 Which Is Better?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: timswift
  • Date Created: 15 Nov 2016 5:03 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:57 PM
  • Views 4367 views
  • Likes 1 like
  • Comments 11 comments
Related
Recommended

6502 or Z80 Which Is Better?

I have seen lots of discussions on the 6502 and the Z80 microprocessors so I thought I would start this poll.

And be sure to comment on why you voted for the ------ processor!

  • microprocessor
  • z80
  • 6502
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 9 years ago +7
    Better is a dodgy word in this context. My favorite processor of that era was the Motorola 6809 - in many ways way ahead of it's time. The 6502 was nice and in many ways much easier to code effectively…
  • jc2048
    jc2048 over 9 years ago +5
    I voted for the 6502 because it was the first microprocessor I ever owned. I was a student back in the mid seventies, but couldn't afford any of the processors that were then on offer (the various Intel…
  • e14 Contributor
    e14 Contributor over 10 years ago +4
    timswift "Better" is open to a wide set of interpretations. The Z80 was had more CPU functions than the MOS Tech 6502 although the 6502 enjoyed more success at the time because of Apple, Acorn, and Atari…
Parents
  • COMPACT
    COMPACT over 8 years ago

    I've used many old MPUs ranging from COP1802, 2560 SCMP, Z80, 8080, 68xx, 6502 and derivatives (and the list goes on...)

     

    The Z80 and 6502 can't really be compared against each other because of their disparate features.

     

    Here are some aspects;

     

    You can't directly compare clock speeds against each other because the timing of the CPUs differ relative from their system clocks.

     

    The Z80 has many inbuilt registers allowing it to operate without any external RAM whereas the R6502 is dependent upon external RAM at page 0 (0000-00FF) but this RAM at page 0 has special instructions that make extremely versatile.

     

    The Z80 has I/O port addressing which does not consume precious memory space.

     

    The Z80 has inbuilt DRAM refresh circuitry but this is also can be a hinderance.

     

    The Z80 handles the DAA instruction different to the Intel 8080. - It basically corrected it.  This instruction is often used to sense whether an 8080 or Z80 is present.

     

    Z80 peripherals have a daisy chained interrupt priority scheme.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 8 years ago

    I've used many old MPUs ranging from COP1802, 2560 SCMP, Z80, 8080, 68xx, 6502 and derivatives (and the list goes on...)

     

    The Z80 and 6502 can't really be compared against each other because of their disparate features.

     

    Here are some aspects;

     

    You can't directly compare clock speeds against each other because the timing of the CPUs differ relative from their system clocks.

     

    The Z80 has many inbuilt registers allowing it to operate without any external RAM whereas the R6502 is dependent upon external RAM at page 0 (0000-00FF) but this RAM at page 0 has special instructions that make extremely versatile.

     

    The Z80 has I/O port addressing which does not consume precious memory space.

     

    The Z80 has inbuilt DRAM refresh circuitry but this is also can be a hinderance.

     

    The Z80 handles the DAA instruction different to the Intel 8080. - It basically corrected it.  This instruction is often used to sense whether an 8080 or Z80 is present.

     

    Z80 peripherals have a daisy chained interrupt priority scheme.

    • Cancel
    • Vote Up +3 Vote Down