Polls Re-Entering Old Projects In Project14 Contests
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dougw
  • Date Created: 4 Jan 2018 3:48 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 2573 views
  • Likes 1 like
  • Comments 25 comments
Related
Recommended

Re-Entering Old Projects In Project14 Contests

The question is pretty simple - Should old projects be eligible for Project14 contests if they have already been entered in previous contests?

Personally I see no reason why not but others may and probably do have different opinions.

If projects are re-entered they may suffer a natural penalty in judgments.

I expect some of the Project14 topics to recur, especially the popular ones, and members may want to tweak their old designs and re-enter.

And some projects may have been entered as a poor fit to a topic, but a more appropriate Project14 topic comes up later.

I realize there is more than one question to answer in the poll, but only one check box, so feel free to add comments.

This poll is really an experiment to see if I can embed this poll in an appropriate place, but the content may be interesting as well.

  • project recycling
  • project14 re-use
  • project re-enter
  • project14 topics
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • Jan Cumps
    Jan Cumps over 8 years ago in reply to Robert Peter Oakes +7
    Robert Peter Oakes wrote: I ran a contest at the end of last year on Hackster.io and I can tell you, it is very hard to determine what deserves to win and what does not even qualify, this was with a prize…
  • tariq.ahmad
    tariq.ahmad over 8 years ago +7
    I've sorta evolved my thinking on this topic since the program got started. One of the challenges in the beginning was not knowing what was going to work and what wasn't. The more ideas and projects that…
  • beacon_dave
    beacon_dave over 8 years ago in reply to gadget.iom +6
    That reminds me of the 70's/80's TV show 'The Great Egg Race' which was hosted by the late Prof Heinz Wolff, where if I recall correctly the scoring system was based upon " design ", " courage " and "…
Parents
  • beacon_dave
    beacon_dave over 8 years ago

    This issue perhaps could get complex for microcontroller-centric type projects as the hardware design between two project entries could be almost identical e.g. a microcontroller, a display panel, some sensors/actuators and a 3D printed enclosure, making them physically look the same, however even subtle changes in the programming side could completely change the behaviour of the system as a whole.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • beacon_dave
    beacon_dave over 8 years ago

    This issue perhaps could get complex for microcontroller-centric type projects as the hardware design between two project entries could be almost identical e.g. a microcontroller, a display panel, some sensors/actuators and a 3D printed enclosure, making them physically look the same, however even subtle changes in the programming side could completely change the behaviour of the system as a whole.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • dougw
    dougw over 8 years ago in reply to beacon_dave

    Microcontrollers are such general purpose building blocks, they can often be re-purposed in multiple projects, and it is an excellent strategy to design them as a general platform specifically so the IP can be re-used - minimizing future development costs and schedules. This is really important in short projects like Project14 where the member also must foot the bill. Re-use of, and expansion of, previous work will allow more complex projects to be completed within the time available. Designing a microcontroller card from scratch for a one-off Project14 is going to be a rare occurrence.

    • Cancel
    • Vote Up +3 Vote Down