Polls Z80 Vs. 6502 (POLL)
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: electrorubixtech
  • Date Created: 4 Feb 2018 1:28 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 1396 views
  • Likes 1 like
  • Comments 15 comments
Related
Recommended

Z80 Vs. 6502 (POLL)

Z80 and 6502 really popular cpus butf which one is better in support, availability and ease of use things i want to make both of them can handle but the availability and the documentation is the important part for me

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • DAB
    DAB over 8 years ago in reply to electrorubixtech +5
    Yes, but the differences in the architecture also means that the tools and learning curve is different for both processors. I will admit, I have no idea how the current development tools are to use. What…
  • DAB
    DAB over 8 years ago +4
    I have used both processors. They have different types of architectures, so you really cannot compare the two until you establish your project requirements. Each architecture has advantages depending upon…
  • mistermagoo
    mistermagoo over 8 years ago +2
    If I'm not mistaken, the TI-83 and up uses/used an instruction set based on, if not similar to, the Z-80's.
Parents
  • dang74
    dang74 over 5 years ago

    I have a soft spot for the 6502 because it and its variants were in my favourite computers and gaming consoles from when I was growing up, and I've used it for 'home projects'.  However, the 6502 is hard to interface with because it is not very generous with its data and address hold times on writes.  I think it's read/write direction bit hold timing is the same as its data/address hold timing.  I have not dug too deeply into the Z80 but it's prevalence in early 80s arcade boards suggests to me that it is easier to work with as far as hardware design goes.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • dang74
    dang74 over 5 years ago

    I have a soft spot for the 6502 because it and its variants were in my favourite computers and gaming consoles from when I was growing up, and I've used it for 'home projects'.  However, the 6502 is hard to interface with because it is not very generous with its data and address hold times on writes.  I think it's read/write direction bit hold timing is the same as its data/address hold timing.  I have not dug too deeply into the Z80 but it's prevalence in early 80s arcade boards suggests to me that it is easier to work with as far as hardware design goes.