Polls Feedback Desired: What Application first Comes To Mind from the Term "High Voltage Op Amps"?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: rscasny
  • Date Created: 20 Jun 2018 3:33 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 2:58 PM
  • Views 1292 views
  • Likes 1 like
  • Comments 17 comments
Related
Recommended

Feedback Desired: What Application first Comes To Mind from the Term "High Voltage Op Amps"?

I am working on another project regard High Voltage Op Amps. I wanted to get member input regarding High voltage Op Amp applications.

 

Here's my question:

 

When you hear the term "High Voltage Op Amps" what's the first application that comes to mind for you from the list below?

 

I realize that High Voltage Op Amps can be used in a variety of applications. But I wanted to get your input on the main one that comes to mind for you. Granted, I'm asking something subjective. If you prefer to comment below, that's fine.

 

Thanks.

 

Randall

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dougw
    dougw over 8 years ago +6
    What do you consider high voltage? Most op-amps used to run off +- 15V or +-18V so I think of high voltage op-amps as anything over 36 volts.
  • rscasny
    rscasny over 8 years ago in reply to dougw +6
    Good question. I was thinking about the same as you: over 36V. But the person I am working with defines it as over 27V. Randall
  • DAB
    DAB over 8 years ago +5
    High power to me is in the Kwatt range, so I am thinking >1000 volts. I would envision that these types of opamps would be used in Audio amps, long distant RC apps, motor controls, induction heating, and…
  • jc2048
    jc2048 over 8 years ago in reply to michaelkellett

    That's a very nice amplifier. Up to 100MHz it's really good - bit iffy from there upwards where you'd have to be very careful of what was being driven. Not one for people who like using autorouters, though, is it?

     

    I just wish someone would invent a package where the thermal pad extended a little way from the ends (like larger SMD power transistors do) - that way you could just solder them with a big iron and not have all the bother of the SMD stuff and whether or not the pad had soldered properly (I think I'm getting to be a bit of a dinosaur now).

     

    TI seem to be describing +/-15V devices as "High Voltage" now,

    This is what their op-amp product page says (>6V!)

     

    image

     

    Analog Devices aim a bit higher with 12V

     

    image

     

    Instead of the 6V parts being 'low voltage', it looks like they're becoming the new normal and everything else is high voltage.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to michaelkellett

    Here's a nice High(ish) voltage amplifier:

     

    THS3491 900-MHz, High Power Output, Current Feedback Amplifier | TI.com

     

    TI seem to be describing +/-15V devices as "High Voltage" now, this device is pretty amazing in that it can deliver +/-10V at serious current at 100MHz.

    The example application on the first page of the data sheet would suit Shabaz' DDS signal generator quite well.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to jc2048

    I wasn't serious about the "off topic" comment - all the best stuff is off topic image

     

    Op amps don't have to be monolithic in my book.

     

    MK

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to michaelkellett

    Yes, it's an interesting app note - I read it through before saying anything. My comment was meant as a serious question of definition that I thought snidhi might like to consider.

     

    The output can only drive positive and the negative slew is defined entirely by the output capacitor discharging through the load, as is the case with most power supplies. The claimed bandwidth is something like 50Hz, which also seems to place it with power supplies.

     

    The Apex parts that Doug refers to above are hybrid circuits (not surprising for amplifiers that can handle 1000 or 2000 volts). Would they also be off topic? Does it have to be monolithic to be an 'op amp'?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 8 years ago in reply to michaelkellett

    yea, right. It is quite fun to read though

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 8 years ago in reply to jc2048

    No, but it's off topic since it doesn't actually use a high voltage op amp . It comes form a rather nifty National Semiconductors app note (now TI of course , at http://www.ti.com/lit/an/snoa600b/snoa600b.pdf ).

    The LM3524 is a switcher regulator and the complete design is claimed to manage 1000V at 300mA.

     

    It's a fun app note which I would never have spotted without s nidhi's quote of it, so thanks.

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jc2048
    jc2048 over 8 years ago in reply to snidhi

    Isn't that a power supply?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • snidhi
    snidhi over 8 years ago

    1000V  Son of Godzilla Booster image

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • colporteur
    colporteur over 8 years ago

    My thoughts are division of power through isolation. Two or more sides with different power requirements but have ability to pass signals.

     

    The high voltage part triggers visions of levels only seen with vacuum tubes. Since I lived in the first era of tubes and been physically shocked by the levels, I tend to smile when I see 5KV isolation across the gap. Yeah, I've seen that! No it wasn't 5KV that work me up, only 350VDC.

     

    Sean 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • NigelB
    NigelB over 8 years ago

    Good Question... Most of the designs I do are 24V and below (and of that, mostly 5V and below) , yet I would consider +-15V rail op-amps as fairly standard in circuits of old.

     

    So applications for high voltage optical circuits or relatively high impedance ceramic resonators for imaging in medical research (high voltage, mainly low current applications) would be the only place where I would have used more esoteric/unusual devices in my career - and that was into the hundreds of volts at the most rather than over the 1kV in the case of the optical switches...

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
>