Polls How do you handle jumper cables?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 18 Mar 2020 11:44 AM Date Created
  • Last Updated Last Updated: 28 Mar 2020 10:41 PM
  • Views 1740 views
  • Likes 1 like
  • Comments 12 comments
Related
Recommended

How do you handle jumper cables?

In light of Making 0.1" Jumper Cables - Crimp Tools Tested  how do you handle cables that you need ? - be sure to check out Round-Up and Review - Projects, News and Polls

  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 6 years ago +5
    I made these, since they're unobtanium, but quite useful I think! They are chained jumper cables, with a pin on the end, but also a socket! That way it is possible to do two things easily: 1. connect to…
  • cstanton
    cstanton over 6 years ago in reply to Gough Lui +5
    So long as you don't say 'with my sharp, pointy teeth' like the Killer Rabbit of Caerbannog .
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to ntewinkel +4
    I do that too: use a breadboard like the patch bay in an audio studio.
  • cstanton
    cstanton over 6 years ago in reply to Gough Lui

    So long as you don't say 'with my sharp, pointy teeth' like the Killer Rabbit of Caerbannog.

     

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago in reply to Gough Lui

    I'm glad you were able to resist.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Gough Lui
    Gough Lui over 6 years ago

    I was so tempted to say "with my bare hands ..."

     

    - Gough

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dubbie
    dubbie over 6 years ago

    I used to make my few jumper cables last for a long time, moving them from project to project, but then I made the LDR camera (LDR Camera #8 : Fully Working Camera ) and needed many many jumper wires. So I bought loads and found it very useful having plenty of each type (plug - plug, socket - socket and plug - socket) so now if I run out I just buy a load more. I sometimes cut the plug/socket off and solder the wire directly to the PCB as I did for the NanoRama Rocket (Nano Rocket #1 : Hand Thrown with TTL Serial Communications ) as this means I can easily make and unmake connections, make longer connections when testing and then have short connections when the project is in use.

     

    Dubbie

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 6 years ago

    I was looking for the "Sticks of Arduino" voting option.

     

    Reference:

    https://www.reddit.com/r/arduino/comments/9ji18p/honey_i_found_a_stick_of_arduino_on_the_ground_i/

     

    - W.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jw0752
    jw0752 over 6 years ago

    I like to use high strand wire and solder it to gold plate pins from a header. A little heat shrink and it is ready to go. The high strand wire makes the jumper very flexible and durable with high current capabilities. As usual shabaz  has a great idea for added flexibility. I will have to make up a few of those. I also have made up a bunch of cords with a pin on one end and an alligator clip on the other for hooking up to things that do not easily integrate with the bread board.

     

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to ntewinkel

    I do that too: use a breadboard like the patch bay in an audio studio.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • ntewinkel
    ntewinkel over 6 years ago in reply to shabaz

    That's a great idea, Shabaz!

    I often want to do a quick mockup with just a few bits, only to find I need a breadboard to accommodate extra connections. Especially when it comes to VCC and GND connections!

     

    I might have to do something similar to what you did, maybe with triple ends for the power rails...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shabaz
    shabaz over 6 years ago

    I made these, since they're unobtanium, but quite useful I think!

    They are chained jumper cables, with a pin on the end, but also a socket! That way it is possible to do two things easily:

     

    1. connect to a board with either a pin or a socket : ) without having to search for another cable

    2. If there are two existing boards connected to each other with an existing jumper cable (pin or socket, it doesn't matter), I can use this chained jumper cable to get a tap off the connection, by temporarily unplugging one of the boards, and putting the jumper cable into the pin or the socket, and then putting the other connector onto the board. In other words, the boards still have an electrical connection and yet I've got a tapped off connection too. Hope that makes sense to follow..

     

    I'm finding such a cable useful with the DIY Logic Analyzer and Protocol Tester – L.I.S.A.!  (would also be useful with a 'salae logic' type device).

     

    The only downside, in scenario (1) is that the pins may touch since they are bare, but careful positioning works fine (or could use sleeving over it, but it's maybe overkill).

     

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kmikemoo
    kmikemoo over 6 years ago

    Right now, I buy.  There will come a time where I am rolling my own.  I make my own network cables.  Why not "right size" my jumpers?  Besides... I could double my short jumpers in a pinch. image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>