Polls Should we hide ratings?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: cstanton
  • Date Created: 21 Jun 2021 10:04 AM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:00 PM
  • Views 1859 views
  • Likes 2 likes
  • Comments 12 comments
Related
Recommended

Should we hide ratings?

You may have seen these on blogs/documents/content:

 

image

 

It allows you to rate the content on a scale of 1-5 out of stars.

 

I've heard good and bad reasons for keeping these (publicly) viewable and I'm looking into how we can do something about it. A lot of websites or social media sites simply allow you to 'like' content, or not and don't use a rating system like this.

 

It's partly a relic of the content management system that we use, Jive, but it's also something I'm concerned about for the next platform we use.

 

So let's have a decider.

  • community survey
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • dubbie
    dubbie over 5 years ago +10
    At present the rating system does not seem to have any accountable purpose. I used to be rated on a similar system at work, (1 to 5 in numbers rather than stars, but it is essentially the same). If you…
  • fmilburn
    fmilburn over 5 years ago +10
    I don’t find them useful and try to ignore them. The star ratings on most posts are statistically insignificant. For example, my last roadtest received only three ratings which is too few to accurately…
  • beacon_dave
    beacon_dave over 5 years ago +6
    I seem to recall that star ratings tend to be used in the Essentials quizzes, e.g. 'give a star rating' to earn the badge, so removing them completely may need some changes there.
Parents
  • dougw
    dougw over 5 years ago

    This forum benefits from being multifaceted. There are many aspects of the forum that only appeal to or get traction with a subset of members.

    All the tracking information is used differently by different members, so it is not accurate to assume that the count of Helpfuls means the same as if everyone used the same criteria for clicking on it. (Likes, Helpfuls, comments and star rating, etc are all exercised with different criteria by different members) Members may or may not find meaning in the numbers, and if they do, it may not be the same meaning, but it all adds to the richness of the forum.

    If the forum only catered to aspects that every member liked, it would probably appeal less to everyone, and it might have no aspects left at all. Caution should be exercised when contemplating a reduction in scope and features of the forum.

    I have seen star ratings on other sites that automatically ask for a reason why a particular star rating was awarded as soon as you click on a rating.

    I am aware of the arguments regarding the star feature and I am still not a big fan of losing the feature.  I have to say that the attention it has drawn has encouraged me use it more than I did before.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • cstanton
    cstanton over 5 years ago in reply to dougw

    On Jive, when you do rate, it does then suggest 'do you want to leave a review?' which then associates the rating with the comment that's made, and as an admin at least I can then see the rating associated with the comment on the top right of the comment. Not many people use that functionality, or it wasn't obvious at least that this's how it would behave. I can see the pro's to a 'here's a rating, and that's an overview of the comment you're about to read'.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • cstanton
    cstanton over 5 years ago in reply to dougw

    On Jive, when you do rate, it does then suggest 'do you want to leave a review?' which then associates the rating with the comment that's made, and as an admin at least I can then see the rating associated with the comment on the top right of the comment. Not many people use that functionality, or it wasn't obvious at least that this's how it would behave. I can see the pro's to a 'here's a rating, and that's an overview of the comment you're about to read'.

    • Cancel
    • Vote Up +4 Vote Down