Polls What tool or technology do you reach for most often as an engineer?
  • Blog
  • Forum
  • Documents
  • Quiz
  • Events
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Community Hub to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: bluescreen
  • Date Created: 29 Apr 2014 5:45 PM Date Created
  • Last Updated Last Updated: 11 Oct 2021 3:01 PM
  • Views 5538 views
  • Likes 1 like
  • Comments 83 comments
Related
Recommended

What tool or technology do you reach for most often as an engineer?

Tell us what tool, technology, or instrument you reach for most often in your engineering work.

 

(And don't forget to click the Vote button at the bottom to make it count!)

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • johnbeetem
    johnbeetem over 12 years ago +2
    The notebook. I use those granite composition books which you can buy for US$1 or so during annual back-to-school sales. Ideas get sketched in the notebook long before they're typed in, and it's a great…
  • michaelkellett
    michaelkellett over 12 years ago in reply to jw0752 +2
    Hello John, Go for the temperature controlled iron for anything/everything. The Ersa one I mentioned is very nice but a bit pricey - I've used a few cheapo ones and they have been OK. I prototype on pcbs…
  • michaelwylie
    michaelwylie over 12 years ago +1
    Multimeter hands down. Most frequent problem is no power, and the multimeter is key for troubleshooting power issues.
Parents
  • michaelkellett
    michaelkellett over 12 years ago

    Being very literal about it I suppose the most commonly used tool is the bench power supply, I have at least 10 but the one I use most is Thurlby TS3021S - 0-30V, 2A, lcd digital meters for current and volts, when the output switch is in the off position the current meter shows the current limit setting.

    I don't count the notebook as  a tool but I use one all the time, I use the PC a lot as well but that's pretty much universal so not interesting.

    Between scope and DMM  - hard to say but if I had to give up one it would be the DMM because the scope can stand in better for it than it can for the scope (mind you the scope is useless as a continuity tester).

    How about changing the power supply picture for a bench supply and then I'll vote for that image

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett

    Add glasses and a magnifying glass for us ... these are becoming necessary tools.

     

    Mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to mcb1

    I never realized how true this was. I'm only 32, and I cannot see small things easily anymore.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelwylie

    Michael Wylie wrote:

     

    I never realized how true this was. I'm only 32, and I cannot see small things easily anymore.

    I can still see the small things, I've just got to the point that by the time they're at the right distance to be able to read the markings I can't focus on them. Large illuminated magnifier is the best thing I've ever bought image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to michaelwylie

    Michael Wylie wrote:

     

    I never realized how true this was. I'm only 32, and I cannot see small things easily anymore.

    I can still see the small things, I've just got to the point that by the time they're at the right distance to be able to read the markings I can't focus on them. Large illuminated magnifier is the best thing I've ever bought image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mcb1
    mcb1 over 12 years ago in reply to e14 Contributor

    You know you need glasses when you have to put the menu on the ground to read it.

    Problem is the font is now too small to read.

     

    We have issues with monitors and the distance they are, sometimes it suits, sometimes it doesn't, and since there are 22 mostly in a line, it's hard to move all of them.

    And no you can't just make the picture bigger, most are fixed size due to the application.

     

    Mark