Arduino Projects
  • Products
  • Arduino
  • Arduino Projects
  • More
  • Cancel
Arduino Projects
Blog 2. AardEnergy – Set Up Uno and Due
  • Blog
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • More
  • Cancel
  • New
Join Arduino Projects to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: peterjcs23
  • Date Created: 26 Nov 2015 11:57 AM Date Created
  • Views 3590 views
  • Likes 4 likes
  • Comments 20 comments
  • debug
  • setup
  • meter
  • due
  • uno
  • energy
  • arduino
Related
Recommended

2. AardEnergy – Set Up Uno and Due

peterjcs23
peterjcs23
26 Nov 2015

In this Blog

Download the Arduino software and power up the Uno and Due. Look at debug, does it exist from the Arduino GUI?

See previous Blog…

http://www.element14.com/community/groups/arduino/blog/2015/11/23/1-aardenergy-kick-off--a-new-project

IDE Download

IDE Down load from Uno board page, version 1.6.6 (I had already installed 1.6.5, so an upgrade). 1.6.5 uninstalled first, 1.6.6 now in place.

image

However, under Tools>Board…Due is not listed.

Get Started with Uno

Use the IDE, Help>Getting Started.

  • Plug USB into socket on Uno
  • Power LED is on (and port  LED is blinking)
  • In Windows Device manager select Ports and find Arduino Uno (COM3) (note Windows 8.1)
  • Right click and update driver from C:\Program Files (x86)\Arduino\drivers
  • Open Blink in IDE File > Examples >01.Basics > Blink
  • Select board as Uno
  • Select Serial Port (COM3 as determined above)
  • Upload, TX, RX LEDs flash happily.
  • And LED on pin 13 is flashing, so all good.

That went well but the Due was not listed so let’s try that from the link above.

Get Started with Due

Due board needs a micro B USB cable. Order this one:

http://www.amazon.co.uk/dp/B00FAAGNLU/ref=pe_385721_37986871_TE_item

The cable has arrived and fits the board programmer port (and it fits the Native USB port). The Due powers up, Green LED is on and the yellow LED blinks.

There are some special factors to keep in mind with the Due, read the guide:

https://www.arduino.cc/en/Guide/ArduinoDue

Follow the guidance on the drivers:

(Note that is says “tested on Windows XP and, but we are using 8.1)

From Device Manager>Ports, Arduino Due Programming Port is COM4. Right Click and Update Driver Software. Browse to C:\Program Files (x86)\Arduino\drivers. Hit Next and drivers are up to date.

Also load the core software to support the Due:

From Tools>Board>Boards Manager

image

Install the SAM board ARM Cortex-M3

The Due can now be selected from the list of boards.

image

Test the set up by loading the Blink programme:

  • Open Blink in IDE File > Examples >01.Basics > Blink
  • Select board as Due
  • Select Serial Port (COM4 as determined above)
  • Upload, TX, RX LEDs flash happily.
  • And yellow LED is flashing, so all good.

Software Debug

I am curious about how to debug the software, is there a Debug Mode or JTAG port? There is nothing on the GUI as far as I can tell at the moment. A Search for Arduino Uno Debug threw up a discussion on element14:

http://www.element14.com/community/thread/17697/l/debugging-atmega328?displayFullThread=true

Looks like print on the serial port is the Arduino “debug” unless you add some other utility. In essence a Uno Sketch needs to be simple to get away with no debug tool. This also might help:

http://www.element14.com/community/groups/arduino/blog/2012/09/30/the-first-practical-arduino-debugger

On the Due there is a Debug connector marked up but is not described in the top level Arduino document. A search throws up comments about the port as JTAG but used with third party tools:

http://forum.arduino.cc/index.php?topic=134907.0

So as a challenge I’ll attempt to use Arduino GUI and see how far I get with a fairly ambitious project to do real time calculations using Due board!

Other Blogs:

1. AardEnergy – Kick Off - a new project

3. AardEnergy – Current and Voltage Transformers

 

Next Steps

After a bit more shopping I have a Current Transformer and a Voltage Transformer to evaluate. In the next blog there will be some analysis of the signals from these sensors as well as some measurements to assess performance. That should lead on to a design for the Uno and the Due interface. The plan is to use a metering chip with the Uno and to a use direct analog input to the Due.

 

These are the sensors:

image

And, here is the ARDUINO MEGA, REV 3 Farnell 2285197 prototype board, which appears to be compatible with the Due.

image

  • Sign in to reply

Top Comments

  • peterjcs23
    peterjcs23 over 10 years ago in reply to mcb1 +2
    I am limiting the scope of my blog to this set up: All other connections, that in any way access live cabling, are out of scope for an essentially home hobby style project. The content of your blog goes…
  • mcb1
    mcb1 over 10 years ago in reply to peterjcs23 +1
    That is the insulated and armoured service cable into the house If that were true you wouldn't be able to get the clamp around it, and secondly you wouldn't get any current reading. I used to deal with…
  • peterjcs23
    peterjcs23 over 10 years ago in reply to peterjcs23 +1
    The service feed into the house is an armoured cable and the live and neutral tails are terminated in the meter. The CT is on the live tail, the insulation on the live wire is reinforced so meets the same…
  • mcb1
    mcb1 over 10 years ago in reply to Robert Peter Oakes

    Does anyone know of a person where the ELCB saved their life

    No without looking ....

     

    They have got much better, and the false tripping of the past has been eliminated.

    In the 12 years we have been here, I haven't had one trip (we have 4 ... three phase plus one for wet areas)

     

    Considering they trip in less than 20mS, its only a single cycle, so you may hardly know it.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mcb1

    Just as a matter of interest, Does anyone know of a persone where the ELCB saved there life, dont get me wrong, there a good thing, I just dont know anyone that was about to be electrocuted where the ELCB tripped and prevented it and im not about to stick my finger in the socket to try it out, the last time I zapped myself was about 20 or 30 years ago and these where not very popular back then

     

    Anyone ???

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to mcb1

    Ah, that explains why it is still in my head, I was re-reading that a few days ago image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 10 years ago in reply to Robert Peter Oakes

    attaching the CT to the neutral (Low voltage side) would technically be much safer in a fault condition

    That's exactly what we did with our current monitor loops.

     

    I'm certain there is little chance of a problem with the actual CT.

    Passing a non mains rated cable out of the switchboard to a low voltage device that is floating is where I cringe.

     

    Luckily in NZ we have been forced to fit ELCB's (Earth Leakage Circuit Breakers) on nearly all the circuits for the last 12 years.

    It does offer some protection, but is really a backstop in case the primary protection mechanism fails.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 10 years ago in reply to peterjcs23

    A minor point but attaching the CT to the neutral (Low voltage side) would technically be much safer in a fault condition as in many countries this is effectivly ground also, it certainly is in America and Canada and excluding fault conditions it will read the same current anyway

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>