A 4DOF Keyestudio KS0198X robotic arm trained in simulation using reinforcement learning to reach a target, and transferred via serial to the physical arm. Task: reach — moving the tip of the arm (tool) towards a red dot generated within th...
A webcam watches your hands. Python (using mediapipe) tracks the landmarks of both hands in real-time, translates them into angles for the 4 servomotors of the arm, and sends them via serial port to an Arduino which applies them.
...
The project involves the development of an autonomous robotic system based on a 4-degree-of-freedom (4DOF) arm.
Devices & Components
1
Arduino Uno Rev3
1
Keyestudio 4DOF Robot Arm Kit
...
An interactive robotic system (MeArm) capable of challenging a human to a game of Tic-Tac-Toe
Devices & Components
1
Arduino Uno Rev3
1
Robot Arm Kit
TrisVision MeArm
Mixed Reality a...
An autonomous 4-wheel drive explorer robot based on Arduino UNO R4 WiFi, designed to navigate through paths and mazes while detecting surrounding obstacles. The robot performs 180° radar scans via an ultrasonic sensor mounted on a servo motor...
A discovery from 2007 fully exploited in 2026 - hacking the Casio calculator serial protocol
The Arduino Uno is the board most schools already own for senior classes. Using these as cross-curricula sensor units requires adding a display, a keypad, SD...
Project: Heating System Monitor IV
Why use Heating System Monitor IV?
Answer questions your thermostat can't. A thermostat knows the setpoint. HSM IV knows what the system actually did: how many minutes the blower ran today, how long ...
www.youtube.com/watchMy project is so cool, but i have nothing to say about it. it was a pain to get this thing working. I figured it out. No one wants to hear I wired it wrong, I put the HC-SR04 on pins 9,10, only to figure out that ...
GitHub project "EoRa PI Foundation" receiver has 175 µA average current consumption using SX1262 LoRa Duty Cycle and Deep Sleep. Current measurement images; done with Nordic Power Profiler Kit II.
Project is a web based, remote load cont...
This video demonstrates how to wirelessly control two DC motors using two Arduino Unos. One Arduino acts as a controller with a joystick and XBee module, while the other acts as a receiver with a motor shield and XBee module. The video shows the conn...
Pedro 2.0 is a fully open-source project, designed to be accessible and customizable for everyone. It’s easy to assemble no screws, no glue, no tools required! Perfect for makers, students, and educators looking to explore robotics and program...
Hey, smile! Hello everyone!I made a small project with LEDs and a MAX7219 matrix.
The blue board contains an ATMega8AU-TH (but it should work with any ATMega8-AU), I bought several ICs, cheap of course (I don't think I need to advertise the website),...
This is code I cooked up in the Arduino Forum a few days ago to help someone who wanted to hack their kid's Powerwheels/Peg Perego 2WD ride on toy using a Sabertooth 2x60 motor controller.
I was never happy with Dimension Engineering exampl...
What is MQTT, and how is Arduino combined with MQTT for Internet of Things applications? These questions may have crossed your mind after reading the title.
In this article, we will learn how MQTT (Message Queuing Telemetry Transport) uses low-bandwi...
Created and installed rpi4 based router to access internet. This also has PoE hat on it..
Introduction
Recently, I was having a need for a router or a wifi range extender. Because, the high speed internet in my home router was not connec...
A stepper motor is an electric motor that moves in discrete steps. Each step is a fraction of a full rotation, and the motor's position can be controlled precisely without the need for feedback systems. This makes stepper motors hi...
A stepper motor is an electric motor that moves in discrete steps. Each step is a fraction of a full rotation, and the motor's position can be controlled precisely without the need for feedback systems. This makes stepper motors highly...
DC motors power everything from toothbrushes to robots. Controlling their speed and direction is crucial. In this project, we'll use an Arduino, a potentiometer, and a MOSFET transistor to control a DC motor. Our versatile, low-cost design can al...
Despite numerous precautions, fire accidents still occur, risking human lives during rescues and firefighting. With advancements in robotics, we can now replace humans with robots for firefighting, enhancing efficiency and safety.
In this project, we...
Just a fun simple project using the Arduino Beetle and a Z502 Dekatron tube to create a simple spinner out of this classic display tube. The design of the circuit was adapted from the circuit diagram I attached from "Dekatron Drive Basics M. Moo...
This project is not entirely Arduino, but I think it is a good example of how Arduino's can be incorporated into other systems. The initial design of this project was to automatically open and close the cat door and track the cat's activity a...